AVR1631 - Energy Meter Reference Design with ATxmega32A4  Rev 1.0
 All Data Structures Files Functions Variables Typedefs Macros
avr_compiler.h File Reference

This file implements some macros that makes the IAR C-compiler and avr-gcc work with the same code base for the AVR architecture. More...

#include <stdint.h>
#include <stdbool.h>
#include <stdlib.h>

Go to the source code of this file.

Macros

#define F_CPU   32000000UL
 Define default CPU frequency, if this is not already defined.
#define AVR_ENTER_CRITICAL_REGION()
 This macro will protect the following code from interrupts.
#define AVR_LEAVE_CRITICAL_REGION()   SREG = saved_sreg;
 This macro must always be used in conjunction with AVR_ENTER_CRITICAL_REGION so the interrupts are enabled again.

Detailed Description

This file implements some macros that makes the IAR C-compiler and avr-gcc work with the same code base for the AVR architecture.

Documentation
For comprehensive code documentation, supported compilers, compiler settings and supported devices see readme.html
Author
Atmel Corporation: http://www.atmel.com
Support email: avr@a.nosp@m.tmel.nosp@m..com
Revision:
2772
Date:
2009-09-11 12:40:26 +0200 (fr, 11 sep 2009)


Copyright (c) 2008, Atmel Corporation All rights reserved.

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

  1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
  1. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
  1. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Definition in file avr_compiler.h.

Macro Definition Documentation

#define AVR_ENTER_CRITICAL_REGION ( )
Value:
uint8_t volatile saved_sreg = SREG; \
cli();

This macro will protect the following code from interrupts.

Definition at line 58 of file avr_compiler.h.