AVR1600 Using the XMEGA Quadrature Decoder
qdec_driver.c File Reference

The XMEGA Quadrature Decoder driver source file. More...

#include "qdec_driver.h"
Include dependency graph for qdec_driver.c:

Go to the source code of this file.

Functions

bool QDEC_EVSYS_Setup (uint8_t qEvMux, EVSYS_CHMUX_t qPinInput, bool useIndex, EVSYS_QDIRM_t qIndexState)
 This function configure the event system for quadrature decoding. More...
 
uint8_t QDEC_Get_Direction (TC0_t *qTimer)
 This function return the direction of the counter/QDEC. More...
 
bool QDEC_Port_Setup (PORT_t *qPort, uint8_t qPin, bool useIndex, bool invIO)
 This function set up the needed configuration for the port used for the quadrature decoding. More...
 
void QDEC_TC_Dec_Setup (TC0_t *qTimer, TC_EVSEL_t qEventChannel, uint8_t lineCount)
 This function set up the needed configuration for the Timer/Counter to handle the quadrature decoding from the event system. More...
 
void QDEC_TC_Freq_Setup (TC0_t *qTimer, TC_EVSEL_t qEventChannel, EVSYS_CHMUX_t qPinInput, TC_CLKSEL_t clksel)
 This function set up the needed configuration for a Timer/Counter to handle the frequency/speed measurement from the event system. More...
 
bool QDEC_Total_Setup (PORT_t *qPort, uint8_t qPin, bool invIO, uint8_t qEvMux, EVSYS_CHMUX_t qPinInput, bool useIndex, EVSYS_QDIRM_t qIndexState, TC0_t *qTimer, TC_EVSEL_t qEventChannel, uint8_t lineCount)
 Wrapperfunction to set up all parameters for the quadrature decoder. More...
 

Detailed Description

The XMEGA Quadrature Decoder driver source file.

This file contains the function prototypes and enumerator definitions for various configuration parameters for the XMEGA Quadrature Decoder.

The driver is not intended for size and/or speed critical code. The driver is intended for rapid prototyping and documentation purposes for getting started with the XMEGA Quadrature Decoder.

For size and/or speed critical code, it is recommended to copy the function contents directly into your application instead of making a function call.

Several functions use the following construct: "some_register = ... | (some_parameter ? SOME_BIT_bm : 0) | ..." Although the use of the ternary operator ( if ? then : else ) is discouraged, in some occasions the operator makes it possible to write pretty clean and neat code. In this driver, the construct is used to set or not set a configuration bit based on a boolean input parameter, such as the "some_parameter" in the example above.

Application note:
AVR1600: Using the XMEGA Quadrature Decoder
Documentation
For comprehensive code documentation, supported compilers, compiler settings and supported devices see readme.html
Author
Atmel Corporation, now Microchip Technology Inc.: http://www.microchip.com
Revision
7623
Date
2017-09-06 14:57:02 +0200 (on, 06 sep 2017)

Copyright (c) 2012, Atmel Corporation All rights reserved.

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

  1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
  2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
  3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Definition in file qdec_driver.c.

Function Documentation

◆ QDEC_EVSYS_Setup()

bool QDEC_EVSYS_Setup ( uint8_t  qEvMux,
EVSYS_CHMUX_t  qPinInput,
bool  useIndex,
EVSYS_QDIRM_t  qIndexState 
)

This function configure the event system for quadrature decoding.

Parameters
qEvMuxWhich event channel to use. Only 0, 2 and 4 is available.
qPinInputThe pin input of QDPH0 to the EVSYS.CHMUX .
useIndexTrue if an optional Index pin is used.
qIndexStateIn which state the index signal will trigger.
Returns
bool True if setup was ok, false if any errors.

Definition at line 158 of file qdec_driver.c.

Referenced by QDEC_Total_Setup().

162 {
163  switch (qEvMux){
164  case 0:
165 
166  /* Configure event channel 0 for quadrature decoding of pins. */
167  EVSYS.CH0MUX = qPinInput;
168  EVSYS.CH0CTRL = EVSYS_QDEN_bm | EVSYS_DIGFILT_2SAMPLES_gc;
169  if(useIndex){
170  /* Configure event channel 1 as index channel. Note
171  * that when enabling Index in channel n, the channel
172  * n+1 must be configured for the index signal.*/
173  EVSYS.CH1MUX = qPinInput + 2;
174  EVSYS.CH1CTRL = EVSYS_DIGFILT_2SAMPLES_gc;
175  EVSYS.CH0CTRL |= (uint8_t) qIndexState | EVSYS_QDIEN_bm;
176 
177  }
178  break;
179  case 2:
180  EVSYS.CH2MUX = qPinInput;
181  EVSYS.CH2CTRL = EVSYS_QDEN_bm | EVSYS_DIGFILT_2SAMPLES_gc;
182  if(useIndex){
183  EVSYS.CH3MUX = qPinInput + 2;
184  EVSYS.CH3CTRL = EVSYS_DIGFILT_2SAMPLES_gc;
185  EVSYS.CH2CTRL |= (uint8_t) qIndexState | EVSYS_QDIEN_bm;
186  }
187  break;
188  case 4:
189  EVSYS.CH4MUX = qPinInput;
190  EVSYS.CH4CTRL = EVSYS_QDEN_bm | EVSYS_DIGFILT_2SAMPLES_gc;
191  if(useIndex){
192  EVSYS.CH5MUX = qPinInput + 2;
193  EVSYS.CH5CTRL = EVSYS_DIGFILT_2SAMPLES_gc;
194  EVSYS.CH4CTRL |= (uint8_t) qIndexState | EVSYS_QDIEN_bm;
195  }
196  break;
197  default:
198  return false;
199  }
200  return true;
201 }

◆ QDEC_Get_Direction()

uint8_t QDEC_Get_Direction ( TC0_t *  qTimer)

This function return the direction of the counter/QDEC.

Parameters
qTimerThe timer used for QDEC.
Return values
CW_DIRif clockwise/up counting,
CCW_DIRif counter clockwise/down counting.

Definition at line 255 of file qdec_driver.c.

References CCW_DIR, and CW_DIR.

256 {
257  if (qTimer->CTRLFSET & TC0_DIR_bm){
258  return CW_DIR;
259  }else{
260  return CCW_DIR;
261  }
262 }
#define CW_DIR
Definition: qdec_driver.h:63
#define CCW_DIR
Definition: qdec_driver.h:64

◆ QDEC_Port_Setup()

bool QDEC_Port_Setup ( PORT_t *  qPort,
uint8_t  qPin,
bool  useIndex,
bool  invIO 
)

This function set up the needed configuration for the port used for the quadrature decoding.

Parameters
qPortThe port to use.
qPinThe first input pin (QDPH0) to use (0 - 5/6).
useIndexTrue if an optional Index pin is used.
invIOTrue if IO pins should be inverted.
Returns
bool True if setup was ok, false if any errors.

Definition at line 118 of file qdec_driver.c.

Referenced by QDEC_Total_Setup().

119 {
120  /* Make setup depending on if Index signal is used. */
121  if(useIndex){
122  if(qPin > 5){
123  return false;
124  }
125  qPort->DIRCLR = (0x07<<qPin);
126 
127  /* Configure Index signal sensing. */
128  PORTCFG.MPCMASK = (0x04<<qPin);
129  qPort->PIN0CTRL = (qPort->PIN0CTRL & ~PORT_ISC_gm) | PORT_ISC_BOTHEDGES_gc
130  | (invIO ? PORT_INVEN_bm : 0);
131 
132 
133  }else{
134  if(qPin > 6){
135  return false;
136  }
137  qPort->DIRCLR = (0x03<<qPin);
138  }
139 
140  /* Set QDPH0 and QDPH1 sensing level. */
141  PORTCFG.MPCMASK = (0x03<<qPin);
142  qPort->PIN0CTRL = (qPort->PIN0CTRL & ~PORT_ISC_gm) | PORT_ISC_LEVEL_gc
143  | (invIO ? PORT_INVEN_bm : 0);
144 
145  return true;
146 }

◆ QDEC_TC_Dec_Setup()

void QDEC_TC_Dec_Setup ( TC0_t *  qTimer,
TC_EVSEL_t  qEventChannel,
uint8_t  lineCount 
)

This function set up the needed configuration for the Timer/Counter to handle the quadrature decoding from the event system.

Parameters
qTimerThe timer to use for QDEC.
qEventChannelThe event channel to listen to.
lineCountThe number of lines in the quadrature encoder.

Definition at line 210 of file qdec_driver.c.

Referenced by QDEC_Total_Setup().

211 {
212  /* Configure TC as a quadrature counter. */
213  qTimer->CTRLD = (uint8_t) TC_EVACT_QDEC_gc | qEventChannel;
214  qTimer->PER = (lineCount * 4) - 1;
215  qTimer->CTRLA = TC_CLKSEL_DIV1_gc;
216 }
uint8_t lineCount
Number of lines in the quadrature encoder.
Definition: qdec_example.c:72

◆ QDEC_TC_Freq_Setup()

void QDEC_TC_Freq_Setup ( TC0_t *  qTimer,
TC_EVSEL_t  qEventChannel,
EVSYS_CHMUX_t  qPinInput,
TC_CLKSEL_t  clksel 
)

This function set up the needed configuration for a Timer/Counter to handle the frequency/speed measurement from the event system.

Note
The real frequency of rotation can be calculated from the capture register by using the folowing function. FREQ = ( F_CPU / clk_div ) / ( CAPTURE * lineCount )
Parameters
qTimerThe timer to use for QDEC.
qEventChannelThe event channel to listen to.
qPinInputThe pin input of QDPH0 to the EVSYS.CHMUX.
clkselThe clk div to use for timer.

Definition at line 231 of file qdec_driver.c.

Referenced by main().

235 {
236  /* Configure channel 2 to input pin for freq calculation. */
237  EVSYS.CH2MUX = qPinInput;
238  EVSYS.CH2CTRL = EVSYS_DIGFILT_4SAMPLES_gc;
239 
240  /* Configure TC to capture frequency. */
241  qTimer->CTRLD = (uint8_t) TC_EVACT_FRQ_gc | qEventChannel;
242  qTimer->PER = 0xFFFF;
243  qTimer->CTRLB = TC0_CCAEN_bm;
244  qTimer->CTRLA = clksel;
245 }

◆ QDEC_Total_Setup()

bool QDEC_Total_Setup ( PORT_t *  qPort,
uint8_t  qPin,
bool  invIO,
uint8_t  qEvMux,
EVSYS_CHMUX_t  qPinInput,
bool  useIndex,
EVSYS_QDIRM_t  qIndexState,
TC0_t *  qTimer,
TC_EVSEL_t  qEventChannel,
uint8_t  lineCount 
)

Wrapperfunction to set up all parameters for the quadrature decoder.

This function combines the following functions for a total setup: QDEC_Port_Setup, QDEC_EVSYS_Setup and QDEC_TC_Dec_Setup.

Parameters
qPortThe port to use.
qPinThe first input pin (QDPH0) to use (0 - 5/6).
invIOTrue if IO pins should be inverted.
qEvMuxWhich event channel to use. Only 0, 2 and 4 is available.
qPinInputThe pin input of QDPH0 to the EVSYS.CHMUX .
useIndexTrue if an optional Index pin is used.
qIndexStateIn which state the index signal will trigger.
qTimerThe timer to use for QDEC.
qEventChannelThe event channel to listen to.
lineCountThe number of lines in the quadrature encoder.
Returns
bool True if setup was ok, false if any errors.

Definition at line 87 of file qdec_driver.c.

References QDEC_EVSYS_Setup(), QDEC_Port_Setup(), and QDEC_TC_Dec_Setup().

Referenced by main().

97 {
98  if( !QDEC_Port_Setup(qPort, qPin, useIndex, invIO) )
99  return false;
100  if( !QDEC_EVSYS_Setup(qEvMux, qPinInput, useIndex, qIndexState ) )
101  return false;
102  QDEC_TC_Dec_Setup(qTimer, qEventChannel, lineCount);
103 
104  return true;
105 }
bool QDEC_EVSYS_Setup(uint8_t qEvMux, EVSYS_CHMUX_t qPinInput, bool useIndex, EVSYS_QDIRM_t qIndexState)
This function configure the event system for quadrature decoding.
Definition: qdec_driver.c:158
bool QDEC_Port_Setup(PORT_t *qPort, uint8_t qPin, bool useIndex, bool invIO)
This function set up the needed configuration for the port used for the quadrature decoding...
Definition: qdec_driver.c:118
uint8_t lineCount
Number of lines in the quadrature encoder.
Definition: qdec_example.c:72
void QDEC_TC_Dec_Setup(TC0_t *qTimer, TC_EVSEL_t qEventChannel, uint8_t lineCount)
This function set up the needed configuration for the Timer/Counter to handle the quadrature decoding...
Definition: qdec_driver.c:210
Here is the call graph for this function:
@DOC_TITLE@
Generated on Thu Oct 26 2017 13:33:37 for AVR1600 Using the XMEGA Quadrature Decoder by doxygen 1.8.13