![]() |
AVR1600 Using the XMEGA Quadrature Decoder
|
This file implements some macros that makes the IAR C-compiler and avr-gcc work with the same code base for the AVR architecture. More...
#include <stdint.h>#include <stdbool.h>#include <stdlib.h>

Go to the source code of this file.
Macros | |
| #define | AVR_ENTER_CRITICAL_REGION() |
| This macro will protect the following code from interrupts. More... | |
| #define | AVR_LEAVE_CRITICAL_REGION() SREG = saved_sreg; |
| This macro must always be used in conjunction with AVR_ENTER_CRITICAL_REGION so the interrupts are enabled again. More... | |
| #define | F_CPU 2000000UL |
| Define default CPU frequency, if this is not already defined. More... | |
This file implements some macros that makes the IAR C-compiler and avr-gcc work with the same code base for the AVR architecture.
Copyright (c) 2008, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file avr_compiler.h.
| #define AVR_ENTER_CRITICAL_REGION | ( | ) |
This macro will protect the following code from interrupts.
Definition at line 57 of file avr_compiler.h.
| #define AVR_LEAVE_CRITICAL_REGION | ( | ) | SREG = saved_sreg; |
This macro must always be used in conjunction with AVR_ENTER_CRITICAL_REGION so the interrupts are enabled again.
Definition at line 63 of file avr_compiler.h.
| #define F_CPU 2000000UL |
Define default CPU frequency, if this is not already defined.
Definition at line 49 of file avr_compiler.h.
Referenced by generate_qdec_signal(), and main().
Generated on Thu Oct 26 2017 13:33:37 for AVR1600 Using the XMEGA Quadrature Decoder by 1.8.13
|