| Xmega Application Note | |||||
#include "avr_compiler.h"
#include "clksys_driver.h"

Go to the source code of this file.
Defines | |
| #define | LEDMASK 0xFF |
| #define | LEDPORT PORTD |
| #define | SWITCHMASK 0xFF |
| #define | SWITCHPORT PORTC |
Functions | |
| ISR (TCC0_OVF_vect) | |
| int | main (void) |
| Example code that switch between different clocks. | |
| void | WaitForSwitches (void) |
| This function waits for a button push and release before proceeding. | |
This file contains an example application that demonstrates the Clock System driver. The recommended setup for this demonstration is to connect an external 2-9MHz crystal to the XTAL1/XTAL2 pins with proper decoupling.
Copyright (c) 2008, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file clksys_example.c.
| #define LEDMASK 0xFF |
| #define LEDPORT PORTD |
| #define SWITCHMASK 0xFF |
| #define SWITCHPORT PORTC |
| ISR | ( | TCC0_OVF_vect | ) |
| int main | ( | void | ) |
Example code that switch between different clocks.
This example code shows how to change between 5 different system clocks and how to prescale and divide the clocks to make use of dynamic clocking for the different parts on the device. When changes are made to the clocks, blocking functions are used to make sure the clocks are stable before they can be used.
Definition at line 76 of file clksys_example.c.
References CLKSYS_Disable(), CLKSYS_Enable, CLKSYS_IsReady, CLKSYS_Main_ClockSource_Select(), CLKSYS_PLL_Config(), CLKSYS_Prescalers_Config(), CLKSYS_XOSC_Config(), LEDMASK, LEDPORT, SWITCHMASK, SWITCHPORT, and WaitForSwitches().
00077 { 00078 /* Set up user interface. */ 00079 LEDPORT.DIRSET = LEDMASK; 00080 LEDPORT.OUTSET = LEDMASK; 00081 SWITCHPORT.DIRCLR = SWITCHMASK; 00082 00083 /* Set up Timer/Counter 0 to work from CPUCLK/64, with period 10000 and 00084 * enable overflow interrupt. 00085 */ 00086 TCC0.PER = 10000; 00087 TCC0.CTRLA = ( TCC0.CTRLA & ~TC0_CLKSEL_gm ) | TC_CLKSEL_DIV64_gc; 00088 TCC0.INTCTRLA = ( TCC0.INTCTRLA & ~TC0_OVFINTLVL_gm ) | 00089 TC_OVFINTLVL_MED_gc; 00090 00091 /* Enable low interrupt level in PMIC and enable global interrupts. */ 00092 PMIC.CTRL |= PMIC_MEDLVLEN_bm; 00093 sei(); 00094 00095 00096 /* This while loop run through and switch between the different 00097 * system clock sources available. 00098 */ 00099 while(1) { 00100 00101 /* Wait for user input while the LEDs toggle. */ 00102 WaitForSwitches(); 00103 00104 00105 /* Enable internal 32 MHz ring oscillator and wait until it's 00106 * stable. Divide clock by two with the prescaler C and set the 00107 * 32 MHz ring oscillator as the main clock source. Wait for 00108 * user input while the LEDs toggle. 00109 */ 00110 CLKSYS_Enable( OSC_RC32MEN_bm ); 00111 CLKSYS_Prescalers_Config( CLK_PSADIV_1_gc, CLK_PSBCDIV_1_2_gc ); 00112 do {} while ( CLKSYS_IsReady( OSC_RC32MRDY_bm ) == 0 ); 00113 CLKSYS_Main_ClockSource_Select( CLK_SCLKSEL_RC32M_gc ); 00114 WaitForSwitches( ); 00115 00116 00117 /* Enable for external 2-9 MHz crystal with quick startup time 00118 * (256CLK). Check if it's stable and set the external 00119 * oscillator as the main clock source. Wait for user input 00120 * while the LEDs toggle. 00121 */ 00122 CLKSYS_XOSC_Config( OSC_FRQRANGE_2TO9_gc, 00123 false, 00124 OSC_XOSCSEL_EXTCLK_gc ); 00125 CLKSYS_Enable( OSC_XOSCEN_bm ); 00126 do {} while ( CLKSYS_IsReady( OSC_XOSCRDY_bm ) == 0 ); 00127 CLKSYS_Main_ClockSource_Select( CLK_SCLKSEL_XOSC_gc ); 00128 CLKSYS_Disable( OSC_RC32MEN_bm ); 00129 WaitForSwitches(); 00130 00131 00132 /* Divide Prescaler C by two and Prescaler C by two, and wait 00133 * for user input. 00134 */ 00135 CLKSYS_Prescalers_Config( CLK_PSADIV_1_gc, CLK_PSBCDIV_2_2_gc ); 00136 WaitForSwitches(); 00137 00138 00139 /* Enable internal 32 kHz calibrated oscillator and check for 00140 * it to be stable and set prescaler A, B and C to none. Set 00141 * the 32 kHz oscillator as the main clock source. Wait for 00142 * user input while the LEDs toggle. 00143 */ 00144 CLKSYS_Enable( OSC_RC32KEN_bm ); 00145 CLKSYS_Prescalers_Config( CLK_PSADIV_1_gc, CLK_PSBCDIV_1_1_gc ); 00146 do {} while ( CLKSYS_IsReady( OSC_RC32KRDY_bm ) == 0 ); 00147 CLKSYS_Main_ClockSource_Select( CLK_SCLKSEL_RC32K_gc ); 00148 CLKSYS_Disable( OSC_XOSCEN_bm ); 00149 WaitForSwitches(); 00150 00151 00152 /* Configure PLL with the 2 MHz RC oscillator as source and 00153 * multiply by 30 to get 60 MHz PLL clock and enable it. Wait 00154 * for it to be stable and set prescaler C to divide by two 00155 * to set the CPU clock to 30 MHz. Disable unused clock and 00156 * wait for user input. 00157 */ 00158 CLKSYS_PLL_Config( OSC_PLLSRC_RC2M_gc, 30 ); 00159 CLKSYS_Enable( OSC_PLLEN_bm ); 00160 CLKSYS_Prescalers_Config( CLK_PSADIV_1_gc, CLK_PSBCDIV_1_2_gc ); 00161 do {} while ( CLKSYS_IsReady( OSC_PLLRDY_bm ) == 0 ); 00162 CLKSYS_Main_ClockSource_Select( CLK_SCLKSEL_PLL_gc ); 00163 CLKSYS_Disable( OSC_XOSCEN_bm ); 00164 WaitForSwitches( ); 00165 00166 00167 /* Select 2 MHz RC oscillator as main clock source and diable 00168 * unused clock. 00169 */ 00170 do {} while ( CLKSYS_IsReady( OSC_RC2MRDY_bm ) == 0 ); 00171 CLKSYS_Main_ClockSource_Select( CLK_SCLKSEL_RC2M_gc ); 00172 CLKSYS_Disable( OSC_PLLEN_bm ); 00173 00174 } 00175 }

| void WaitForSwitches | ( | void | ) |
This function waits for a button push and release before proceeding.
Definition at line 179 of file clksys_example.c.
References SWITCHMASK, and SWITCHPORT.
Referenced by main().
00180 { 00181 do {} while ( ( SWITCHPORT.IN & SWITCHMASK ) == SWITCHMASK ); 00182 delay_us( 1000 ); 00183 do {} while ( ( SWITCHPORT.IN & SWITCHMASK ) != SWITCHMASK ); 00184 delay_us( 1000 ); 00185 }
Generated on Mon Sep 14 09:48:10 2009 for AVR1003 Using the XMEGA Clock System by 1.5.8
|