I N L I N E    A S M

GCC asm Statement
=================
       asm ( assembler template 
           : output operands                  /* optional */
           : input operands                   /* optional */
           : list of clobbered registers      /* optional */
           );
           
Let's start with a simple example of reading a value from port D:
    asm("in %0, %1" : "=r" (value) : "I" (_SFR_IO_ADDR(PORTD)) );

Each asm statement is devided by colons into (up to) four parts:
    1. The assembler instructions, defined as a single string constant:
       "in %0, %1"
    2. A list of output operands, separated by commas. Our example uses just
       one:
       "=r" (value)
    3. A comma separated list of input operands. Again our example uses one 
       operand only:
       "I" (_SFR_IO_ADDR(PORTD))
    4. Clobbered registers, left empty in our example.

   You can write assembler instructions in much the same way as you would write 
assembler programs. However, registers and constants are used in a different 
way if they refer to expressions of your C program. The connection between 
registers and C operands is specified in the second and third part of the 
asm instruction, the list of input and output operands, respectively. The 
general form is:
    asm(code : output operand list : input operand list [: clobber list]);

    In the code section, operands are referenced by a percent sign followed by a 
single digit. 0 refers to the first 1 to the second operand and so forth. From 
the above example:
    0 refers to "=r" (value) and
    1 refers to "I" (_SFR_IO_ADDR(PORTD)).

This may still look a little odd now, but the syntax of an operand list will be 
explained soon. Let us first examine the part of a compiler listing which may 
have been generated from our example:
    lds r24,value 
/* #APP */ 
    in r24, 12 
/* #NOAPP */ 
    sts value,r24

The comments have been added by the compiler to inform the assembler that the 
included code was not generated by the compilation of C statements, but by 
inline assembler statements. The compiler selected register r24 for storage of 
the value read from PORTD. The compiler could have selected any other register, 
though. It may not explicitely load or store the value and it may even decide 
not to include your assembler code at all. All these decisions are part of the 
compiler's optimization strategy. For example, if you never use the variable 
value in the remaining part of the C program, the compiler will most likely 
remove your code unless you switched off optimization. To avoid this, you can 
add the volatile attribute to the asm statement:
    asm volatile("in %0, %1" : "=r" (value) : "I" (_SFR_IO_ADDR(PORTD)));

The last part of the asm instruction, the clobber list, is mainly used to tell 
the compiler about modifications done by the assembler code. This part may be 
omitted, all other parts are required, but may be left empty. If your assembler 
routine won't use any input or output operand, two colons must still follow the 
assembler code string. A good example is a simple statement to disable 
interrupts:
    asm volatile("cli"::);

Assembler Code
==============
You can use the same assembler instruction mnemonics as you'd use with any 
other AVR assembler. And you can write as many assembler statements into one 
code string as you like and your flash memory is able to hold.

Note:
    The available assembler directives vary from one assembler to another.

To make it more readable, you should put each statement on a seperate line:
    asm volatile("nop\n\t" 
                 "nop\n\t" 
                 "nop\n\t" 
                 "nop\n\t" ::);

The linefeed and tab characters will make the assembler listing generated by 
the compiler more readable. It may look a bit odd for the first time, but 
that's the way the compiler creates it's own assembler code.

You may also make use of some special registers.

,--------------,-----------------------------------------,
|    Symbol    |         Register                        |
|--------------+-----------------------------------------|
| __SREG__     | Status register at address 0x3F         |
| __SP_H__     | Stack pointer high byte at address 0x3E |
| __SP_L__     | Stack pointer low byte at address 0x3D  |
| __tmp_reg__  | Register r0, used for temporary storage |
| __zero_reg__ | Register r1, always zero                |
'--------------'-----------------------------------------'

Register r0 may be freely used by your assembler code and need not be restored 
at the end of your code. It's a good idea to use __tmp_reg__ and __zero_reg__ 
instead of r0 or r1, just in case a new compiler version changes the register 
usage definitions.

Input and Output Operands
=========================
Each input and output operand is described by a constraint string followed by 
a C expression in parantheses. AVR-GCC 3.3 knows the following constraint 
characters:

Note:
    The most up-to-date and detailed information on contraints for the avr can 
    be found in the gcc manual.

    The x register is r27:r26, the y register is r29:r28, 
    and the z register is r31:r30

,------------,---------------------------------,--------------------,
| Constraint |            Used for             |       Range        |
|------------+---------------------------------+--------------------|
|     a      | Simple upper registers          | r16 to r23         | 
|     b      | Base pointer registers pairs    | y, z               | 
|     d      | Upper register                  | r16 to r31         |
|     e      | Pointer register pairs          | x, y, z            |
|     G      | Floating point constant         | 0.0                |
|     I      | 6-bit positive integer constant | 0 to 63            |
|     J      | 6-bit negative integer constant | -63 to 0           |
|     K      | Integer constant                | 2                  |
|     L      | Integer constant                | 0                  |
|     l      | Lower registers                 | r0 to r15          |
|     M      | 8-bit integer constant          | 0 to 255           |
|     N      | Integer constant                | -1                 |
|     O      | Integer constant                | 8, 16, 24          |
|     P      | Integer constant                | 1                  |
|     q      | Stack pointer register          | SPH:SPL            |
|     r      | Any register                    | r0 to r31          |
|     t      | Temporary register              | r0                 |
|     w      | Special upper register pairs    | r24, r26, r28, r30 |
|     x      | Pointer register pair X  x      | (r27:r26)          |
|     y      | Pointer register pair Y  y      | (r29:r28)          |
|     z      | Pointer register pair Z  z      | (r31:r30)          |
'------------'---------------------------------'--------------------'

These definitions seem not to fit properly to the AVR instruction set. The 
author's assumption is, that this part of the compiler has never been really 
finished in this version, but that assumption may be wrong. The selection of 
the proper contraint depends on the range of the constants or registers, which 
must be acceptable to the AVR instruction they are used with. The C compiler 
doesn't check any line of your assembler code. But it is able to check the 
constraint against your C expression. However, if you specify the wrong 
constraints, then the compiler may silently pass wrong code to the assembler. 
And, of course, the assembler will fail with some cryptic output or internal 
errors. For example, if you specify the constraint "r" and you are using this 
register with an "ori" instruction in your assembler code, then the compiler 
may select any register. This will fail, if the compiler chooses r2 to r15. 
(It will never choose r0 or r1, because these are uses for special purposes.) 
That's why the correct constraint in that case is "d". On the other hand, if 
you use the constraint "M", the compiler will make sure that you don't pass 
anything else but an 8-bit value. Later on we will see how to pass multibyte 
expression results to the assembler code.

The following table shows all AVR assembler mnemonics which require operands, 
and the related contraints. Because of the improper constraint definitions 
in version 3.3, they aren't strict enough. There is, for example, no 
constraint, which restricts integer constants to the range 0 to 7 for bit set 
and bit clear operations.

,----------,-------------,----------,-------------,
| Mnemonic | Constraints | Mnemonic | Constraints |
|----------+-------------+----------+-------------|
|      adc | r,r         |     add  | r,r         |
|     adiw | w,I         |     and  | r,r         |
|     andi | d,M         |     asr  | r           |
|     bclr | I           |     bld  | r,I         |
|     brbc | I,label     |    brbs  | I,label     |
|     bset | I           |     bst  | r,I         |
|      cbi | I,I         |     cbr  | d,I         |
|      com | r           |      cp  | r,r         |
|      cpc | r,r         |     cpi  | d,M         |
|     cpse | r,r         |     dec  | r           |
|     elpm | t,z         |     eor  | r,r         |
|       in | r,I         |     inc  | r           |
|       ld | r,e         |     ldd  | r,b         |
|      ldi | d,M         |     lds  | r,label     |
|      lpm | t,z         |     lsl  | r           |
|      lsr | r           |     mov  | r,r         |
|     movw | r,r         |     mul  | r,r         |
|      neg | r           |      or  | r,r         |
|      ori | d,M         |     out  | I,r         |
|      pop | r           |    push  | r           |
|      rol | r           |     ror  | r           |
|      sbc | r,r         |    sbci  | d,M         |
|      sbi | I,I         |    sbic  | I,I         |
|     sbiw | w,I         |     sbr  | d,M         |
|     sbrc | r,I         |    sbrs  | r,I         |
|      ser | d           |      st  | e,r         |
|      std | b,r         |     sts  | label,r     |
|      sub | r,r         |    subi  | d,M         |
|     swap | r           |----------'-------------'
'----------'-------------'

Constraint characters may be prepended by a single constraint modifier. 
Contraints without a modifier specify read-only operands. Modifiers are:

,----------,----------------------------------------------------------,
| Modifier | Specifies                                                |
|----------+----------------------------------------------------------|
|    =     | Write-only operand, usually used for all output operands |
|    +     | Read-write operand (not supported by inline assembler)   |
|    &     | Register should be used for output only                  |
'----------'----------------------------------------------------------'

Output operands must be write-only and the C expression result must be an 
lvalue, which means that the operands must be valid on the left side of 
assignments. Note, that the compiler will not check if the operands are of 
reasonable type for the kind of operation used in the assembler instructions.

Input operands are, you guessed it, read-only. But what if you need the same 
operand for input and output? As stated above, read-write operands are not 
supported in inline assembler code. But there is another solution. For input 
operators it is possible to use a single digit in the constraint string. Using 
digit n tells the compiler to use the same register as for the n-th operand, 
starting with zero. Here is an example:
    asm volatile("swap %0" : "=r" (value) : "0" (value));

This statement will swap the nibbles of an 8-bit variable named value. 
Constraint "0" tells the compiler, to use the same input register as for the 
first operand. Note however, that this doesn't automatically imply the reverse 
case. The compiler may choose the same registers for input and output, even if 
not told to do so. This is not a problem in most cases, but may be fatal if the 
output operator is modified by the assembler code before the input operator is 
used. In the situation where your code depends on different registers used for 
input and output operands, you must add the & constraint modifier to your 
output operand. The following example demonstrates this problem:
    asm volatile("in %0,%1" "\n\t"
                 "out %1, %2" "\n\t" 
                 : "=&r" (input) 
                 : "I" (_SFR_IO_ADDR(port)), "r" (output) 
                 );
                 
In this example an input value is read from a port and then an output value is 
written to the same port. If the compiler would have choosen the same register 
for input and output, then the output value would have been destroyed on the 
first assembler instruction. Fortunately, this example uses the & constraint
modifier to instruct the compiler not to select any register for the output 
value, which is used for any of the input operands. Back to swapping. Here is 
the code to swap high and low byte of a 16-bit value:
    asm volatile("mov __tmp_reg__, %A0" "\n\t" 
                 "mov %A0, %B0" "\n\t" 
                 "mov %B0, __tmp_reg__" "\n\t" 
                 : "=r" (value) 
                 : "0" (value) 
                 );

First you will notice the usage of register __tmp_reg__, which we listed 
among other special registers in the Assembler Code section. You can use 
this register without saving its contents. Completely new are those letters 
A and B in %A0 and %B0. In fact they refer to two different 8-bit registers, 
both containing a part of value.

Another example to swap bytes of a 32-bit value:
    asm volatile("mov __tmp_reg__, %A0" "\n\t" 
                 "mov %A0, %D0" "\n\t" 
                 "mov %D0, __tmp_reg__" "\n\t" 
                 "mov __tmp_reg__, %B0" "\n\t" 
                 "mov %B0, %C0" "\n\t" 
                 "mov %C0, __tmp_reg__" "\n\t" 
                 : "=r" (value) 
                 : "0" (value) 
                 );

If operands do not fit into a single register, the compiler will automatically 
assign enough registers to hold the entire operand. In the assembler code you 
use %A0 to refer to the lowest byte of the first operand, %A1 to the lowest 
byte of the second operand and so on. The next byte of the first operand will 
be %B0, the next byte %C0 and so on.

This also implies, that it is often neccessary to cast the type of an input 
operand to the desired size.

A final problem may arise while using pointer register pairs. If you define an 
input operand
    "e" (ptr)
and the compiler selects register Z (r30:r31), then
    %A0 refers to r30 and
    %B0 refers to r31.

But both versions will fail during the assembly stage of the compiler, if you 
explicitely need Z, like in
    ld r24,Z
If you write
    ld r24, %a0
with a lower case a following the percent sign, then the compiler will create 
the proper assembler line.

Clobbers
========
Parfois une instruction "demolie" certains registres spcifiques. L'exemple le 
plus commun de ceci d'un appel de fonction, o la fonction appele se permet 
de faire ce que bon lui semble avec certains registres.
Si c'est le cas, vous pouvez numrer les registres spcifiques qui sont
"demolis" par une opration aprs les entres. La syntaxe n'est pas la meme que
des contraintes, vous fournissez juste une liste de registres.
Il y a deux cas spciaux pour des valeurs "demolies". L'une est "memory",
signifiant que cette instruction crit en mmoire (ailleurs que dans la liste de
sorties) et GCC ne doit pas mettre en cache de valeurs dans des registres
au travers cet ASM. Une excution de memcpy() d'ASM aurait besoin de ceci.
Vous *pas* devez numrer la "mmoire" juste parce que les sorties sont dans la
mmoire ; le GCC comprend cela.


As stated previously, the last part of the asm statement, the list of clobbers, 
may be omitted, including the colon seperator. However, if you are using 
registers, which had not been passed as operands, you need to inform the 
compiler about this. The following example will do an atomic increment. It 
increments an 8-bit value pointed to by a pointer variable in one go, without 
being interrupted by an interrupt routine or another thread in a multithreaded 
environment. Note, that we must use a pointer, because the incremented value 
needs to be stored before interrupts are enabled.

asm volatile("cli"           "\n\t" 
             "ld r24, %a0"   "\n\t" 
             "inc r24"       "\n\t" 
             "st %a0, r24"   "\n\t" 
             "sei"           "\n\t" 
             : 
             : "e" (ptr) 
             : "r24" 
             );

The compiler might produce the following code:

    cli 
    ld r24, Z 
    inc r24 
    st Z, r24 
    sei

One easy solution to avoid clobbering register r24 is, to make use of the 
special temporary register __tmp_reg__ defined by the compiler.

asm volatile("cli"                   "\n\t" 
             "ld __tmp_reg__, %a0"   "\n\t" 
             "inc __tmp_reg__"       "\n\t" 
             "st %a0, __tmp_reg__"   "\n\t" 
             "sei"                   "\n\t" 
             : 
             : "e" (ptr) 
             );

The compiler is prepared to reload this register next time it uses it. 
Another problem with the above code is, that it should not be called in code 
sections, where interrupts are disabled and should be kept disabled, because 
it will enable interrupts at the end. We may store the current status, but then 
we need another register. Again we can solve this without clobbering a fixed, 
but let the compiler select it. This could be done with the help of a local C 
variable.

{ 
uint8_t s; 
asm volatile("in %0, __SREG__"       "\n\t" 
             "cli"                   "\n\t" 
             "ld __tmp_reg__, %a1"   "\n\t" 
             "inc __tmp_reg__"       "\n\t" 
             "st %a1, __tmp_reg__"   "\n\t" 
             "out __SREG__, %0"      "\n\t" 
             : "=&r" (s) 
             : "e" (ptr) 
             ); 
}

Now every thing seems correct, but it isn't really. The assembler code modifies 
the variable, that ptr points to. The compiler will not recognize this and may 
keep its value in any of the other registers. Not only does the compiler work 
with the wrong value, but the assembler code does too. The C program may have 
modified the value too, but the compiler didn't update the memory location for 
optimization reasons. The worst thing you can do in this case is:

{ 
uint8_t s; 
asm volatile("in %0, __SREG__" "\n\t" 
             "cli" "\n\t" 
             "ld __tmp_reg__, %a1" "\n\t" 
             "inc __tmp_reg__" "\n\t" 
             "st %a1, __tmp_reg__" "\n\t" 
             "out __SREG__, %0" "\n\t" 
             : "=&r" (s) 
             : "e" (ptr) : "memory" 
             ); 
}

The special clobber "memory" informs the compiler that the assembler code may 
modify any memory location. It forces the compiler to update all variables for 
which the contents are currently held in a register before executing the 
assembler code. And of course, everything has to be reloaded again after this 
code.

In most situations, a much better solution would be to declare the pointer 
destination itself volatile:

volatile uint8_t *ptr;

This way, the compiler expects the value pointed to by ptr to be changed and 
will load it whenever used and store it whenever modified.

Situations in which you need clobbers are very rare. In most cases there will 
be better ways. Clobbered registers will force the compiler to store their 
values before and reload them after your assembler code. Avoiding clobbers 
gives the compiler more freedom while optimizing your code.

C Stub Functions
================
Macro definitions will include the same assembler code whenever they are 
referenced. This may not be acceptable for larger routines. In this case you 
may define a C stub function, containing nothing other than your assembler code.

void delay(uint8_t ms) 
{ 
uint16_t cnt; 
asm volatile ("\n"
              "L_dl1%=:" "\n\t" 
              "mov %A0, %A2"  "\n\t" 
              "mov %B0, %B2"  "\n\t" 
              "L_dl2%=:"      "\n\t" 
              "sbiw %A0, 1"   "\n\t" 
              "brne L_dl2%="  "\n\t" 
              "dec %1"        "\n\t" 
              "brne L_dl1%="  "\n\t" 
              : "=&w" (cnt) 
              : "r" (ms), "r" (delay_count)
              );
}

The purpose of this function is to delay the program execution by a specified 
number of milliseconds using a counting loop. The global 16 bit variable 
delay_count must contain the CPU clock frequency in Hertz divided by 4000 and 
must have been set before calling this routine for the first time. As described 
in the clobber section, the routine uses a local variable to hold a temporary 
value.

Another use for a local variable is a return value. The following function 
returns a 16 bit value read from two successive port addresses.

uint16_t inw(uint8_t port) 
{ 
uint16_t result; 
asm volatile ("in %A0,%1"        "\n\t" 
              "in %B0,(%1) + 1"  "\n\t"
              : "=r" (result) 
              : "I" (_SFR_IO_ADDR(port)) 
              );
return result; 
}

Note:
    inw() is supplied by avr-libc.

================================================================================

#define rep_movsl(src, dest, numwords) \
    __asm__ __volatile__ ( \
                           "cld\n\t" \
                           "rep\n\t" \
                           "movsl" \
                            : : "S" (src), "D" (dest), "c" (numwords) \
                            : "%ecx", "%esi", "%edi" )
                            
================================================================================
                            
#define __boot_page_write_normal(address)                       \
    ({ __asm__ __volatile__(                                    \
                            "movw r30, %2\n\t"                  \
                            "sts %0, %1\n\t"                    \
                            "spm\n\t"                           \
                            : "=m" (__SPM_REG)                  \
                            : "r" ((uint8_t)__BOOT_PAGE_WRITE), \
                              "r" ((uint16_t)address)           \
                            : "r30", "r31"                      \
                           );                                   \
    })

================================================================================

#define __boot_lock_bits_set_alternate(lock_bits)          \
({                                                         \
    uint8_t value = (uint8_t)(~(lock_bits));               \
    __asm__ __volatile__                                   \
    (                                                      \
        "ldi r30, 1\n\t"                                   \
        "ldi r31, 0\n\t"                                   \
        "mov r0, %2\n\t"                                   \
        "sts %0, %1\n\t"                                   \
        "spm\n\t"                                          \
        ".word 0xffff\n\t"                                 \
        "nop\n\t"                                          \
        : "=m" (__SPM_REG)                                 \
        : "r" ((uint8_t)__BOOT_LOCK_BITS_SET),       \
          "r" (value)                                      \
        : "r0", "r30", "r31"                               \
    );                                                     \
})

================================================================================

PAS DE COMMENTAIRE DANS LE CORPS DE LA FONCTION ECRITE EN ASSEMBLEUR !!!!!