| Xmega Application Note | |||||
This file contains an example application that demonstrates the AES driver using back to back polled functions.
Copyright (c) 2008, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file AES_example_backtoback.c.
#include "avr_compiler.h"
#include "AES_driver.h"

Go to the source code of this file.
Defines | |
| #define | BLOCK_COUNT 3 |
| #define | BLOCK_LENGTH 16 |
Functions | |
| int | main (void) |
Variables | |
| uint8_t | data1 [BLOCK_LENGTH] |
| uint8_t | data2 [BLOCK_LENGTH] |
| uint8_t | key [BLOCK_LENGTH] |
| uint8_t | lastsubkey [BLOCK_LENGTH] |
| uint8_t | read_key [BLOCK_LENGTH] |
| uint8_t | single_ans1 [BLOCK_LENGTH] |
| uint8_t | single_ans2 [BLOCK_LENGTH] |
| bool | success |
| #define BLOCK_COUNT 3 |
| #define BLOCK_LENGTH 16 |
| int main | ( | void | ) |
Definition at line 79 of file AES_example_backtoback.c.
References AES_decrypt_backtoback(), AES_encrypt(), AES_encrypt_backtoback(), AES_software_reset, BLOCK_LENGTH, data1, data2, key, single_ans1, single_ans2, and success.
00080 { 00081 /* Assume that everything is ok*/ 00082 success = true; 00083 00084 /* Before using the AES it is recommended to do an AES software reset to put 00085 * the module in known state, in case other parts of your code has accessed 00086 * the AES module. */ 00087 AES_software_reset(); 00088 00089 /* Do AES encryption and decryption every other time with the same key on 00090 * two data blocks. */ 00091 success = AES_encrypt(data1, single_ans1, key); 00092 success = AES_decrypt_backtoback(single_ans1, single_ans1); 00093 success = AES_encrypt_backtoback(data2, single_ans2); 00094 success = AES_decrypt_backtoback(single_ans2, single_ans2); 00095 00096 /* Check if decrypted answers is equal to plaintext. */ 00097 for(uint8_t i = 0; i < BLOCK_LENGTH ; i++ ){ 00098 if (data1[i] != single_ans1[i]){ 00099 success = false; 00100 } 00101 if (data2[i] != single_ans2[i]){ 00102 success = false; 00103 } 00104 } 00105 00106 if(success){ 00107 while(true){ 00108 /* If the example ends up here every thing is ok. */ 00109 nop(); 00110 } 00111 }else{ 00112 while(true){ 00113 /* If the example ends up here something is wrong. */ 00114 nop(); 00115 } 00116 } 00117 }

| uint8_t data1[BLOCK_LENGTH] |
Initial value:
{0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08,
0x09, 0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16}
Definition at line 57 of file AES_example_backtoback.c.
Referenced by main().
| uint8_t data2[BLOCK_LENGTH] |
Initial value:
{0xAA, 0xAA, 0xAA, 0xBB, 0xBB, 0xBB, 0xCC, 0xCC,
0xCC, 0xDD, 0xDD, 0xDD, 0xEE, 0xEE, 0xEE, 0x0F}
Definition at line 60 of file AES_example_backtoback.c.
Referenced by main().
| uint8_t key[BLOCK_LENGTH] |
Initial value:
{0x94, 0x74, 0xB8, 0xE8, 0xC7, 0x3B, 0xCA, 0x7D,
0x28, 0x34, 0x76, 0xAB, 0x38, 0xCF, 0x37, 0xC2}
Definition at line 68 of file AES_example_backtoback.c.
Referenced by main().
| uint8_t lastsubkey[BLOCK_LENGTH] |
| uint8_t read_key[BLOCK_LENGTH] |
Definition at line 73 of file AES_example_backtoback.c.
| uint8_t single_ans1[BLOCK_LENGTH] |
| uint8_t single_ans2[BLOCK_LENGTH] |
| bool success |
Generated on Wed Apr 23 08:53:41 2008 for AVR1318 Using the XMEGA built in AES accelerator by 1.5.5
|