| Xmega Application Note | |||||
This file contains an example application that demonstrates the DES driver. It shows how to do a DES encryption and decryption, a 3DES encryption and decryption and a DES cipher block chaining encryption and decryption. It can be used with both the driver optimized for speed and the driver optimized for size.
Copyright (c) 2008, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DES_example.c.
#include "avr_compiler.h"
#include "DES_driver.h"

Go to the source code of this file.
Defines | |
| #define | DES_BLOCK_COUNT 3 |
| #define | DES_BLOCK_LENGTH 8 |
Functions | |
| int | main (void) |
| Main example doing DES encryption/decryption. | |
Variables | |
| uint8_t | block_ans [DES_BLOCK_LENGTH *DES_BLOCK_COUNT] |
| Variable used to store decrypted plaintext from DES Cipher Block Chaining. | |
| uint8_t | cipher_block_ans [DES_BLOCK_LENGTH *DES_BLOCK_COUNT] |
| Variable used to store ciphertext from DES Cipher Block Chaining. | |
| uint8_t | data [DES_BLOCK_LENGTH] = {0xAB, 0xBA, 0x00, 0xBE, 0xEF, 0x00, 0xDE, 0xAD} |
| Plaintext block used by DES and 3DES. | |
| uint8_t | data_block [DES_BLOCK_LENGTH *DES_BLOCK_COUNT] |
| Plain text used during DES Cipher Block Chaining. | |
| uint8_t | init [DES_BLOCK_LENGTH] = {0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88} |
| Initial vector used during DES Cipher Block Chaining. | |
| uint8_t | keys [DES_BLOCK_LENGTH *DES_BLOCK_COUNT] |
| Keys used by all DES operations. (single DES only uses the first 64-bit key). | |
| uint8_t | single_ans [DES_BLOCK_LENGTH] |
| Variable used to store DES and tripleDES results. | |
| #define DES_BLOCK_COUNT 3 |
| #define DES_BLOCK_LENGTH 8 |
| int main | ( | void | ) |
Main example doing DES encryption/decryption.
Definition at line 102 of file DES_example.c.
References block_ans, cipher_block_ans, data, data_block, DES_3DES_Decrypt(), DES_3DES_Encrypt(), DES_BLOCK_COUNT, DES_BLOCK_LENGTH, DES_CBC_Decrypt(), DES_CBC_Encrypt(), DES_Decrypt(), DES_Encrypt(), init, keys, and single_ans.
00103 { 00104 bool success = true; 00105 00106 /* Example of how to use Single DES encryption and decryption functions. */ 00107 DES_Encrypt(data, single_ans, keys); 00108 DES_Decrypt(single_ans, single_ans, keys); 00109 00110 /* Check if decrypted answer is equal to plaintext. */ 00111 for (uint8_t i = 0; i < DES_BLOCK_LENGTH ; i++ ){ 00112 if (data[i] != single_ans[i]){ 00113 success = false; 00114 break; 00115 } 00116 } 00117 00118 if (success){ 00119 00120 /* Example of how to use 3DES encryption and decryption functions. */ 00121 DES_3DES_Encrypt(data, single_ans, keys); 00122 DES_3DES_Decrypt(single_ans, single_ans, keys); 00123 00124 /* Check if decrypted answer is equal to plaintext. */ 00125 for (uint8_t i = 0; i < DES_BLOCK_LENGTH ; i++ ){ 00126 if (data[i] != single_ans[i]){ 00127 success = false; 00128 break; 00129 } 00130 } 00131 } 00132 00133 if (success){ 00134 /* Example of how to use DES Cipher Block Chaining encryption and 00135 * decryption functions. 00136 */ 00137 DES_CBC_Encrypt(data_block, cipher_block_ans, keys, init, true, DES_BLOCK_COUNT); 00138 DES_CBC_Decrypt(cipher_block_ans, block_ans, keys, init, true, DES_BLOCK_COUNT); 00139 00140 /* Check if decrypted answer is equal to plaintext. */ 00141 for (uint8_t i = 1; i < (DES_BLOCK_LENGTH * DES_BLOCK_COUNT); i++ ){ 00142 if (data_block[i] != block_ans[i]){ 00143 success = false; 00144 break; 00145 } 00146 } 00147 } 00148 00149 if (success){ 00150 while (true){ 00151 /* If the example ends up here everything is ok. */ 00152 nop(); 00153 } 00154 }else{ 00155 while (true){ 00156 /* If the example ends up here something is wrong. */ 00157 nop(); 00158 } 00159 } 00160 }

| uint8_t block_ans[DES_BLOCK_LENGTH *DES_BLOCK_COUNT] |
Variable used to store decrypted plaintext from DES Cipher Block Chaining.
Definition at line 96 of file DES_example.c.
Referenced by main().
| uint8_t cipher_block_ans[DES_BLOCK_LENGTH *DES_BLOCK_COUNT] |
Variable used to store ciphertext from DES Cipher Block Chaining.
Definition at line 87 of file DES_example.c.
Referenced by main().
| uint8_t data[DES_BLOCK_LENGTH] = {0xAB, 0xBA, 0x00, 0xBE, 0xEF, 0x00, 0xDE, 0xAD} |
Plaintext block used by DES and 3DES.
Definition at line 63 of file DES_example.c.
Referenced by main().
| uint8_t data_block[DES_BLOCK_LENGTH *DES_BLOCK_COUNT] |
Initial value:
{0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08,
0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F, 0x00,
0xAB, 0xBA, 0x00, 0x00, 0xDE, 0xAD, 0x00, 0x00}
Definition at line 81 of file DES_example.c.
Referenced by main().
| uint8_t init[DES_BLOCK_LENGTH] = {0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88} |
Initial vector used during DES Cipher Block Chaining.
Definition at line 78 of file DES_example.c.
Referenced by main().
| uint8_t keys[DES_BLOCK_LENGTH *DES_BLOCK_COUNT] |
Initial value:
{0x94, 0x74, 0xB8, 0xE8, 0xC7, 0x3B, 0xCA, 0x7D,
0x28, 0x34, 0x76, 0xAB, 0x38, 0xCF, 0x37, 0xC2,
0xFE, 0x98, 0x6C, 0x38, 0x23, 0xFC, 0x2D, 0x23}
Definition at line 72 of file DES_example.c.
Referenced by main().
| uint8_t single_ans[DES_BLOCK_LENGTH] |
Variable used to store DES and tripleDES results.
Definition at line 66 of file DES_example.c.
Referenced by main().
Generated on Wed Apr 23 08:31:42 2008 for AVR1317 Using the XMEGA bulit in DES accelerator by 1.5.5
|