| Xmega Application Note | |||||
Consider the following example:
/*! Invisible class because of truncation */ class Invisible { }; /*! Truncated class, inheritance relation is hidden */ class Truncated : public Invisible { }; /* Class not documented with doxygen comments */ class Undocumented { }; /*! Class that is inherited using public inheritance */ class PublicBase : public Truncated { }; /*! A template class */ template<class T> class Templ { }; /*! Class that is inherited using protected inheritance */ class ProtectedBase { }; /*! Class that is inherited using private inheritance */ class PrivateBase { }; /*! Class that is used by the Inherited class */ class Used { }; /*! Super class that inherits a number of other classes */ class Inherited : public PublicBase, protected ProtectedBase, private PrivateBase, public Undocumented, public Templ<int> { private: Used *m_usedClass; };
MAX_DOT_GRAPH_HEIGHT tag in the configuration file is set to 240 this will result in the following graph:
The boxes in the above graph have the following meaning:
Generated on Wed Apr 23 07:45:46 2008 for AVR1306 Using the XMEGA Timer/Counter by 1.5.5
|