| Xmega Application Note | |||||
This file contains an example application that demonstrates the Timer/ Counter driver.
Copyright (c) 2008, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file TC_example.c.
#include "avr_compiler.h"
#include "TC_driver.h"

Go to the source code of this file.
Defines | |
| #define | CPU_PRESCALER 1 |
| #define | F_CPU 2000000UL |
Functions | |
| void | Example1 (void) |
| This example shows how to configure TCC0 for basic timer operation. | |
| void | Example2 (void) |
| This function shows how to use the Input Capture functionality. | |
| void | Example3 (void) |
| This example shows how to configure TCC0 for measurement of Frequency and Duty cycle of a signal applied to PC0. | |
| void | Example4 (void) |
| This example shows how to configure TCC0 for pulse width modulation output with varying duty cycle on channel A. | |
| void | Example5 (void) |
| This example shows how to configure TCC0 to count events. | |
| void | Example6 (void) |
| This example shows how to configure Timer/Counter for 32-bit counting with input capture. | |
| ISR (TCC0_OVF_vect) | |
| ISR (TCC0_CCA_vect) | |
| int | main (void) |
| #define CPU_PRESCALER 1 |
| #define F_CPU 2000000UL |
Definition at line 51 of file TC_example.c.
| void Example1 | ( | void | ) |
This example shows how to configure TCC0 for basic timer operation.
This function implements example 1, "Basic Timer/Counter Operation" from the "Getting Started" section of application note AVR1306.
Definition at line 86 of file TC_example.c.
References TC0_ConfigClockSource(), and TC_SetPeriod.
Referenced by main().
00087 { 00088 /* Set period/TOP value. */ 00089 TC_SetPeriod( &TCC0, 0x1000 ); 00090 00091 /* Select clock source. */ 00092 TC0_ConfigClockSource( &TCC0, TC_CLKSEL_DIV1_gc ); 00093 00094 do { 00095 /* Wait while the timer counts. */ 00096 } while (1); 00097 }

| void Example2 | ( | void | ) |
This function shows how to use the Input Capture functionality.
This function implements example 2, "Using the Input Capture Functionality" from the "Getting Started" section of application note AVR1306.
Definition at line 106 of file TC_example.c.
References TC0_ConfigClockSource(), TC0_ConfigInputCapture(), TC0_EnableCCChannels(), TC_GetCaptureA, and TC_GetCCAFlag.
00107 { 00108 uint16_t inputCaptureTime; 00109 00110 /* Configure PC0 for input, triggered on falling edge. */ 00111 PORTC.PIN0CTRL = PORT_ISC_FALLING_gc; 00112 PORTC.DIRCLR = 0x01; 00113 00114 /* Configure Port D for output. */ 00115 PORTD.DIRSET = 0xFF; 00116 00117 /* Select PC0 as input to event channel 2. */ 00118 EVSYS.CH2MUX = EVSYS_CHMUX_PORTC_PIN0_gc; 00119 00120 /* Configure TCC0 for Input Capture using event channel 2. */ 00121 TC0_ConfigInputCapture( &TCC0, TC_EVSEL_CH2_gc ); 00122 00123 /* Enable Input Capture channel A. */ 00124 TC0_EnableCCChannels( &TCC0, TC0_CCAEN_bm ); 00125 00126 /* Start timer by selecting a clock source. */ 00127 TC0_ConfigClockSource( &TCC0, TC_CLKSEL_DIV1_gc ); 00128 00129 do { 00130 do { 00131 /* Wait for Input Capture. */ 00132 } while ( TC_GetCCAFlag( &TCC0 ) == 0 ); 00133 00134 inputCaptureTime = TC_GetCaptureA( &TCC0 ); 00135 PORTD.OUT = (uint8_t) (inputCaptureTime >> 8); 00136 } while (1); 00137 }

| void Example3 | ( | void | ) |
This example shows how to configure TCC0 for measurement of Frequency and Duty cycle of a signal applied to PC0.
This function implements example 3, "Using Input Capture to Calculate Frequency and Duty Cycle of a Signal" from the "Getting Started" section of application note AVR1306.
Definition at line 147 of file TC_example.c.
References TC0_ConfigClockSource(), TC0_ConfigInputCapture(), TC0_EnableCCChannels(), TC0_SetCCAIntLevel(), and TC_SetPeriod.
00148 { 00149 /* Configure PC0 for input, triggered on both edges. */ 00150 PORTC.PIN0CTRL = PORT_ISC_BOTHEDGES_gc; 00151 PORTC.DIRCLR = 0x01; 00152 00153 /* Select PC0 as input to event channel 0. */ 00154 EVSYS.CH0MUX = EVSYS_CHMUX_PORTC_PIN0_gc; 00155 00156 /* Configure TCC0 for Input Capture using event channel 2. */ 00157 TC0_ConfigInputCapture( &TCC0, TC_EVSEL_CH0_gc ); 00158 00159 /* Enable Input "Capture or Compare" channel A. */ 00160 TC0_EnableCCChannels( &TCC0, TC0_CCAEN_bm ); 00161 00162 /* Clear MSB of PER[H:L] to allow for propagation of edge polarity. */ 00163 TC_SetPeriod( &TCC0, 0x7FFF ); 00164 00165 /* Start timer by selecting a clock source. */ 00166 TC0_ConfigClockSource( &TCC0, TC_CLKSEL_DIV1_gc ); 00167 00168 /* Enable CCA interrupt. */ 00169 TC0_SetCCAIntLevel( &TCC0, TC_CCAINTLVL_LO_gc ); 00170 PMIC.CTRL |= PMIC_LOLVLEN_bm; 00171 00172 sei(); 00173 00174 do { 00175 /* Wait while interrupt measure Frequency and Duty cycle. */ 00176 } while (1); 00177 }

| void Example4 | ( | void | ) |
This example shows how to configure TCC0 for pulse width modulation output with varying duty cycle on channel A.
This function implements example 4, "Using a Timer/Counter for PWM Generation" from the "Getting Started" section of application note AVR1306.
Definition at line 210 of file TC_example.c.
References TC0_ConfigClockSource(), TC0_ConfigWGM(), TC0_EnableCCChannels(), TC_ClearOverflowFlag, TC_GetOverflowFlag, TC_SetCompareA, and TC_SetPeriod.
00211 { 00212 uint16_t compareValue = 0x0000; 00213 00214 /* Enable output on PC0. */ 00215 PORTC.DIR = 0x01; 00216 00217 /* Set the TC period. */ 00218 TC_SetPeriod( &TCC0, 0xFFFF ); 00219 00220 /* Configure the TC for single slope mode. */ 00221 TC0_ConfigWGM( &TCC0, TC_WGMODE_SS_gc ); 00222 00223 /* Enable Compare channel A. */ 00224 TC0_EnableCCChannels( &TCC0, TC0_CCAEN_bm ); 00225 00226 /* Start timer by selecting a clock source. */ 00227 TC0_ConfigClockSource( &TCC0, TC_CLKSEL_DIV1_gc ); 00228 00229 do { 00230 /* Calculate new compare value. */ 00231 compareValue += 32; 00232 00233 /* Output new compare value. */ 00234 TC_SetCompareA( &TCC0, compareValue ); 00235 00236 do { 00237 /* Wait for the new compare value to be latched 00238 * from CCABUF[H:L] to CCA[H:L]. This happens at 00239 * TC overflow (UPDATE ). 00240 */ 00241 } while( TC_GetOverflowFlag( &TCC0 ) == 0 ); 00242 00243 /* Clear overflow flag. */ 00244 TC_ClearOverflowFlag( &TCC0 ); 00245 00246 } while (1); 00247 }

| void Example5 | ( | void | ) |
This example shows how to configure TCC0 to count events.
This function implements example 5, "Event Counting" from the "Getting Started" section of application note AVR1306.
This example shows how to configure TCC0 to count the number of switch presses for a switch connected to PC0. PD0 is used as output and will be toggled for every 5 switch presses on PC0.
Definition at line 259 of file TC_example.c.
References TC0_ConfigClockSource(), TC0_SetOverflowIntLevel(), and TC_SetPeriod.
00260 { 00261 /* Configure PORTC as input on PC0, sense on falling edge. */ 00262 PORTC.PIN0CTRL = PORT_ISC_RISING_gc; 00263 PORTC.DIRCLR = 0x01; 00264 00265 /* Configure PORTD as output on PD0. */ 00266 PORTD.DIRSET = 0x01; 00267 00268 /* Select PC0 as input to event channel 0, enable filtering. */ 00269 EVSYS.CH0MUX = EVSYS_CHMUX_PORTC_PIN0_gc; 00270 EVSYS.CH0CTRL = EVSYS_DIGFILT_8SAMPLES_gc; 00271 00272 /* Set period ( TOP value ). */ 00273 TC_SetPeriod( &TCC0, 4 ); 00274 00275 /* Enable overflow interrupt at low level */ 00276 TC0_SetOverflowIntLevel( &TCC0, TC_OVFINTLVL_LO_gc ); 00277 PMIC.CTRL |= PMIC_LOLVLEN_bm; 00278 00279 sei(); 00280 00281 /* Start Timer/Counter. */ 00282 TC0_ConfigClockSource( &TCC0, TC_CLKSEL_EVCH0_gc ); 00283 00284 do { 00285 /* Wait for user input. */ 00286 } while (1); 00287 }

| void Example6 | ( | void | ) |
This example shows how to configure Timer/Counter for 32-bit counting with input capture.
This function implements example 6, "Setting up a 32-bit Timer/Counter With Input Capture" from the "Getting Started" section of application note AVR1306.
This example shows how to configure TCC0 and TCC1 for 32-bit Timer/Counter operation with input capture. The overflow from TCC0 is routed through event channel 0 to TCC1. An input capture is triggered by a falling edge on PC0, routed through event channel 1.
Definition at line 309 of file TC_example.c.
References TC0_ConfigClockSource(), TC0_ConfigInputCapture(), TC0_EnableCCChannels(), TC1_ConfigClockSource(), TC1_ConfigInputCapture(), TC1_EnableCCChannels(), TC_EnableEventDelay, TC_GetCaptureA, and TC_GetCCAFlag.
00310 { 00311 uint32_t inputCaptureTime; 00312 00313 /* Configure PC0 for input, triggered on falling edge. */ 00314 PORTC.PIN0CTRL = PORT_ISC_FALLING_gc; 00315 PORTC.DIRCLR = 0x01; 00316 00317 /* Configure PORTD as output. */ 00318 PORTD.DIRSET = 0xFF; 00319 00320 /* Use PC0 as multiplexer input for event channel 1. */ 00321 EVSYS.CH1MUX = EVSYS_CHMUX_PORTC_PIN0_gc; 00322 00323 /* Use TCC0 overflow as input for event channel 0. */ 00324 EVSYS.CH0MUX = EVSYS_CHMUX_TCC0_OVF_gc; 00325 00326 /* Configure TCC0 and TCC1 for input capture with event channel 1 as 00327 * trigger source. 00328 */ 00329 TC0_ConfigInputCapture( &TCC0, TC_EVSEL_CH1_gc ); 00330 TC1_ConfigInputCapture( &TCC1, TC_EVSEL_CH1_gc ); 00331 00332 /* Enable event delay on TCC1. */ 00333 TC_EnableEventDelay( &TCC1 ); 00334 00335 /* Enable input capture channel A on TCC0 and TCC1 */ 00336 TC0_EnableCCChannels( &TCC0, TC0_CCAEN_bm ); 00337 TC1_EnableCCChannels( &TCC1, TC1_CCAEN_bm ); 00338 00339 /* Use event channel 0 as clock source for TCC1. */ 00340 TC1_ConfigClockSource( &TCC1, TC_CLKSEL_EVCH0_gc ); 00341 00342 /* Select system clock as TCC0 clock source. */ 00343 TC0_ConfigClockSource( &TCC0, TC_CLKSEL_DIV1_gc ); 00344 00345 do { 00346 do { 00347 /* Wait for Input Capture. */ 00348 } while ( TC_GetCCAFlag( &TCC0 ) == 0 ); 00349 00350 uint16_t highWord = TC_GetCaptureA( &TCC1 ); 00351 uint16_t lowWord = TC_GetCaptureA( &TCC0 ); 00352 inputCaptureTime = ( (uint32_t) highWord << 16 ) | lowWord; 00353 00354 PORTD.OUT = (uint8_t) (inputCaptureTime >> 24); 00355 00356 } while (1); 00357 00358 }

| ISR | ( | TCC0_OVF_vect | ) |
| ISR | ( | TCC0_CCA_vect | ) |
Definition at line 180 of file TC_example.c.
References CPU_PRESCALER, F_CPU, TC_GetCaptureA, and TC_Restart.
00181 { 00182 static uint32_t frequency; 00183 static uint32_t dutyCycle; 00184 static uint16_t totalPeriod; 00185 static uint16_t highPeriod; 00186 00187 uint16_t thisCapture = TC_GetCaptureA( &TCC0 ); 00188 00189 /* Save total period based on rising edge and reset counter. */ 00190 if ( thisCapture & 0x8000 ) { 00191 totalPeriod = thisCapture & 0x7FFF; 00192 TC_Restart( &TCC0 ); 00193 } 00194 /* Calculate duty cycle based on time from reset and falling edge. */ 00195 else { 00196 highPeriod = thisCapture; 00197 } 00198 00199 dutyCycle = ( ( ( highPeriod * 100 ) / totalPeriod ) + dutyCycle ) / 2; 00200 frequency = ( ( ( F_CPU / CPU_PRESCALER ) / totalPeriod ) + frequency ) / 2; 00201 }
| int main | ( | void | ) |
Definition at line 70 of file TC_example.c.
References Example1().
00071 { 00072 Example1(); 00073 /*Example2();*/ 00074 /*Example3();*/ 00075 /*Example4();*/ 00076 /*Example5();*/ 00077 /*Example6();*/ 00078 }

Generated on Wed Apr 23 07:45:46 2008 for AVR1306 Using the XMEGA Timer/Counter by 1.5.5
|