| Xmega Application Note | |||||
00001 /* This file has been prepared for Doxygen automatic documentation generation.*/ 00055 #include "ac_driver.h" 00056 00057 /* The Analog comparator used in the example.*/ 00058 #define AC ACA 00059 00060 int main(void) 00061 { 00062 /* Enable Analog comparator submodule 0. */ 00063 AC_Enable(&AC, ANALOG_COMPARATOR0, false); 00064 00065 /* By defalut the Analog comparators interupt flag triggers on changes on 00066 * both edges. If another trigger setting (INTMODE) is preferd use the 00067 * AC_ConfigInterrupt function to change the settings. */ 00068 00069 /* Set up MUXes to sense pin 0 and 1. */ 00070 AC_ConfigMUX(&AC, ANALOG_COMPARATOR0, AC_MUXPOS_PIN0_gc, AC_MUXNEG_PIN1_gc); 00071 00072 /* Set up AC with a small hysteresis. */ 00073 AC_ConfigHysteresis(&AC, ANALOG_COMPARATOR0, AC_HYSMODE_SMALL_gc); 00074 00075 /* Sense for 4 changes on comparator output. */ 00076 for(uint8_t i=0; i < 4; i++){ 00077 /* Wait for Comparator to change value. */ 00078 AC_WaitForComparator_Blocking(&AC, ANALOG_COMPARATOR0); 00079 } 00080 00081 /* Disable submodule 0. */ 00082 AC_Disable(&ACA, ANALOG_COMPARATOR0); 00083 00084 do{ 00085 /* Stop here. */ 00086 }while(true); 00087 }
Generated on Tue Apr 22 15:13:25 2008 for AVR1302 Using the XMEGA Analog Comparator by 1.5.5
|