| XMEGA Application Note | |||||
#include "avr_compiler.h"
#include "ccpwrite.h"
#include "rtc_driver.h"
#include "sleepmgr.h"
#include "lowpower.h"

Go to the source code of this file.
Defines | |
| #define | F_CPU 2000000 |
| Enable the 32 kHz XTAL oscillator for RTC. (Otherwise, use ULP.). | |
| #define | RTC_PERIOD 5 |
| Configure RTC wakeup period in seconds. (Approximate if ULP is used..). | |
| #define | SLEEP_MODE SLEEPMGR_SAVE |
| #define | USE_RTC |
Functions | |
| ISR (RTC_COMP_vect) | |
| int | main (void) |
| The main RTC example. | |
This file contains an example program which initializes the XMEGA to the least power consuming state, and puts the device to sleep.
By default, the XMEGA is put in POWER-SAVE mode, and wakes up every five seconds. The device stays in ACTIVE mode for 0.5 sec before going back to sleep. This gives a duty cycle of 10%.
The interval timing is done with the RTC and ULP as default clock source, which should result in approximately 1 ľA current consumption.
Copyright (c) 2008, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file xmega_sleep_example.c.
| #define F_CPU 2000000 |
Enable the 32 kHz XTAL oscillator for RTC. (Otherwise, use ULP.).
Define the CPU frequency, for use with delay_us(). (2 MHz is default clock.)
Definition at line 101 of file xmega_sleep_example.c.
| #define RTC_PERIOD 5 |
Configure RTC wakeup period in seconds. (Approximate if ULP is used..).
Definition at line 94 of file xmega_sleep_example.c.
| #define SLEEP_MODE SLEEPMGR_SAVE |
Specify which sleep mode to use.
The default alternatives are:
SLEEPMGR_IDLE - Idle SLEEPMGR_ESTDBY - Extended standby SLEEPMGR_SAVE - Power-save SLEEPMGR_STDBY - Standby SLEEPMGR_DOWN - Power-down
The device cannot wake itself up from Standby or Power-down because the RTC is disabled in these modes.
Definition at line 83 of file xmega_sleep_example.c.
| #define USE_RTC |
Configure if RTC should be used. (Comment out otherwise.)
This wakes the device up at the specified number of seconds.
Definition at line 92 of file xmega_sleep_example.c.
| ISR | ( | RTC_COMP_vect | ) |
| int main | ( | void | ) |
The main RTC example.
This function initializes the XMEGA to the least power consuming state, before initializing the sleep manager and RTC as configured above.
The main loop doesn't do anything but put the device back to the configured sleep mode after a delay of 0.5 second.
Definition at line 112 of file xmega_sleep_example.c.
References CCPWrite(), LOWPOWER_Init(), RTC_Busy, RTC_Initialize(), RTC_PERIOD, RTC_SetCompareIntLevel(), SLEEP_MODE, SLEEPMGR_Init(), SLEEPMGR_Lock(), and SLEEPMGR_Sleep().
00113 { 00114 // Initialize to the least power consuming state. 00115 LOWPOWER_Init(); 00116 00117 // Enable EEPROM and Flash power reduction mode. 00118 CCPWrite(&NVM.CTRLB, NVM_EPRM_bm | NVM_FPRM_bm); 00119 00120 // Initialize the sleep manager, lock a sleep mode if configured. 00121 SLEEPMGR_Init(); 00122 #ifdef SLEEP_MODE 00123 SLEEPMGR_Lock( SLEEP_MODE ); 00124 #endif // SLEEP_MODE 00125 00126 00127 // If use of the RTC as interval timer is configured, set it up. 00128 #ifdef USE_RTC 00129 // Clear bit for RTC in PRR (set by LOWPOWER_Init()). 00130 PR.PRGEN &= ~PR_RTC_bm; 00131 00132 #ifndef RTC_XTAL 00133 // Set internal 32kHz ULP oscillator as clock source for RTC. 00134 CLK.RTCCTRL = CLK_RTCSRC_ULP_gc | CLK_RTCEN_bm; 00135 #else 00136 // Enable external 32 kHz XTAL oscillator in low-power mode. 00137 OSC.XOSCCTRL = OSC_XOSCSEL_32KHz_gc | OSC_X32KLPM_bm; 00138 OSC.CTRL |= OSC_XOSCEN_bm; 00139 00140 // Wait for oscillator to stabilize. 00141 do { } while (!( OSC.STATUS & OSC_XOSCRDY_bm )); 00142 00143 // Set the oscillator as clock source for RTC. 00144 CLK.RTCCTRL = CLK_RTCSRC_TOSC_gc | CLK_RTCEN_bm; 00145 #endif // RTC_XTAL 00146 00147 // Wait until RTC is ready. 00148 do { } while ( RTC_Busy() ); 00149 00150 // Configure RTC wakeup period. 00151 RTC_Initialize( RTC_PERIOD, 0, 0, RTC_PRESCALER_DIV1024_gc ); 00152 00153 // Enable the RTC compare interrupts so that the device can wake up. 00154 RTC_SetCompareIntLevel( RTC_COMPINTLVL_LO_gc ); 00155 PMIC.CTRL |= PMIC_LOLVLEN_bm; 00156 sei(); 00157 #endif // USE_RTC 00158 00159 // Main loop. 00160 do { 00161 /* On wake-up, stay in ACTIVE mode for 0.5 s and then go back to sleep. 00162 * 00163 * In an actual application, you would process events/data here. 00164 */ 00165 delay_us(500000); 00166 00167 // Due to errata, disable Flash power reduction before sleep. 00168 CCPWrite(&NVM.CTRLB, NVM_EPRM_bm); 00169 00170 SLEEPMGR_Sleep(); 00171 00172 // Re-enable EEPROM and Flash power reduction mode after sleep. 00173 CCPWrite(&NVM.CTRLB, NVM_EPRM_bm | NVM_FPRM_bm); 00174 } while (1); 00175 }

Generated on Mon Nov 9 13:44:41 2009 for XMEGA power consumption evaluation code by 1.5.9
|