| XMEGA Application Note | |||||
#include "avr_compiler.h"
#include "ccpwrite.h"
#include "sleepmgr.h"
#include "lowpower.h"
#include "rtc32_driver.h"

Go to the source code of this file.
Defines | |
| #define | F_CPU 2000000 |
| Define the CPU frequency, for use with delay_us(). (2 MHz is default clock.). | |
| #define | RTC_PERIOD 8 |
| Configure RTC wakeup period in seconds. (Approximate if ULP is used..). | |
Functions | |
| ISR (RTC32_COMP_vect) | |
| int | main (void) |
| The main RTC example. | |
Variables | |
| uint8_t | gState = 0 |
| Global variable to keep track of which state the program is in. | |
This file contains a simple program for measuring the current consumption of XMEGA devices in different sleep modes.
The device cycles through ACTIVE, IDLE, POWER-SAVE and POWER-DOWN modes, spending 8 seconds in each mode.
Note that the device will stay in POWER-DOWN.
The interval timing is done with the 32-bit RTC, clocked by the external 32 kHz crystal oscillator.
Copyright (c) 2008, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file xmega_rtc32_power_consumption.c.
| #define F_CPU 2000000 |
Define the CPU frequency, for use with delay_us(). (2 MHz is default clock.).
Definition at line 74 of file xmega_rtc32_power_consumption.c.
| #define RTC_PERIOD 8 |
Configure RTC wakeup period in seconds. (Approximate if ULP is used..).
Definition at line 70 of file xmega_rtc32_power_consumption.c.
| ISR | ( | RTC32_COMP_vect | ) |
RTC compare ISR
This ISR simply updates gState so that the device cycles through the different sleep modes.
Definition at line 136 of file xmega_rtc32_power_consumption.c.
References gState, RTC32_SetCompareIntLevel(), SLEEPMGR_DOWN, SLEEPMGR_IDLE, SLEEPMGR_Init(), SLEEPMGR_Lock(), SLEEPMGR_SAVE, and SLEEPMGR_Unlock().
00137 { 00138 switch(gState) { 00139 // The device starts out in active mode. Go to Idle. 00140 case 0: 00141 SLEEPMGR_Lock( SLEEPMGR_IDLE ); 00142 ++gState; 00143 break; 00144 00145 // Power-save follows after Idle. 00146 case 1: 00147 SLEEPMGR_Unlock( SLEEPMGR_IDLE ); 00148 SLEEPMGR_Lock( SLEEPMGR_SAVE ); 00149 ++gState; 00150 break; 00151 00152 // Power-down follows after Power-save. 00153 case 2: 00154 SLEEPMGR_Unlock( SLEEPMGR_SAVE ); 00155 SLEEPMGR_Lock( SLEEPMGR_DOWN ); 00156 ++gState; 00157 00158 // Disable interrupt to remain in sleep. (RTC32 will keep running.) 00159 RTC32_SetCompareIntLevel( RTC32_COMPINTLVL_OFF_gc ); 00160 break; 00161 00162 // Shouldn't end up here.. Go to Idle. 00163 default: 00164 SLEEPMGR_Init(); 00165 SLEEPMGR_Lock( SLEEPMGR_IDLE ); 00166 gState = 1; 00167 } 00168 }

| int main | ( | void | ) |
The main RTC example.
This function initializes the XMEGA to the least power consuming state, before initializing the sleep manager and RTC.
The function waits for gState to change (due to RTC compare ISR), after which an infinite loop is entered in which the device is put to sleep.
Definition at line 89 of file xmega_rtc32_power_consumption.c.
References CCPWrite(), gState, LOWPOWER_Init(), RTC32_Initialize(), RTC32_Reset(), RTC32_SetCompareIntLevel(), RTC32_ToscEnable(), RTC_PERIOD, SLEEPMGR_Init(), and SLEEPMGR_Sleep().
00090 { 00091 // Initialize device to the least power consuming state. 00092 LOWPOWER_Init(); 00093 00094 // Enable Flash and EEPROM power reduction modes. 00095 CCPWrite(&NVM.CTRLB, NVM_EPRM_bm | NVM_FPRM_bm); 00096 00097 // Initialize the sleep manager. 00098 SLEEPMGR_Init(); 00099 00100 // Clear bit for RTC in PRR (it is set by LOWPOWER_Init()). 00101 PR.PRGEN &= ~PR_RTC_bm; 00102 00103 // Reset the battery backup module. 00104 RTC32_Reset(); 00105 00106 // Configure and enable TOSC, then set up and enable the RTC32 module. 00107 RTC32_ToscEnable( false ); 00108 RTC32_Initialize( RTC_PERIOD, 0, RTC_PERIOD-1 ); 00109 00110 // Enable RTC compare interrupts. 00111 RTC32_SetCompareIntLevel( RTC32_COMPINTLVL_LO_gc ); 00112 PMIC.CTRL |= PMIC_LOLVLEN_bm; 00113 sei(); 00114 00115 // The device should first spend time in ACTIVE, so wait for 00116 // the RTC compare ISR to change the state. 00117 do { } while(gState == 0); 00118 00119 // Disable Flash power reduction mode due to errata. 00120 // (The device will spend most of its time in sleep from now on, so we 00121 // won't bother clearing/setting FPRM before and after sleep.) 00122 CCPWrite(&NVM.CTRLB, NVM_EPRM_bm); 00123 00124 // Go to sleep. The RTC compare ISR configures the sleep modes. 00125 do { 00126 SLEEPMGR_Sleep(); 00127 } while (1); 00128 }

| uint8_t gState = 0 |
Global variable to keep track of which state the program is in.
Definition at line 79 of file xmega_rtc32_power_consumption.c.
Generated on Mon Nov 9 13:44:39 2009 for XMEGA power consumption evaluation code by 1.5.9
|