Readme File for Code Example:
		Achieving Higher ADC Resolution Using Oversampling 
           	    ----------------------------------------

This file contains the following sections:
1. Code Example Description
2. Folder Contents
3. Suggested Development Resources
4. Reconfiguring the project for a different dsPIC33F device
5. Revision History


1. Code Example Description:
----------------------------

In this example, ADC is configured to over-sample (AN5) at 256 KHz rate and the converted data is assembled in a 512-sample buffer. This input data is then filtered using the block FIR filter function from the DSP library. A 101-tap filter is used.
Timer 3 is setup to time-out every 4 microseconds (250 KHz rate). On every Timer3 time-out (every Ts = 4 microsecs), the ADC module will stop sampling and trigger a 10-bit A/D conversion. At that time, the conversion process starts and completes Tc = 12*Tad = 1.2 microsecs later. When the conversion is complete, the module starts sampling again. However, since Timer3 is already on and counting, about (Ts-Tc) secs later Timer3 will expire again and trigger the next conversion. The DMA is configured in continuous, ping pong mode, such that after the DMA channel has read 480 samples into a buffer (BufferA/BufferB) a DMA interrupt is generated. These samples are filtered by a function call in the main function while the DMA controller starts filling new ADC samples into buffer (BufferB/BufferA). Thus the two buffers are alternately filled and processed in an infinite loop.
The ADC module clock time period is configured as Tad = Tcy*(ADCS+1) = (1/40M)*1 = 100ns nanosecs with ADCS = 3. Hence the conversion time for 10-bit A/D is 12*Tad = 1.2 microsecs.

void initTmr3();
Timer 3 is configured to time-out at 256 KHz rate. 

void initAdc1(void);
ADC module is set-up to convert AIN5 input using CH0 S/H on Timer 3 event in 10-bit mode.

void initDma0(void);
DMA channel0 is confiured in ping-pong mode to move the converted data from ADC to DMA RAM on every sample/convert sequence. 
It generates interrupt after every 512 sample transfer. 

void __attribute__((__interrupt__)) _DMA0Interrupt(void);
DMA interrupt service routine sets flag for FIR filtering on the data buffer.

Code can be run in simulation mode or hardware mode by toggling USE_SIMULATION at the beginning of main.c.
#define USE_SIMULATION 1 => simulation mode. Prints SNR improvement.
#define USE_SIMULATION 0 => hardware mode


2. Folder Contents:
-------------------
This folder contains the following sub-folders:
a. C:\Program Files\Microchip\MPLAB C30\support\gld
        This folder will have the device GLD file, it is used for building the project. 
	This file was provided with the MPLAB C30 toolsuite.

b. C:\Program Files\Microchip\MPLAB C30\support\h
        This folder contains C header files useful in building this
        project. Device register and bit definitions are provided in
        the *.h file that follows the device name. These files were provided
        with the MPLAB C30 toolsuite.

c. C:\Program Files\Microchip\MPLAB C30\lib
        This folder contains library archive files, which are a
        collection of precompiled object files. The file
        named "libpic30-coff.a" contains the C run-time start-up
        library. These file were provided with the
        MPLAB C30 toolsuite.

d. hex
        This folder contains three file types - coff, hex and map.
        These are files generated by the MPLAB C30 toolsuite on build
        operation performed within MPLAB IDE. The *.map file contains
        details on memory allocation for various variables, constants
        and dsPIC instructions specified in the source and library
        code. The *.hex file contains a binary file that may be
        programmed into the dsPIC device. The *.coff file contains
        a binary file that is used by MPLAB IDE for simulation.

e. h
        This folder contains include files for the code example.


f. src
        This folder contains all the C and Assembler source files (*.c,
        *.s) used in demonstrating the described example. This folder
        also contains a sub-folder named "obj" that stores compiled
        object files generated when the project is built.


3. Suggested Development Resources:
-----------------------------------
        a. Explorer16 board with dsPIC33FJ256GP710 controller

4. Reconfiguring the project for a different dsPIC33F device:
-------------------------------------------------------------
The Project/Workspace can be easily reconfigured for any dsPIC33F device.
Please use the following general guidelines:
        a. Change device selection within MPLAB IDE to a dsPIC33F device of
        your choice by using the following menu option:
        MPLAB IDE>>Configure>>Select Device

        b. Provide the correct device linker script and header file for your
        device. Device linker scripts and header files are available in your
        MPLAB C30 installation folder under:
        Device Linker Script-
                YourDrive:>Program Files\Microchip\MPLAB C30\support\gld
        Device C Header file-
                YourDrive:>Program Files\Microchip\MPLAB C30\support\h
        Device ASM Include file-
                YourDrive:>Program Files\Microchip\MPLAB C30\support\inc

        c. Provide the appropriate path to your MPLAB C30 support file locations
        using the menu option:
        MPLAB IDE>>Project>>Build Options>>Project

        d. Chose the development board applicable to your device. Some options
        are provided below:


        e. Re-build the MPLAB project using the menu option:
        MPLAB IDE>>Project>>Build All

        f. Download the hex file into the device and run.

5. Revision History :
---------------------
        12/05/2007 - Initial Release of the Code Example