***********************************************************************
* Software License Agreement                                          *
* The software supplied herewith by Microchip Technology Incorporated *
* (the "Company") is intended and supplied to you, the Company's      *
* customer, for use solely and exclusively on Microchip products.     *
*                                                                     *
* The software is owned by the Company and/or its supplier, and is    *
* protected under applicable copyright laws. All rights are reserved. *
* Any use in violation of the foregoing restrictions may subject the  *
* user to criminal sanctions under applicable laws, as well as to     *
* civil liability for the breach of the terms and conditions of this  *
* license.                                                            *
*                                                                     *
* THIS SOFTWARE IS PROVIDED IN AN "AS IS" CONDITION. NO WARRANTIES,   *
* WHETHER EXPRESS, IMPLIED OR STATU-TORY, INCLUDING, BUT NOT LIMITED  *
* TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A         *
* PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. THE COMPANY SHALL NOT,   *
* IN ANY CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL OR          *
* CONSEQUENTIAL DAMAGES, FOR ANY REASON WHATSOEVER.                   *
*                                                                     *
***********************************************************************

This file contains general design notes for the functions, tasks, state machines, timing,
priority control, communications and command structures of the LumiLED LED driver software.
This file is for the Buck configuration driver.
************************************************************************************************
Software Functions
1.	Generate a PWM output for intensity control
2.	Decode key press
3.	Decode key push
4.	Decode key hold
5.	Intensity control
6.	Mode select
7.	EEPROM reader
8.	Intensity command
9.	Time command
10.	Repeat command
11. 	Goto command
12.	Power up configure
13. 	Power down configure
14.	Battery monitoring
15.	Intensity correction for battery voltage

Task list
Timer task
1.	PWM for intensity control
2.	System Timing

Key task
1.	Decode Key press
2.	Decode key push
3.	Decode key hold

Command task
1.	Power up read and configure
2.	Power down store and shut down
3.	Intensity Control
4.	Mode Select

Auto sequence Task
1.	Intensity command
2.	Time command
3.	Repeat command
4.	Goto command

Eprom Task (handled as macros in the command and Auto Sequence tasks, no state machine created)
1.	Read eeprom
2.	Write eeprom

ADC task
1.	Battery monitoring
2.	Intensity correction

****************************************************************************************************************
Inter-Task Communications

Item	Source		Destination		Communications
1.	Command		Auto Seq		Bright				both for command feedback and flash lite mode
2,	Auto Seq	ADC			Inten_chng			Notifies ADC of change in intensity
3.	Cmd/Tmr		Cmd/Tmr			Timing				for Mode select, 3 second timer start/done 
4.	Key		Command			press, push, hold		intesity and mode select flags
5.	CMD/EEPROM	EEPROM/CMD		System State			Save mode & intensity on pwrdn, retrieve on Pwrup
6.	Command		Auto Seq		Mode				Mode select, 1,2,3,4 or 5.  1 is do nothing
7.	AuSq/EEPROM	EEPROM/AuSq		Commands			given an address, return the command
8.	AuSq/TMR	TMR/AuSq		Time delay			for Time delay command, time, start, done
9.	Auto Seq	ADC			Intensity			in modes 2-5, intensity setting per command
10.	Auto Seq	ADC			Inten_chng			notifies ADC of change in intensity
11.	ADC 		Timer			Final duty cycle		corrected for battery sag


****************************************************************************************************************
System Timing
								skip timer
Timer			1kHz			  1 msec	  1:1
Key			100 Hz or faster	 10 msec	 10:1
Command			100 Hz			 10 msec	 10:1
Auto Sequence		10 Hz +/- 10%		100 msec	100:1
ADC			10 Hz			100 msec	100:1

Minimum Tick = 1 msec

****************************************************************************************************************
System Priorities
System States

Mode/Intensity Select
1.	Key
2.	Command
3.	Timer
4.	ADC

Auto Sequence
1.	Auto sequence
2.	Timer
3.	ADC

Flash Light
1.	Key
2.	Timer
3.	ADC
4.	Command

Power up/down
1.	Command
2.	EEPROM

Auto Sequence only needed in Auto Sequence mode
Key and Timer are optional in power up and down
Command becomes important when key detects activity
ADC needed only when actual intensity output is performed

***************************************************************************************************************

Timer State machine design
Not a true state machine, rather is a timer system with a PWM pulse generator
as part of the execution path.

Timing algorithm

Wait for TMR0 roll over
switch (duty cycle)
{
	case 0%:	output low
			return
			
	case 100%:	output high
			return
			
	case 1-50%:	generate high output pulse
			return
			
	case 50-100%:	generate low output pulse
			return
}

if (key_skip_timer-- == 0)
{
	do_key = true
	key_skip_timer = 10
}

if (cmd_skip_timer-- == 0)
{
	do_cmd = true
	cmd_skip_timer = 5
}

if (auto_skip_timer-- == 0)
{
	do_auto = true
	auto_skip_timer = 100
}

if (adc_skip_timer-- == 0)
{
	do_adc = true
	adc_skip_timer = 100
}

***************************************************************************************************************

Key State machine design
Execution indexed state machine

	State
0	Idle		no key pressed
1	press		key held < 1.5 sec
2	push		key held < 3.0 sec
3	hold		key held > 3.0 sec
4	delay		auto repeat delay for hold
5	default		error state
6	default		error state
7	default		error state

STATE TO STATE TRANSITIONS
From	Conditional		if True		if False	comments
-----------------------------------------------------------------------------------------
Idle	if key press detected	press		Idle		no key

press	if keypress = 0		Idle		press		key stable at open press
press	is time > 1.5 sec	push		press		if held > 1.5 s then push

push	if keypress = 0		Idle		push		key stable at open Push
push 	if time > 3.0 sec	hold		push		if held > 3.0 s then hold

hold	if keypress = 0		Idle		hold		key stable at open hold
hold				delay		----		goto delay for auto repeat

delay	if keypress = 0		Idle		delay		key stable at open delay
delay	if time = 3.0 sec	hold		delay		auto repeat
	
ACTIONS
Idle	none
press	if release send press command
push	if release send push command
hold	send hold command
delay 	delay 3.0 seconds then return to hold

Code segment prior to state variable decoder, monitors the button and debounces
with keypress as an output.
(Algorithm)

	if (key == 0) and (bcounter < 7) then bcounter++
	if (key == 1) and (bcounter > 0) then bcounter--
	if bcounter == 6	then keypress = 1
	if bcounter == 2 	then keypress = 0
	
		
INPUT/OUTPUT
		input			output
Idle		keypress		----
press		keypress		press cmd
push		keypress		push cmd
hold		keypress		hold cmd
delay		keypress		----


***************************************************************************************************************

Command State machine design
Hybrid Execution and Data indexed state machine

	State
0	Incint		Intensity increment mode
1	Decint		Intensity decrement mode
2	Modesel		Mode select mode
3	Display		data indexed state machine for mode number display
Note: no default state needed

STATE TO STATE TRANSITIONS
From	Conditional			if True		if False	comments
-------------------------------------------------------------------------------------------------------------------
Incint	if push command			Decint		Incint		change from inc to dec
Incint	if hold command			Modesel		Incint		change to mode select

Decint	if push command			Incint		Decint		change from dec to inc
Decint	if hold command			Modesel		Decint		change to mode select

Modesel	if keypress = 0			Incint		Modesel		key is released go back to keypress
Modesel	if hold command			Display		Modesel		display next mode number

Display	if display complete		Modesel		Display		display routine completes if started.
	
ACTIONS
Incint
	if (Push == 1) and (old_push == 1) then power off
	if (Push == 1) then old_push = 1
	if (Press == 1) or (Hold == 1) old_push = 0
	clear Push

	if (Press == 1) and (intensity < max) then intensity++ and store in eeprom
	clear Press
Decint
	if (Push == 1) and (old_push == 1) then power off
	if (Push == 1) then old_push = 1
	if (Press == 1) or (Hold == 1) old_push = 0
	clear Push

	if (Press == 1) and (intensity > 0) then intensity-- and store in eeprom
	clear Press
Modesel
	set asq_hold
	if keypress = 0
		clear asq_hold
		set new_mode flag
	mode++
	if mode = number_of_modes+2
		mode = 1
Display
	flash .5 second off with 1 second gap for mode index 1-5 (i.e. 1 to 5 flashes)


INPUT/OUTPUT
		input					output
Incint		press, push, hold			intensity
Decint		press, push, hold			intensity
Modesel		hold, keypress				Mode
Display		----					intensity

DISPLAY SEQUENCE
counter = 0
pointer = mode * 2

loop
	if counter == 0
		if pointer is odd
			counter = 20
			intensity = 1/2
		else
			counter = 10
			intensity = full
		pointer--
		if pointer == 0
		goto	Modesel_state
	counter--

***************************************************************************************************************
Auto Sequence State machine design
Hybrid Execution and Data indexed state machine

Auto sequence Task		D7	D6	D5	D4-0
1.	Intensity command	0	0	Intensity
2.	Time command		0	1	Time delay
3.	Repeat command		1	0	repeat count
	Return at the end	1	0	0	0000
4.	Goto command		1	1	destination
	shut down command	1	1	0	0000

if asq_hold is true, this state machine is idle
if new_mode, state is reset to asq_change
	
sequence numbers 1-63, zero causes shut down

	State
0	Decode		Fetch a command and decode it
1	Set_Intens	Intensity set command
2	Time_Delay	Time Delay command
3	Jump		goto different step number
4	Repeat		repeat section command
5	Delay		used for time command
6	ASQ_change	auto sequence, sequence change.  Reset of system for next sequence
7	flash_lite	no sequence, continuous mode only

STATE TO STATE TRANSITIONS
From		Conditional						if True		if False
Decode		if command = Intensity					Set_Intens	Decode
Decode		if command = Time					Time_delay	Decode
Decode		if command = Jump					Jump		Decode
Decode		if command = Repeat					Repeat		Decode
Set_Itens	none							Decode
Time_Delay	none							Delay
Jump		none							Decode
Repeat		none							Decode
Delay		if timer == 0						Decode		Delay
ASQ_change	mode = 1						flash_lite	Decode

ACTIONS
Decode		
		get command(addr_next)
		addr_next++
		decode command & 0xC0
		ASQ_data = command & 0x3F
Set_Intens
		intensity = ASQ_data
		set int_chng
Time_Delay
		Timer = ASQ_data
Jump
		addr_next = ASQ_data
Repeat
		addr_next++
		if ASQ_data == 0			; indicates a return to a repeat
			pop ret_addr
			pop counter			; retrieve counter and return address
			counter--			; count this pass
			if counter == 0
				break (return)
			else
				push counter
				push ret_addr
				addr_next = ret_addr			
		else					; not a return
			push ASQ_data
			push addr_next
Delay
		Decrement timer
ASQ_change
		reset repeat stack
		clear new_mode flag
		if mode > 1
			addr_next = eeprom(start,mode)
flash_lite
		intensity = eeprom(EE_intensity)
		set int_chng

***************************************************************************************************************

ADC State machine design
Execution indexed state machine

	State
0	Idle		wait state
1	Convert		do battery voltage conversion
2	Calculate	correct intensity for battery voltage
3	LowBattery	shut down state


STATE TO STATE TRANSITIONS
From	Conditional					if True		if False	comments
-------------------------------------------------------------------------------------------------------------------
Idle		if intensity change			Calculate	Idle		waiting
Idle		if convert timer timeout		Convert		Idle
Idle		if intensity change			Calculate	Idle

Convert		none					Calculate

Calculate	none					Idle

LowBattery	shutdown

	
ACTIONS
Idle		none
Convert		set PWM output high and convert battery voltage
Calculate	using ADC of battery convert intensity to duty cycle
LowBattery	shutdown

INPUT/OUTPUT
		input					output
Idle		ADC_skip_timer, Intensity_change	none
Convert		ADC, dutycycle				ADRESH
Calculate	Intensity, ADRESH			dutycycle
LowBattery	none					none

Math functions

DATA For Buck system
VDC	ADC	Max PWM	CF	
4.0	2E	.337	100%
4.5	29	.385	91%
5.0	25	.435	80%
5.5	21	.483	72%
6.0	1E	.535	65%

Maximum intensity @ 350 mV

Conversion factor = (ADC*6 - 0B)
Duty cycle    	  = Scaling value * Intensity * 2 / 256


***************************************************************************************************************

Error recovery handler

Error		State machine	Reason for error	Response

pwm_err		Timer routine	PWM value to large	reset dutycycle to 7F
adc_err		ADC routine	state variable wrong	reset to idle state
cmd_err		Command		state variable wrong	reset to idle state
asq_err		Autosequence	state variable wrong	reset to change state
key_err		Key		default state reached	reset to idle state