# README	General information
* Unified Bootloader Host Application 
- Used with the MCC Bootloader Generated Software Library for 8-bit or 16-bit MCU devices, or the 32-bit AN1388 bootloader.
- The graphical front-end of the 8-bit, 16-bit and 32-bit Bootloader project.

# Support
Email: MCC_Support@microchip.com
This application requires the Java 1.8 runtime.
For the required Java FX support, and an alternative source to the legacy Java installer can be found here:
Azul Zulu Community OpenJDK with OpenJFX is recommended; OpenJFX is required for use with UBHA.
https://www.azul.com/downloads/zulu-community/?&version=java-8-lts&package=jdk-fx 

Ensure to select the appropriate operating system, and architecture (32/64 bit).
Additional info: https://www.azul.com/products/zulu-enterprise/jdk-comparison-matrix/

Users of Microchip products can receive assistance through several channels:

 - Distributor or Representative
 - Local Sales Office
 - Field Application Engineer (FAE)
 - Technical Support

Customers should contact their distributor, representative or Field Application Engineer (FAE) for support.
Local sales offices are also available to help customers.
A listing of sales offices and locations may be found on the [Microchip web site][3].

Technical support is available through the [Microchip web site][4].

# CHANGELOG	A detailed changelog, intended for programmers
v 0.1.9:	Added readme, added logger, added checksum support to PIC32; added handling for record type 0x05 (currently ignored)
v 0.1.10:	Internal release
v 0.1.11:	Internal release
v 0.1.14:	Added PIC32 CRC bytes used at end of packets. Added Erase feature to USB PIC32 command chain. Extended Timeouts added support for 24-bit packet length.
v 0.1.15:	Fixed bug in PIC16 erase being half expected length during command chain. Added support for larger PIC18 device checksum commands, appending over previous Access Key bytes.
v 1.0.0:	Release version to support PIC24 family of devices. Added beta support for AVR devices.
v 1.15.0:   Release version to support dsPIC33 family of devices. Release support for AVR devices.
v 1.15.1:   Fixed bugs to support PIC-IOT WG Development Board, phantom byte for degenerate blocks and restrict data packet size to MAX_PACKET_SIZE - HEADER_SIZE.
v 1.16.0:   AVR code protocol modified to handle large future devices.
v 1.16.1:   Updated HID4JAVA library used for USB communication. Updates to AVR support to support MCC generated code. Extended PIC32 timeout(s) to 20s (from 8) UDP, USB
v 1.16.2:   32-bit devices no longer wait for responds from Reset Command. Bug fixes for 16-bit support: 1) Self Verify issue with larger parts with 2) no report, 3) End Address corruption on read properties, 4) Exception thrown on UART disconnect.
v 1.16.3:   Corrects an issue with 16-bit devices where flash data was unable to be written if located at the end of the last flash page.
v 1.17.0:   Add CAN and CAN-FD support for PIC24/dsPIC devices.  Expand console logging capability for PIC24/dsPIC devices.
v 1.17.1:   Improved console logging messages. Added provision to package the dependencies as a hotfix.
v 1.18.0:   Add I2C support for PIC24/dsPIC devices. Added support for select PIC18F Q device families (Q40, Q41, Q43, Q83, Q84).
v 1.19.0:   Add LIN support for PIC24/dsPIC devices. Fix issue causing readback errors when only a partial instruction worth of data is specified in the .hex file.
v 1.19.1:   Fix CAN DLL issue with latest USB drivers
v 1.19.2:   Fix MCP2221 DLL issue with latest drivers

# NEWS	A basic changelog, intended for users
-Incremented version information; see Changelog
-Added readme file on release of version: 0.1.14
-Added Checksum support for PIC32
-Bug fixes, Added Release Notes v 0.1.15 along with readme file. Added support for up to 32-bit checksum value calculation.
-Added Synch Byte expectation to AVR packet support.
-Fixed Typo in Help-->About text which indicated incorrect Utility version
-Added logger support requires launching from command prompt with below text:
* -Djava.util.logging.config.file="C:\<DirectoryLocation>"
- Bugfix for 16-bit flash write.

# Known Issues
- When using a version of java greater than v1.8.0_251, selecting a UART COM port and selecting "Apply" causes the Unified Bootloader Host Application to crash. In order to avoid this please ensure to use
a version of java at or below version 1.8.0_251. 
- The warning 'Application Offset exist between ROWS/PAGE boundaries' might be shown incorrectly, even though the application offset is at the start of a page. Please make sure that the application start adress is at the beginning of a page by referring to the device datasheet.

# Debug Log
The UBHA supports the ability to view Debug Logger message through use of the packaged logging.properties file.
i.e.: To Launch from Command Prompt
>java -Djava.util.logging.config.file="<Drive: e.g. C>:\<MyDirectory>\<UnifiedHost-version>\logging.properties" -jar UnifiedHost-<version>.jar

# INSTALL	Installation instructions
Installation of Java JRE

# COPYING / LICENSE	Copyright and licensing information
See LICENSE.txt for licensing information.