MEGA-1284P Xplained Example Application
Functions | Variables

init.c File Reference

Initialization file used to init all I/O modules used in the example. More...

#include "init.h"

Functions

void io_init_terminal_mode (void)
 Function to setup IO for terminal mode.
void io_init_demo_mode (void)
 Function to setup IO for demo mode.
void power_reduction_enable (void)
 Function to reduce power consumption.
void usart1_init (void)
 Function to setup USART1.
void adc_init (void)
 Function to setup ADC.
void timer1_lightdemo_init (void)
 Function to setup timer1 for light sensor demo.
void stop_timer1_lightdemo (void)
 Function to stop timer1 used in the light sensor demo.
void timer1_init (void)
 Function to setup timer1 as a time base for the touch lib.
void qt_set_parameters (void)
 Function to set values for touch sensing.
void touch_init (void)
 Function to setup touch button.

Variables

TOUCH_DATA_T SNS_array [2][2]
TOUCH_DATA_T SNSK_array [2][2]

Detailed Description

Initialization file used to init all I/O modules used in the example.

Copyright (C) 2011 Atmel Corporation. All rights reserved.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines