/*******************************************************************************
 * (c) Copyright 2016-2017 Microsemi SoC Products Group. All rights reserved.
 *
 * This simple example demonstrates how to use the CoreUARTapb driver and
 * CoreGPIO driver. This example application prints Hello World! on Serial
 * Terminal program and blinks LEDs on PolarFire Evaluation Kit.
 *
 */
#include <stdlib.h>
//#include "riscv_hal.h"
#include "miv_rv32_hal.h"
#include "core_uart_apb.h"
#include "core_gpio.h"
#include "hw_platform.h"


#include "hw_reg_access.h"
//#include "core_spi.h"
//#include "mt25ql01gbbb.h"

#if 0

#define BUFFER_A_SIZE   512

/* Manufacture and device IDs for Micron MT25QL01GBBB SPI Flash. */
#define FLASH_MANUFACTURER_ID   (uint8_t)0x20
#define FLASH_DEVICE_ID         (uint8_t)0xBB

/*
 * Static global variables
 */
static uint8_t g_flash_wr_buf[BUFFER_A_SIZE];
static uint8_t g_flash_rd_buf[BUFFER_A_SIZE];

/* Local Function. */
static uint8_t verify_write(uint8_t* write_buff, uint8_t* read_buff, uint16_t size);

/***************************************************************************//**
 * Read the date from SPI FLASH and compare the same with write buffer.
 */
static uint8_t verify_write(uint8_t* write_buff, uint8_t* read_buff, uint16_t size)
{
	uint8_t error = 0;
	uint16_t index = 0;

	while(size != 0)
	{
		if(write_buff[index] != read_buff[index])
		{
			error = 1;
			break;
		}
		index++;
		size--;
	}

	return error;
}

#endif


/*
 * Delay loop down counter load value.
 */
#define DELAY_LOAD_VALUE     0x00080000
#define DELAY_LOAD_UART_VALUE     0x80000

/******************************************************************************
 * Instruction message. This message will be transmitted over the UART to
 * HyperTerminal when the program starts.
 *****************************************************************************/

uint8_t testmsg[] = {"\r\n\r\nHello World!\0"};
uint8_t testmsgddr[] = {"\r\n\r\nApplication is running from DDR.\n\rThe variable address stored in DDR memory is 0x"};
/*-----------------------------------------------------------------------------
 * UART instance data.
 */
UART_instance_t g_uart;

/*-----------------------------------------------------------------------------
 * GPIO instance data.
 */
gpio_instance_t g_gpio_out;

void delay()
{
	volatile uint32_t count = 1000000;
	while(count)
	{
		count--;
	}
}
/*-----------------------------------------------------------------------------
 * main
 */
int main()
{
	volatile uint32_t delay_count = 0,delay_count_uart=0;
	uint32_t temp =0;
	uint8_t buffer[10];

#if 1
	/**************************************************************************
	 * Initialize the CoreGPIO driver with the base address of the CoreGPIO
	 * instance to use and the initial state of the outputs.
	 *************************************************************************/
	//GPIO_init(&g_gpio_out, COREGPIO_BASE_ADDR, GPIO_APB_32_BITS_BUS);

	/**************************************************************************
	 * Configure the GPIOs.
	 *************************************************************************/
//	GPIO_config( &g_gpio_out, GPIO_0, GPIO_OUTPUT_MODE );
//	GPIO_config( &g_gpio_out, GPIO_1, GPIO_OUTPUT_MODE );
//	GPIO_config( &g_gpio_out, GPIO_2, GPIO_OUTPUT_MODE );
//	GPIO_config( &g_gpio_out, GPIO_3, GPIO_OUTPUT_MODE );

	/**************************************************************************
	 * Set the GPIO outputs.
	 *************************************************************************/
	GPIO_set_output( &g_gpio_out, GPIO_0,1 );
	GPIO_set_output( &g_gpio_out, GPIO_1,0 );
	GPIO_set_output( &g_gpio_out, GPIO_2,1 );
	GPIO_set_output( &g_gpio_out, GPIO_3,0 );


	/**************************************************************************
	 * Initialize CoreUARTapb with its base address, baud value, and line
	 * configuration.
	 *************************************************************************/
	UART_init(&g_uart,
			COREUARTAPB0_BASE_ADDR,
			BAUD_VALUE_115200,
			(DATA_8_BITS | NO_PARITY));

	/**************************************************************************
	 * Send the instructions message.
	 *************************************************************************/
	UART_polled_tx_string(&g_uart, (const uint8_t *)&testmsg);



#endif
#if 1
	/*
	 * Set initial delay used to blink the LED.
	 */
	delay_count = DELAY_LOAD_VALUE;
	delay_count_uart = DELAY_LOAD_UART_VALUE;
	/*
	 * Infinite loop.
	 */
	for(;;)
	{
		uint32_t gpio_pattern;
		/*
		 * Decrement delay counter.
		 */
		--delay_count;
		--delay_count_uart;

		/*
		 * Check if delay expired.
		 *
		 */
		if ( delay_count_uart <= 0 )
		{
			/*
			 * Reload delay counter.
			 */
			delay_count_uart = DELAY_LOAD_UART_VALUE;

			UART_polled_tx_string(&g_uart, (const uint8_t *)&testmsgddr);
            itoa((uint32_t)&temp,buffer,16);
            UART_polled_tx_string(&g_uart, buffer);
		}
		if ( delay_count <= 0 )
		{
			/*
			 * Reload delay counter.
			 */
			delay_count = DELAY_LOAD_VALUE;

			/*
			 * Toggle GPIO output pattern by doing an exclusive OR of all
			 * pattern bits with ones.
			 */
			gpio_pattern = GPIO_get_outputs( &g_gpio_out );
			gpio_pattern ^= 0x0000000F;
			GPIO_set_outputs( &g_gpio_out, gpio_pattern );

		}
	}

#endif

	return 0;

}