/*******************************************************************************
 * (c) Copyright 2008-2013 Microsemi SoC Products Group.  All rights reserved.
 * 
 * SmartFusion2 microcontroller subsystem SPI bare metal software driver
 * implementation.
 *
 * SVN $Revision: 6227 $
 * SVN $Date: 2014-03-15 12:04:24 +0000 (Sat, 15 Mar 2014) $
 */
#include "mss_spi.h"
#include "../../CMSIS/mss_assert.h"
#include <string.h>

#ifdef __cplusplus
extern "C" {
#endif 

/***************************************************************************//**
 * Mask of transfer protocol and SPO, SPH bits within control register.
 */
#define PROTOCOL_MODE_MASK  ((uint32_t)0x0300000Cu)

/***************************************************************************//**
 * Mask of theframe count bits within the SPI control register.
 */
#define TXRXDFCOUNT_MASK    ((uint32_t)0x00FFFF00u)
#define TXRXDFCOUNT_SHIFT   ((uint32_t)8u)

/***************************************************************************//**
 * SPI hardware FIFO depth.
 */
#define RX_FIFO_SIZE    4u
#define BIG_FIFO_SIZE   32u

/***************************************************************************//**
 * 
 */
#define RX_IRQ_THRESHOLD    (BIG_FIFO_SIZE / 2u)

/***************************************************************************//**
  Marker used to detect that the configuration has not been selected for a
  specific slave when operating as a master.
 */
#define NOT_CONFIGURED  0xFFFFFFFFu

/***************************************************************************//**
 * CONTROL register bit masks
 */
#define CTRL_ENABLE_MASK    0x00000001u
#define CTRL_MASTER_MASK    0x00000002u

/***************************************************************************//**
  Registers bit masks
 */
/* CONTROL register. */
#define MASTER_MODE_MASK        0x00000002u
#define CTRL_RX_IRQ_EN_MASK     0x00000010u
#define CTRL_TX_IRQ_EN_MASK     0x00000020u
#define CTRL_OVFLOW_IRQ_EN_MASK 0x00000040u
#define CTRL_URUN_IRQ_EN_MASK   0x00000080u
#define CTRL_REG_RESET_MASK     0x80000000u
#define BIGFIFO_MASK            0x20000000u
#define CTRL_CLKMODE_MASK       0x10000000u
#define SPS_MASK                0x04000000u

/* CONTROL2 register */
#define C2_ENABLE_CMD_IRQ_MASK     0x00000010u
#define C2_ENABLE_SSEND_IRQ_MASK   0x00000020u

/* STATUS register */
#define TX_DONE_MASK            0x00000001u
#define RX_DATA_READY_MASK      0x00000002u
#define RX_OVERFLOW_MASK        0x00000004u
#define RX_FIFO_EMPTY_MASK      0x00000040u
#define TX_FIFO_FULL_MASK       0x00000100u
#define TX_FIFO_EMPTY_MASK      0x00000400u

/* MIS register. */
#define TXDONE_IRQ_MASK         0x00000001u
#define RXDONE_IRQ_MASK         0x00000002u
#define RXOVFLOW_IRQ_MASK       0x00000004u
#define TXURUN_IRQ_MASK         0x00000008u
#define CMD_IRQ_MASK            0x00000010u
#define SSEND_IRQ_MASK          0x00000020u

/* COMMAND register */
#define AUTOFILL_MASK           0x00000001u
#define TX_FIFO_RESET_MASK      0x00000008u
#define RX_FIFO_RESET_MASK      0x00000004u

/***************************************************************************//**
  Maximum frame length
 */
#define MAX_FRAME_LENGTH        32u

/***************************************************************************//**
 * SPI instance data structures for SPI0 and SPI1. A pointer to these data
 * structures must be used as first parameter to any of the SPI driver functions
 * to identify the SPI hardware block that will perform the requested operation.
 */
mss_spi_instance_t g_mss_spi0;
mss_spi_instance_t g_mss_spi1;

/***************************************************************************//**
  SPI0 interrupt service routine
 */
#if defined(__GNUC__)
__attribute__((__interrupt__)) void SPI0_IRQHandler(void);
#else
void SPI0_IRQHandler(void);
#endif

/***************************************************************************//**
  SPI1 interrupt service routine
 */
#if defined(__GNUC__)
__attribute__((__interrupt__)) void SPI1_IRQHandler(void);
#else
void SPI1_IRQHandler(void);
#endif

/***************************************************************************//**
  local functions
 */
static void recover_from_rx_overflow(mss_spi_instance_t * this_spi);
static void fill_slave_tx_fifo(mss_spi_instance_t * this_spi);
static void read_slave_rx_fifo(mss_spi_instance_t * this_spi);
static void mss_spi_isr(mss_spi_instance_t * this_spi);

/***************************************************************************//**
 * MSS_SPI_init()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_init
(
    mss_spi_instance_t * this_spi
)
{
    uint16_t slave;
    
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    /*
     * Initialize SPI driver instance data. Relies on the majority
     * of data requiring 0 for initial state so we just need to fill
     * with 0s and finish off with a small number of non zero values.
     */
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    memset(this_spi, 0, sizeof(mss_spi_instance_t));
    
    this_spi->cmd_done = 1u;

    for(slave = 0u; slave < (uint16_t)MSS_SPI_MAX_NB_OF_SLAVES; ++slave)
    {
        this_spi->slaves_cfg[slave].ctrl_reg = NOT_CONFIGURED;
    }

    if(this_spi == &g_mss_spi0)
    {
        this_spi->hw_reg = ((SPI_TypeDef *) SPI0_BASE);
        this_spi->irqn = SPI0_IRQn;

        /* reset SPI0 */
        SYSREG->SOFT_RST_CR |= SYSREG_SPI0_SOFTRESET_MASK;
        /* Clear any previously pended SPI0 interrupt */
        NVIC_ClearPendingIRQ(SPI0_IRQn);
        /* Take SPI0 out of reset. */
        SYSREG->SOFT_RST_CR &= ~SYSREG_SPI0_SOFTRESET_MASK;
    }
    else
    {
        this_spi->hw_reg = ((SPI_TypeDef *) SPI1_BASE);
        this_spi->irqn = SPI1_IRQn;
        
        /* reset SPI1 */
        SYSREG->SOFT_RST_CR |= SYSREG_SPI1_SOFTRESET_MASK;
        /* Clear any previously pended SPI1 interrupt */
        NVIC_ClearPendingIRQ(SPI1_IRQn);
        /* Take SPI1 out of reset. */
        SYSREG->SOFT_RST_CR &= ~SYSREG_SPI1_SOFTRESET_MASK;
    }
    
    /* De-assert reset bit. */
    this_spi->hw_reg->CONTROL &= ~CTRL_REG_RESET_MASK;
}

/***************************************************************************//**
 *
 *
 */
static void recover_from_rx_overflow
(
    mss_spi_instance_t * this_spi
)
{
    uint32_t control_reg;
    uint32_t clk_gen;
    uint32_t frame_size;
    uint32_t control2;
    uint32_t packet_size;
    uint32_t cmd_size;
    uint32_t slave_select;
    
    /*
     * Read current SPI hardware block configuration.
     */
    control_reg = this_spi->hw_reg->CONTROL;
    clk_gen = this_spi->hw_reg->CLK_GEN;
    frame_size = this_spi->hw_reg->TXRXDF_SIZE;
    control2 = this_spi->hw_reg->CONTROL2;
    packet_size = this_spi->hw_reg->PKTSIZE;
    cmd_size = this_spi->hw_reg->CMDSIZE;
    slave_select = this_spi->hw_reg->SLAVE_SELECT;
     
    /*
     * Reset the SPI hardware block.
     */
    if(this_spi == &g_mss_spi0)
    {
        this_spi->hw_reg = ((SPI_TypeDef *) SPI0_BASE);
        this_spi->irqn = SPI0_IRQn;

        /* reset SPI0 */
        SYSREG->SOFT_RST_CR |= SYSREG_SPI0_SOFTRESET_MASK;
        /* Clear any previously pended SPI0 interrupt */
        NVIC_ClearPendingIRQ(SPI0_IRQn);
        /* Take SPI0 out of reset. */
        SYSREG->SOFT_RST_CR &= ~SYSREG_SPI0_SOFTRESET_MASK;

        this_spi->hw_reg->CONTROL &= ~CTRL_REG_RESET_MASK;
    }
    else
    {
        this_spi->hw_reg = ((SPI_TypeDef *) SPI1_BASE);
        this_spi->irqn = SPI1_IRQn;
        
        /* reset SPI1 */
        SYSREG->SOFT_RST_CR |= SYSREG_SPI1_SOFTRESET_MASK;
        /* Clear any previously pended SPI1 interrupt */
        NVIC_ClearPendingIRQ(SPI1_IRQn);
        /* Take SPI1 out of reset. */
        SYSREG->SOFT_RST_CR &= ~SYSREG_SPI1_SOFTRESET_MASK;
        
        this_spi->hw_reg->CONTROL &= ~CTRL_REG_RESET_MASK;
    }
    
    /*
     * Restore SPI hardware block configuration.
     */
    control_reg &= ~(uint32_t)CTRL_ENABLE_MASK;
    this_spi->hw_reg->CONTROL = control_reg;
    this_spi->hw_reg->CLK_GEN = clk_gen;
    this_spi->hw_reg->TXRXDF_SIZE = frame_size;
    this_spi->hw_reg->CONTROL |= CTRL_ENABLE_MASK;
    this_spi->hw_reg->CONTROL2 = control2;
    this_spi->hw_reg->PKTSIZE = packet_size;
    this_spi->hw_reg->CMDSIZE = cmd_size;
    this_spi->hw_reg->SLAVE_SELECT = slave_select;
}

/***************************************************************************//**
 * MSS_SPI_configure_slave_mode()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_configure_slave_mode
(
    mss_spi_instance_t * this_spi,
    mss_spi_protocol_mode_t protocol_mode,
    uint8_t frame_bit_length
)
{
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    ASSERT(frame_bit_length <= MAX_FRAME_LENGTH);
    
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    /* Don't yet know what slave transfer mode will be used */
    this_spi->slave_xfer_mode = MSS_SPI_SLAVE_XFER_NONE;

    /* Set the mode. */
    this_spi->hw_reg->CONTROL &= ~(uint32_t)CTRL_MASTER_MASK;

    /* Set the protocol mode */
    this_spi->hw_reg->CONTROL &= ~(uint32_t)CTRL_ENABLE_MASK;
    this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~PROTOCOL_MODE_MASK) |
                                (uint32_t)protocol_mode | BIGFIFO_MASK;
    
    /* Set number of data frames to 1 by default */
    this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~TXRXDFCOUNT_MASK) |
                                ((uint32_t)1 << TXRXDFCOUNT_SHIFT);
    this_spi->hw_reg->TXRXDF_SIZE = frame_bit_length;
    this_spi->hw_reg->CONTROL |= CTRL_ENABLE_MASK;
    /* Reenable interrupts */
    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_configure_master_mode()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_configure_master_mode
(
    mss_spi_instance_t *    this_spi,
    mss_spi_slave_t         slave,
    mss_spi_protocol_mode_t protocol_mode,
    uint32_t                clk_div,
    uint8_t                 frame_bit_length
)
{
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    ASSERT(slave < MSS_SPI_MAX_NB_OF_SLAVES);
    ASSERT(frame_bit_length <= MAX_FRAME_LENGTH);
     /* Check that the requested clock divider is within range and an even number. */
    ASSERT(clk_div >= 2u);
    ASSERT(clk_div <= 512u);
    ASSERT(0u == (clk_div & 0x00000001));
   
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    /* Reset slave transfer mode to unknown to wipe slate clean */
    this_spi->slave_xfer_mode = MSS_SPI_SLAVE_XFER_NONE;

    /* Set the mode. */
    this_spi->hw_reg->CONTROL &= ~(uint32_t)CTRL_ENABLE_MASK;
    this_spi->hw_reg->CONTROL |= CTRL_MASTER_MASK;
    this_spi->hw_reg->CONTROL |= CTRL_ENABLE_MASK;

    /*
     * Keep track of the required register configuration for this slave. These
     * values will be used by the MSS_SPI_set_slave_select() function to configure
     * the master to match the slave being selected.
     */
    if(slave < MSS_SPI_MAX_NB_OF_SLAVES)     
    {
        uint32_t clk_gen;
        /*
        * Setting the SPS bit ensures the slave select remains asserted even
        * if we don't keep the TX FIFO filled in block mode. We only do it for
        * Motorola modes and if you need the slave selected deselected between
        * frames in modes 0 or 2 then remove SPS_MASK from below.
        */
        if((MSS_SPI_MODE0 == protocol_mode) || (MSS_SPI_MODE1 == protocol_mode) ||
           (MSS_SPI_MODE2 == protocol_mode) || (MSS_SPI_MODE3 == protocol_mode))
        {
            this_spi->slaves_cfg[slave].ctrl_reg = MASTER_MODE_MASK | SPS_MASK |
                                                   BIGFIFO_MASK | CTRL_CLKMODE_MASK |
                                                   (uint32_t)protocol_mode | 
                                                   ((uint32_t)1 << TXRXDFCOUNT_SHIFT);
        }
        else
        {
            this_spi->slaves_cfg[slave].ctrl_reg = MASTER_MODE_MASK |
                                                   BIGFIFO_MASK | CTRL_CLKMODE_MASK |
                                                   (uint32_t)protocol_mode | 
                                                   ((uint32_t)1 << TXRXDFCOUNT_SHIFT);
        }
        this_spi->slaves_cfg[slave].txrxdf_size_reg = frame_bit_length;

        clk_gen = (clk_div / 2u) - 1u;
        this_spi->slaves_cfg[slave].clk_gen = (uint8_t)clk_gen;
    }
    /* Reenable interrupts */
    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_set_slave_select()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_set_slave_select
(
    mss_spi_instance_t * this_spi,
    mss_spi_slave_t slave
)
{
    uint32_t rx_overflow;
    
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    
    /* This function is only intended to be used with an SPI master. */
    ASSERT((this_spi->hw_reg->CONTROL & CTRL_MASTER_MASK) == CTRL_MASTER_MASK);
    
    ASSERT(this_spi->slaves_cfg[slave].ctrl_reg != NOT_CONFIGURED);

    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    /* Recover from receive overflow. */
    rx_overflow = this_spi->hw_reg->STATUS & RX_OVERFLOW_MASK;
    if(rx_overflow)
    {
         recover_from_rx_overflow(this_spi);
    }
    
    /* Set the clock rate. */
    this_spi->hw_reg->CONTROL &= ~(uint32_t)CTRL_ENABLE_MASK;
    this_spi->hw_reg->CONTROL = this_spi->slaves_cfg[slave].ctrl_reg;
    this_spi->hw_reg->CLK_GEN = this_spi->slaves_cfg[slave].clk_gen;
    this_spi->hw_reg->TXRXDF_SIZE = this_spi->slaves_cfg[slave].txrxdf_size_reg;
    this_spi->hw_reg->CONTROL |= CTRL_ENABLE_MASK;
    
    /* Set slave select */
    this_spi->hw_reg->SLAVE_SELECT |= ((uint32_t)1 << (uint32_t)slave);
    /* Reenable interrupts */
    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_clear_slave_select()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_clear_slave_select
(
    mss_spi_instance_t * this_spi,
    mss_spi_slave_t slave
)
{
    uint32_t rx_overflow;
    
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    
    /* This function is only intended to be used with an SPI master. */
    ASSERT((this_spi->hw_reg->CONTROL & CTRL_MASTER_MASK) == CTRL_MASTER_MASK);

    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    /* Recover from receive overflow. */
    rx_overflow = this_spi->hw_reg->STATUS & RX_OVERFLOW_MASK;
    if(rx_overflow)
    {
         recover_from_rx_overflow(this_spi);
    }
    
    this_spi->hw_reg->SLAVE_SELECT &= ~((uint32_t)1 << (uint32_t)slave);
    /* Reenable interrupts */
    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_transfer_frame()
 * See "mss_spi.h" for details of how to use this function.
 */
uint32_t MSS_SPI_transfer_frame
(
    mss_spi_instance_t * this_spi,
    uint32_t tx_bits
)
{
    uint32_t rx_ready;
    uint32_t tx_done;
    
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    
    /* This function is only intended to be used with an SPI master. */
    ASSERT((this_spi->hw_reg->CONTROL & CTRL_MASTER_MASK) == CTRL_MASTER_MASK);
    
    /* Ensure single frame transfer selected so interrupts work correctly */
    this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~TXRXDFCOUNT_MASK)
                                | ((uint32_t)1u << TXRXDFCOUNT_SHIFT);

    /* Flush the Tx and Rx FIFOs. */
    this_spi->hw_reg->COMMAND |= (TX_FIFO_RESET_MASK | RX_FIFO_RESET_MASK);
    
    /* Send frame. */
    this_spi->hw_reg->TX_DATA = tx_bits;
    
    /* Wait for frame Tx to complete. */
    tx_done = this_spi->hw_reg->STATUS & TX_DONE_MASK;
    while(0u == tx_done)
    {
        tx_done = this_spi->hw_reg->STATUS & TX_DONE_MASK;
    }
    
    /* Read received frame. */
    /* Wait for Rx complete. */
    rx_ready = this_spi->hw_reg->STATUS & RX_DATA_READY_MASK;
    while(0u == rx_ready)
    {
        rx_ready = this_spi->hw_reg->STATUS & RX_DATA_READY_MASK;
    }
    /* Return Rx data. */
    return( this_spi->hw_reg->RX_DATA );
}


/***************************************************************************//**
 * MSS_SPI_transfer_block()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_transfer_block
(
    mss_spi_instance_t * this_spi,
    const uint8_t * cmd_buffer,
    uint16_t cmd_byte_size,
    uint8_t * rd_buffer,
    uint16_t rd_byte_size
)
{
    uint16_t transfer_idx = 0u;
    uint16_t tx_idx;
    uint16_t rx_idx;
    uint32_t frame_count;
    volatile uint32_t rx_raw;
    uint16_t transit = 0u;
    uint32_t tx_fifo_full;
    uint32_t rx_overflow;
    uint32_t rx_fifo_empty;
    
    uint16_t transfer_size;     /* Total number of bytes transfered. */
    
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    
    /* This function is only intended to be used with an SPI master. */
    ASSERT((this_spi->hw_reg->CONTROL & CTRL_MASTER_MASK) == CTRL_MASTER_MASK);
    
    /* Compute number of bytes to transfer. */
    transfer_size = cmd_byte_size + rd_byte_size;
    
    /* Adjust to 1 byte transfer to cater for DMA transfers. */
    if(0u == transfer_size)
    {
        frame_count = 1u;
    }
    else
    {
        frame_count = transfer_size;
    }

    /* Flush the Tx and Rx FIFOs. */
    this_spi->hw_reg->COMMAND |= (TX_FIFO_RESET_MASK | RX_FIFO_RESET_MASK);
    
    /* Recover from receive overflow. */
    rx_overflow = this_spi->hw_reg->STATUS & RX_OVERFLOW_MASK;
    if(rx_overflow)
    {
         recover_from_rx_overflow(this_spi);
    }
    
    /* Set frame size to 8 bits and the frame count to the transfer size. */
    this_spi->hw_reg->CONTROL &= ~(uint32_t)CTRL_ENABLE_MASK;
    this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~TXRXDFCOUNT_MASK) | ( (frame_count << TXRXDFCOUNT_SHIFT) & TXRXDFCOUNT_MASK);
    this_spi->hw_reg->TXRXDF_SIZE = MSS_SPI_BLOCK_TRANSFER_FRAME_SIZE;
    this_spi->hw_reg->CONTROL |= CTRL_ENABLE_MASK;

    /* Flush the receive FIFO. */
    rx_fifo_empty = this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK;
    while(0u == rx_fifo_empty)
    {
        rx_raw = this_spi->hw_reg->RX_DATA;
        rx_fifo_empty = this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK;
    }
    
    tx_idx = 0u;
    rx_idx = 0u;
    if(tx_idx < cmd_byte_size)
    {
        this_spi->hw_reg->TX_DATA = cmd_buffer[tx_idx];
        ++tx_idx;
        ++transit;
    }
    else
    {
        if(tx_idx < transfer_size)
        {
            this_spi->hw_reg->TX_DATA = 0x00u;
            ++tx_idx;
            ++transit;
        }
    }
    /* Perform the remainder of the transfer by sending a byte every time a byte
     * has been received. This should ensure that no Rx overflow can happen in
     * case of an interrupt occurs during this function. */
    while(transfer_idx < transfer_size)
    {
        rx_fifo_empty = this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK;
        if(0u == rx_fifo_empty)
        {
            /* Process received byte. */
            rx_raw = this_spi->hw_reg->RX_DATA;
            if(transfer_idx >= cmd_byte_size)
            {
                if(rx_idx < rd_byte_size)
                {
                    rd_buffer[rx_idx] = (uint8_t)rx_raw;   
                }
                ++rx_idx;
            }
            ++transfer_idx;
            --transit;
        }

        tx_fifo_full = this_spi->hw_reg->STATUS & TX_FIFO_FULL_MASK;
        if(0u == tx_fifo_full)
        {
            if(transit < RX_FIFO_SIZE)
            {
                /* Send another byte. */
                if(tx_idx < cmd_byte_size)
                {
                    this_spi->hw_reg->TX_DATA = cmd_buffer[tx_idx];
                    ++tx_idx;
                    ++transit;
                }
                else
                {
                    if(tx_idx < transfer_size)
                    {
                        this_spi->hw_reg->TX_DATA = 0x00u;
                        ++tx_idx;
                        ++transit;
                    }
                }
            }
        }
    }
}

/***************************************************************************//**
 * MSS_SPI_set_frame_rx_handler()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_set_frame_rx_handler
(
    mss_spi_instance_t * this_spi,
    mss_spi_frame_rx_handler_t rx_handler
)
{
    uint32_t tx_fifo_empty;
    
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    
    /* This function is only intended to be used with an SPI slave. */
    ASSERT((this_spi->hw_reg->CONTROL & CTRL_MASTER_MASK) != CTRL_MASTER_MASK);
    
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    /* Disable block Rx handlers as they are mutually exclusive. */
    this_spi->block_rx_handler = 0u;
    this_spi->cmd_handler = 0u;
    
    /* Keep a copy of the pointer to the rx handler function. */
    this_spi->frame_rx_handler = rx_handler;
    
    /* Make sure correct mode is selected */
    this_spi->slave_xfer_mode = MSS_SPI_SLAVE_XFER_FRAME;

    /* Automatically fill the TX FIFO with zeroes if no slave tx frame set.*/
    tx_fifo_empty = this_spi->hw_reg->STATUS & TX_FIFO_EMPTY_MASK;
    if(tx_fifo_empty)
    {
        this_spi->hw_reg->COMMAND |= AUTOFILL_MASK;
    }
    
    /* Ensure single frame transfer selected so interrupts work correctly */
    this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~TXRXDFCOUNT_MASK)
                                | ((uint32_t)1u << TXRXDFCOUNT_SHIFT);

    /* Disable block specific interrupts */
    this_spi->hw_reg->CONTROL2 &= ~(uint32_t)C2_ENABLE_CMD_IRQ_MASK;
    this_spi->hw_reg->CONTROL2 &= ~(uint32_t)C2_ENABLE_SSEND_IRQ_MASK;

    /* Clear down ints to avoid stale ints triggering when we enable them below */
    this_spi->hw_reg->INT_CLEAR = TXURUN_IRQ_MASK | RXOVFLOW_IRQ_MASK |
                                  RXDONE_IRQ_MASK;
    /*
     * Enable TX underrun and RX overflow interrupts to improve error
     * recovery and the Rx interrupt.
     */
    this_spi->hw_reg->CONTROL |= CTRL_URUN_IRQ_EN_MASK | CTRL_OVFLOW_IRQ_EN_MASK |
                                 CTRL_RX_IRQ_EN_MASK;
    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_set_slave_tx_frame()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_set_slave_tx_frame
(
    mss_spi_instance_t * this_spi,
    uint32_t frame_value
)
{
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));

    /* This function is only intended to be used with an SPI slave. */
    ASSERT((this_spi->hw_reg->CONTROL & CTRL_MASTER_MASK) != CTRL_MASTER_MASK);
    
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    /* Make sure correct mode is selected */
    this_spi->slave_xfer_mode = MSS_SPI_SLAVE_XFER_FRAME;

    /* Disable block Rx handlers as they are mutually exclusive. */
    this_spi->block_rx_handler = 0u;
    this_spi->cmd_handler = 0u;

    /* Disable slave block tx buffer as it is mutually exclusive with frame
     * level handling. */    
    this_spi->slave_tx_buffer = 0u;
    this_spi->slave_tx_size = 0u;
    this_spi->slave_tx_idx = 0u;
    
    /* Keep a copy of the slave tx frame value. */
    this_spi->slave_tx_frame = frame_value;
    
    /* Disable automatic fill of the TX FIFO with zeroes.*/
    this_spi->hw_reg->COMMAND &= ~(uint32_t)AUTOFILL_MASK;
    this_spi->hw_reg->COMMAND |= TX_FIFO_RESET_MASK;
    /*
     * Ensure single frame transfer selected so interrupts work correctly
     *
     * IMPORTANT: Note this must be done before writing to the TX_DATA register
     * as it seems that doing these in the opposite order causes the receive
     * and transmit interrupts to be disabled.
     */
    this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~TXRXDFCOUNT_MASK)
                                | ((uint32_t)1u << TXRXDFCOUNT_SHIFT);

    /* Load frame into Tx data register. */
    this_spi->hw_reg->TX_DATA = this_spi->slave_tx_frame;

   /* Disable block specific interrupts */
    this_spi->hw_reg->CONTROL2 &= ~(uint32_t)C2_ENABLE_CMD_IRQ_MASK;
    this_spi->hw_reg->CONTROL2 &= ~(uint32_t)C2_ENABLE_SSEND_IRQ_MASK;

    /* Clear down ints to avoid stale ints triggering when we enable them below */
    this_spi->hw_reg->INT_CLEAR = TXURUN_IRQ_MASK | RXOVFLOW_IRQ_MASK |
                                  TXDONE_IRQ_MASK;
    /*
     * Enable Tx Done interrupt in order to reload the slave Tx frame after each
     * time it has been sent.
     *
     * Enable TX underrun and RX overflow interrupts to improve error
     * recovery.
     */
    this_spi->hw_reg->CONTROL |= CTRL_TX_IRQ_EN_MASK | CTRL_URUN_IRQ_EN_MASK |
                                 CTRL_OVFLOW_IRQ_EN_MASK;

    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_set_slave_block_buffers()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_set_slave_block_buffers
(
    mss_spi_instance_t * this_spi,
    const uint8_t * tx_buffer,
    uint32_t tx_buff_size,
    uint8_t * rx_buffer,
    uint32_t rx_buff_size,
    mss_spi_block_rx_handler_t block_rx_handler
)
{
    uint32_t frame_count;
    uint32_t done = 0u;
    
    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
    
    /* This function is only intended to be used with an SPI slave. */
    ASSERT((this_spi->hw_reg->CONTROL & CTRL_MASTER_MASK) != CTRL_MASTER_MASK);
    
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    /* Make sure correct mode is selected */
    this_spi->slave_xfer_mode = MSS_SPI_SLAVE_XFER_BLOCK;

    /* Set cmd_done correctly to ensure 0 padding works. */
    if(0u == this_spi->cmd_handler)
    {
        this_spi->cmd_done = 1u;
    }
    else
    {
        this_spi->cmd_done = 0u;
    }

    /* Disable Rx frame handler as it is mutually exclusive with block rx handler. */
    this_spi->frame_rx_handler = 0u;
    
    /* Keep a copy of the pointer to the block rx handler function. */
    this_spi->block_rx_handler = block_rx_handler;
    
    this_spi->slave_rx_buffer = rx_buffer;
    this_spi->slave_rx_size = rx_buff_size;
    this_spi->slave_rx_idx = 0u;
    
    /* Initialise the transmit state data. */
    this_spi->slave_tx_buffer = tx_buffer;
    this_spi->slave_tx_size = tx_buff_size;
    this_spi->slave_tx_idx = 0u;

    /* Flush the Tx and Rx FIFOs. Please note this does not have any effect on A2F200. */
    this_spi->hw_reg->COMMAND |= (TX_FIFO_RESET_MASK | RX_FIFO_RESET_MASK);

    /* Recover from receive overflow if needs be */
    if(0u != (this_spi->hw_reg->STATUS & RX_OVERFLOW_MASK))
    {
         recover_from_rx_overflow(this_spi);
    }

    /* Flush Rx FIFO in case we are executing on A2F200. */
    while(0u == (this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK))
    {
        volatile uint32_t dummy;
        dummy = this_spi->hw_reg->RX_DATA;
        dummy = dummy;  /* Prevent Lint warning. */
    }

    /* Use the frame counter to control how often receive interrupts are generated. */
    frame_count = RX_IRQ_THRESHOLD;
    
    this_spi->hw_reg->CONTROL &= ~(uint32_t)CTRL_ENABLE_MASK;
    this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~TXRXDFCOUNT_MASK) |
                                (frame_count << TXRXDFCOUNT_SHIFT);
    this_spi->hw_reg->TXRXDF_SIZE = MSS_SPI_BLOCK_TRANSFER_FRAME_SIZE;
    this_spi->hw_reg->CONTROL |= CTRL_ENABLE_MASK;
    
    /* Load the transmit FIFO. */
    while((0u == (this_spi->hw_reg->STATUS & TX_FIFO_FULL_MASK)) && (0u == done))
    {
        if(this_spi->slave_tx_idx < this_spi->slave_tx_size)
        {
            this_spi->hw_reg->TX_DATA = this_spi->slave_tx_buffer[this_spi->slave_tx_idx];
        }
        else if(0u != this_spi->cmd_done)
        {
            /* Fill with 0s if no need to insert command response */
            this_spi->hw_reg->TX_DATA = 0x00u;
        }
        else
        {
            /* Exit loop early as command response needs to be inserted next */
            done = 1u;
        }
        ++this_spi->slave_tx_idx;
    }

    if(tx_buff_size > 0u)
    {
        /* Clear and enable TX interrupt. Also disable autofill */
        this_spi->hw_reg->COMMAND &= ~(uint32_t)AUTOFILL_MASK;
        this_spi->hw_reg->INT_CLEAR = TXDONE_IRQ_MASK;
        this_spi->hw_reg->CONTROL |= CTRL_TX_IRQ_EN_MASK;
    }
    else
    {
        this_spi->hw_reg->COMMAND |= AUTOFILL_MASK;
    }
    
    /* Ensure command interrupt disabled if no handler */
    if(0u == this_spi->cmd_handler)
    {
        this_spi->hw_reg->CONTROL2 &= ~(uint32_t)C2_ENABLE_CMD_IRQ_MASK;
    }
    /*
     * Enable slave select release interrupt. The SSEND interrupt is used to
     * complete reading of the recieve FIFO and prepare the transmit FIFO for
     * the next transaction.
     *
     * Make sure to clear any pending ssend ints otherwise we will trigger
     * an immediate interrupt.
     */
    this_spi->hw_reg->INT_CLEAR = SSEND_IRQ_MASK;
    this_spi->hw_reg->CONTROL2 |= C2_ENABLE_SSEND_IRQ_MASK;
    
    /* Clear down ints to avoid stale ints triggering when we enable them below */
    this_spi->hw_reg->INT_CLEAR = TXURUN_IRQ_MASK | RXOVFLOW_IRQ_MASK |
                                  RXDONE_IRQ_MASK;
    /*
     * Enable TX underrun and RX overflow interrupts to improve error
     * recovery and enable Rx interrupt.
     */
    this_spi->hw_reg->CONTROL |= CTRL_RX_IRQ_EN_MASK | CTRL_URUN_IRQ_EN_MASK |
                                 CTRL_OVFLOW_IRQ_EN_MASK;

    NVIC_EnableIRQ(this_spi->irqn);
}

/***************************************************************************//**
 * MSS_SPI_set_cmd_handler()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_set_cmd_handler
(
    mss_spi_instance_t * this_spi,
    mss_spi_block_rx_handler_t cmd_handler,
    uint32_t cmd_size
)
{
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    /* Make sure response state is cleared down */
    this_spi->resp_tx_buffer   = 0u;
    this_spi->resp_buff_size   = 0u;
    this_spi->resp_buff_tx_idx = 0u;
    
    if(0u == cmd_handler)
    {
        /*
         * Set this flag so zero padding is enabled
         */
        this_spi->cmd_done = 1u;
        /*
         * Ensure command interrupt disabled if no handler 
         * and handler pointer is wiped clean.
         */
        this_spi->cmd_handler = 0u;
        this_spi->hw_reg->CMDSIZE = 0u;
        this_spi->hw_reg->CONTROL2 &= ~(uint32_t)C2_ENABLE_CMD_IRQ_MASK;
    }
    else
    {
        /*
         * Clear this flag so zero padding is disabled until command response
         * has been taken care of.
         */
        this_spi->cmd_done = 0u;

        this_spi->cmd_handler = cmd_handler;
        this_spi->hw_reg->CMDSIZE = cmd_size;
        /* Flush the Tx FIFO. Please note this does not have any effect on A2F200. */
        this_spi->hw_reg->COMMAND |= (TX_FIFO_RESET_MASK | RX_FIFO_RESET_MASK);
        /*
         * Reload TX FIFO as MSS_SPI_set_slave_block_buffers() may have zero filled
         * the FIFO if command handler was not in place when it was called and so 
         * the first frame sent could be wrong.
         */
        this_spi->slave_tx_idx    = 0u;
        fill_slave_tx_fifo(this_spi);
        /*
         * Make sure to clear any pending command ints otherwise we will trigger
         * an immediate interrupt.
         */
        this_spi->hw_reg->INT_CLEAR = CMD_IRQ_MASK;
        this_spi->hw_reg->CONTROL2 |= C2_ENABLE_CMD_IRQ_MASK;
    }
    
    NVIC_EnableIRQ(this_spi->irqn); /* Safe to allow interrupts again */
}

/***************************************************************************//**
 * MSS_SPI_set_cmd_response()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_set_cmd_response
(
    mss_spi_instance_t * this_spi,
    const uint8_t * resp_tx_buffer,
    uint32_t resp_buff_size
)
{
    this_spi->resp_tx_buffer = resp_tx_buffer;
    this_spi->resp_buff_size = resp_buff_size;
    this_spi->resp_buff_tx_idx = 0u;
    /* Note that we have provided response and start getting it into the FIFO */
    this_spi->cmd_done = 1u;
    fill_slave_tx_fifo(this_spi);
}

/***************************************************************************//**
 * MSS_SPI_enable()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_enable
(
    mss_spi_instance_t * this_spi
)
{
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    this_spi->hw_reg->CONTROL |= CTRL_ENABLE_MASK;
    
    /* Reenable interrupts */
    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_disable()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_disable
(
    mss_spi_instance_t * this_spi
)
{
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    this_spi->hw_reg->CONTROL &= ~(uint32_t)CTRL_ENABLE_MASK;

    /* Reenable interrupts */
    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_set_transfer_byte_count()
 * See "mss_spi.h" for details of how to use this function.
 */
void MSS_SPI_set_transfer_byte_count
(
    mss_spi_instance_t * this_spi,
    uint16_t byte_count
)
{
    /* Shut down interrupts from the MSS SPI while we do this */
    NVIC_DisableIRQ( this_spi->irqn );

    this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~TXRXDFCOUNT_MASK)
                                | (((uint32_t)byte_count << TXRXDFCOUNT_SHIFT) & TXRXDFCOUNT_MASK);
                                
    /* This value can only be updated when the MSS SPI is disabled */
    this_spi->hw_reg->CONTROL &= ~(uint32_t)CTRL_ENABLE_MASK;
    this_spi->hw_reg->TXRXDF_SIZE = MSS_SPI_BLOCK_TRANSFER_FRAME_SIZE;
    this_spi->hw_reg->CONTROL |= CTRL_ENABLE_MASK;
    /* Reenable interrupts */
    NVIC_EnableIRQ( this_spi->irqn );
}

/***************************************************************************//**
 * MSS_SPI_tx_done()
 * See "mss_spi.h" for details of how to use this function.
 */
uint32_t MSS_SPI_tx_done
(
    mss_spi_instance_t * this_spi
)
{
    uint32_t tx_done;
    
    tx_done = this_spi->hw_reg->STATUS & TX_DONE_MASK;
    
    return tx_done;
}

/***************************************************************************//**
 * Fill the transmit FIFO (used for slave block transfers).
 */
static void fill_slave_tx_fifo
(
    mss_spi_instance_t * this_spi
)
{
    uint32_t guard = 0u;

    while((0u == (this_spi->hw_reg->STATUS & TX_FIFO_FULL_MASK)) &&
          (this_spi->slave_tx_idx < this_spi->slave_tx_size))
    {
        /* Sending from primary slave transmit buffer */
        this_spi->hw_reg->TX_DATA = this_spi->slave_tx_buffer[this_spi->slave_tx_idx];
        ++this_spi->slave_tx_idx;
    }

    if(this_spi->slave_tx_idx >= this_spi->slave_tx_size)
    {
        while((0u == (this_spi->hw_reg->STATUS & TX_FIFO_FULL_MASK)) &&
              (this_spi->resp_buff_tx_idx < this_spi->resp_buff_size))
        {
            /* Sending from command response buffer */
            this_spi->hw_reg->TX_DATA = this_spi->resp_tx_buffer[this_spi->resp_buff_tx_idx];
            ++this_spi->resp_buff_tx_idx;
        }
    }

    if((0u != this_spi->cmd_done) && (this_spi->slave_tx_idx >= this_spi->slave_tx_size) &&
       (this_spi->resp_buff_tx_idx >= this_spi->resp_buff_size))
    {
        while((0u == (this_spi->hw_reg->STATUS & TX_FIFO_FULL_MASK)) &&
              (guard < BIG_FIFO_SIZE))
        {
            /* Nothing left so pad with 0s for consistency */
            this_spi->hw_reg->TX_DATA = 0x00u;
            /*
             * We use the guard count to cover the unlikely event that we are
             * never seeing the TX FIFO full because the data is being pulled
             * out as fast as we can stuff it in. In this event we never spend
             * more than a full FIFOs worth of time spinning here.
             */
            guard++;
        }
    }

}

/***************************************************************************//**
 * 
 */
static void read_slave_rx_fifo
(
    mss_spi_instance_t * this_spi
)
{
    volatile uint32_t rx_frame;
    
    if(MSS_SPI_SLAVE_XFER_FRAME == this_spi->slave_xfer_mode)
    {
        while(0u == (this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK))
        {
            /* Single frame handling mode. */
            rx_frame = this_spi->hw_reg->RX_DATA;
            if(0u != this_spi->frame_rx_handler)
            {
                this_spi->frame_rx_handler( rx_frame );
            }
        }
    }
    else if(MSS_SPI_SLAVE_XFER_BLOCK == this_spi->slave_xfer_mode)
    {
        /* Block handling mode. */
        while(0u == (this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK)) /* Something needs to be read from FIFO */
        {
            rx_frame = this_spi->hw_reg->RX_DATA;
            if(this_spi->slave_rx_idx < this_spi->slave_rx_size)
            {
                this_spi->slave_rx_buffer[this_spi->slave_rx_idx] = (uint8_t)rx_frame;
            }

            ++this_spi->slave_rx_idx;
        }
    }
    else
    {
        /* Should not happen... Just purge FIFO */
        while(0u == (this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK))
        {
            rx_frame = this_spi->hw_reg->RX_DATA;
        }
    }
}

/***************************************************************************//**
 * SPI interrupt service routine.
 */
static void mss_spi_isr
(
    mss_spi_instance_t * this_spi
)
{    
    volatile uint32_t rx_frame;
    __I  uint32_t *this_mis = &this_spi->hw_reg->MIS;

    ASSERT((this_spi == &g_mss_spi0) || (this_spi == &g_mss_spi1));
  
    if(0u != (*this_mis & RXDONE_IRQ_MASK))
    {
        if(MSS_SPI_SLAVE_XFER_FRAME == this_spi->slave_xfer_mode)
        {
            /* Single frame handling mode. */
            while(0u == (this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK))
            {
                rx_frame = this_spi->hw_reg->RX_DATA;
                if(0u != this_spi->frame_rx_handler)
                {
                    this_spi->frame_rx_handler( rx_frame );
                }
            }
        }
        else if(MSS_SPI_SLAVE_XFER_BLOCK == this_spi->slave_xfer_mode)
        {
            /* Block handling mode. */
            while(0u == (this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK)) /* Something needs to be read from FIFO */
            {
                rx_frame = this_spi->hw_reg->RX_DATA;                /* Read from FIFO irrespective */
                if(this_spi->slave_rx_idx < this_spi->slave_rx_size) /* Write to array if required */
                {
                    this_spi->slave_rx_buffer[this_spi->slave_rx_idx] = (uint8_t)rx_frame;
                }

                ++this_spi->slave_rx_idx;            
            }
        }
        else
        {
            /* No slave handling in place so just purge FIFO */
            while(0u == (this_spi->hw_reg->STATUS & RX_FIFO_EMPTY_MASK))
            {
                rx_frame = this_spi->hw_reg->RX_DATA;
            }
        }

        this_spi->hw_reg->INT_CLEAR = RXDONE_IRQ_MASK;
    }

   /* Handle transmit. */
    if(0u != (*this_mis & TXDONE_IRQ_MASK))
    {
        if( MSS_SPI_SLAVE_XFER_FRAME == this_spi->slave_xfer_mode )
        {
           /* Reload slave tx frame into Tx data register. */
            this_spi->hw_reg->TX_DATA = this_spi->slave_tx_frame;
        }
        else /* Must be block mode so load FIFO to the max */
        {
            fill_slave_tx_fifo(this_spi);
        }

        this_spi->hw_reg->INT_CLEAR = TXDONE_IRQ_MASK;
    }
    
    /* Handle command interrupt. */
    if(0u != (*this_mis & CMD_IRQ_MASK))
    {
        read_slave_rx_fifo(this_spi);
        
        /*
         * Call the command handler if one exists.
         */
        if(0u != this_spi->cmd_handler)
        {
            (*this_spi->cmd_handler)(this_spi->slave_rx_buffer, this_spi->slave_rx_idx);
            fill_slave_tx_fifo(this_spi);
        }
        /* Set cmd_done to indicate it is now safe to 0 fill TX FIFO */
        this_spi->cmd_done = 1u;
        /* Disable command interrupt until slave select becomes de-asserted to avoid retriggering. */
        this_spi->hw_reg->CONTROL2 &= ~(uint32_t)C2_ENABLE_CMD_IRQ_MASK;
        this_spi->hw_reg->INT_CLEAR = CMD_IRQ_MASK;
    }

    if(0u != (*this_mis & RXOVFLOW_IRQ_MASK))
    {
        /*
         * Receive overflow, not a lot we can do for this. Reset the receive
         *  FIFO, clear the interrupt and hope it doesn't happen again...
         */
        this_spi->hw_reg->COMMAND |= RX_FIFO_RESET_MASK;
        recover_from_rx_overflow(this_spi);
        this_spi->hw_reg->INT_CLEAR = RXOVFLOW_IRQ_MASK;
    }
    /*
     * Transmit underrun, try and recover by reapplying the current
     * slave TX FIFO data setup (if there is one).
     * In block mode this will probably not be very successful as we will
     * be out of synch with the master but the reset on SSEND will hopefully
     * take care of that for the next transfer.
     */
    if(0u != (*this_mis & TXURUN_IRQ_MASK))
    {
        this_spi->hw_reg->COMMAND |= TX_FIFO_RESET_MASK;
        if( MSS_SPI_SLAVE_XFER_FRAME == this_spi->slave_xfer_mode )
        {
            this_spi->hw_reg->CONTROL = (this_spi->hw_reg->CONTROL & ~TXRXDFCOUNT_MASK)
                                        | ((uint32_t)1u << TXRXDFCOUNT_SHIFT);
           /* Reload slave tx frame into Tx data register. */
            this_spi->hw_reg->TX_DATA = this_spi->slave_tx_frame;
        }
        else if( MSS_SPI_SLAVE_XFER_BLOCK == this_spi->slave_xfer_mode )
        {
            /* Block mode so reload FIFO to the max */
            this_spi->slave_tx_idx = 0u;
            fill_slave_tx_fifo(this_spi);
        }
        else
        {
            /* Not frame or block mode? Can't do anything here... */
        }

        this_spi->hw_reg->INT_CLEAR = TXURUN_IRQ_MASK;
    }

    /*
     * Handle slave select becoming de-asserted. Only enables if
     * we are operating in block mode, in frame mode we do everything
     * in the receive and transmit interrupt handlers.
     */
    if(0u != (*this_mis & SSEND_IRQ_MASK))
    {
        uint32_t rx_size;
        
        read_slave_rx_fifo(this_spi);
        rx_size = this_spi->slave_rx_idx;
        /*
         * Re-enable command interrupt if required and clear all the response
         * buffer state in readiness for next response. This must be done
         * before reloading the TX FIFO.
         */
        if(0 != this_spi->cmd_handler)
        {
            this_spi->cmd_done = 0u;
            this_spi->resp_tx_buffer = 0u;
            this_spi->resp_buff_size = 0u;
            this_spi->resp_buff_tx_idx = 0u;
            this_spi->hw_reg->INT_CLEAR = CMD_IRQ_MASK;
            this_spi->hw_reg->CONTROL2 |= C2_ENABLE_CMD_IRQ_MASK;
        }
        /* 
         * Reset the transmit index to 0 to restart transmit at the start of the
         * transmit buffer in the next transaction. This also requires flushing
         * the Tx FIFO and refilling it with the start of Tx data buffer.
         */
        this_spi->slave_tx_idx = 0u;
        this_spi->hw_reg->COMMAND |= (TX_FIFO_RESET_MASK | RX_FIFO_RESET_MASK);
        fill_slave_tx_fifo(this_spi);
        
        /* Prepare to receive next packet. */
        this_spi->slave_rx_idx = 0u;
        /*
         * Call the receive handler if one exists.
         */
        if(0u != this_spi->block_rx_handler)
        {
            (*this_spi->block_rx_handler)(this_spi->slave_rx_buffer, rx_size);
        }
        
        this_spi->hw_reg->INT_CLEAR = SSEND_IRQ_MASK;
    }
}


/***************************************************************************//**
 * SPIO interrupt service routine.
 * Please note that the name of this ISR is defined as part of the SmartFusion2
 * CMSIS startup code.
 */
#if defined(__GNUC__)
__attribute__((__interrupt__)) void SPI0_IRQHandler(void)
#else
void SPI0_IRQHandler( void )
#endif
{
    mss_spi_isr(&g_mss_spi0);
}

/***************************************************************************//**
 * SPI1 interrupt service routine.
 * Please note that the name of this ISR is defined as part of the SmartFusion2
 * CMSIS startup code.
 */
#if defined(__GNUC__)
__attribute__((__interrupt__)) void SPI1_IRQHandler(void)
#else
void SPI1_IRQHandler(void)
#endif
{
    mss_spi_isr(&g_mss_spi1);
}

#ifdef __cplusplus
}
#endif