@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":255:4:255:9|Register bit CORECONFIGP_0.paddr[16] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[31] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[30] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[29] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[28] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[27] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[26] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[25] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[24] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[23] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[22] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[21] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[20] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: MO160 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Register bit CORECONFIGP_0.FIC_2_APB_M_PRDATA[19] (in view view:work.MDDR_Demo_sb(verilog)) is always 0. To keep the instance, apply syn_preserve=1 on the instance.
@W: BN132 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\actel\directcore\coreconfigp\7.1.100\rtl\vlog\core\coreconfigp.v":546:4:546:9|Removing instance MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORECONFIGP_0.FIC_2_APB_M_PRDATA[18] because it is equivalent to instance MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORECONFIGP_0.FIC_2_APB_M_PRDATA[17]. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\hdl\axi_if.v":95:0:95:5|Removing instance MDDR_Demo_top_0.AXI_IF_0.AWLEN[3] because it is equivalent to instance MDDR_Demo_top_0.AXI_IF_0.AWLEN[2]. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\hdl\axi_if.v":95:0:95:5|Removing instance MDDR_Demo_top_0.AXI_IF_0.AWLEN[2] because it is equivalent to instance MDDR_Demo_top_0.AXI_IF_0.AWLEN[1]. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\hdl\axi_if.v":95:0:95:5|Removing instance MDDR_Demo_top_0.AXI_IF_0.AWLEN[1] because it is equivalent to instance MDDR_Demo_top_0.AXI_IF_0.AWLEN[0]. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\hdl\axi_if.v":222:0:222:5|Removing instance MDDR_Demo_top_0.AXI_IF_0.ARLEN[3] because it is equivalent to instance MDDR_Demo_top_0.AXI_IF_0.ARLEN[2]. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\hdl\axi_if.v":222:0:222:5|Removing instance MDDR_Demo_top_0.AXI_IF_0.ARLEN[2] because it is equivalent to instance MDDR_Demo_top_0.AXI_IF_0.ARLEN[1]. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\hdl\axi_if.v":222:0:222:5|Removing instance MDDR_Demo_top_0.AXI_IF_0.ARLEN[1] because it is equivalent to instance MDDR_Demo_top_0.AXI_IF_0.ARLEN[0]. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: MT246 :"c:\users\i63442\desktop\v12.6 updates\smart fusion2\new folder\m2s_dg0568_liberov11p8_sp1_df\sf2_mddr_demo_df\final\m2s_dg0534_df\libero_project\component\work\mddr_demo_sb\ccc_0\mddr_demo_sb_ccc_0_fccc.v":23:36:23:43|Blackbox CCC is missing a user supplied timing model. This may have a negative effect on timing analysis and optimizations (Quality of Results)
@W: MT447 :"c:/users/i63442/desktop/v12.6 updates/smart fusion2/new folder/m2s_dg0568_liberov11p8_sp1_df/sf2_mddr_demo_df/final/m2s_dg0534_df/libero_project/designer/top/synthesis.fdc":13:0:13:0|Timing constraint (from [get_cells { MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORERESETP_0.MSS_HPMS_READY_int }] to [get_cells { MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORERESETP_0.sm0_areset_n_rcosc MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORERESETP_0.sm0_areset_n_rcosc_q1 }]) (false path) was not applied to the design because none of the paths specified by the constraint exist in the design 
@W: MT447 :"c:/users/i63442/desktop/v12.6 updates/smart fusion2/new folder/m2s_dg0568_liberov11p8_sp1_df/sf2_mddr_demo_df/final/m2s_dg0534_df/libero_project/designer/top/synthesis.fdc":14:0:14:0|Timing constraint (from [get_cells { MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORERESETP_0.MSS_HPMS_READY_int MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORERESETP_0.SDIF*_PERST_N_re }] to [get_cells { MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORERESETP_0.sdif*_areset_n_rcosc* }]) (false path) was not applied to the design because none of the paths specified by the constraint exist in the design 
@W: MT447 :"c:/users/i63442/desktop/v12.6 updates/smart fusion2/new folder/m2s_dg0568_liberov11p8_sp1_df/sf2_mddr_demo_df/final/m2s_dg0534_df/libero_project/designer/top/synthesis.fdc":16:0:16:0|Timing constraint (through [get_pins { MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.MDDR_Demo_sb_MSS_0.MSS_ADLIB_INST.CONFIG_PRESET_N }]) (false path) was not applied to the design because none of the paths specified by the constraint exist in the design 
@W: MT447 :"c:/users/i63442/desktop/v12.6 updates/smart fusion2/new folder/m2s_dg0568_liberov11p8_sp1_df/sf2_mddr_demo_df/final/m2s_dg0534_df/libero_project/designer/top/synthesis.fdc":17:0:17:0|Timing constraint (through [get_pins { MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.SYSRESET_POR.POWER_ON_RESET_N }]) (false path) was not applied to the design because none of the paths specified by the constraint exist in the design 
@W: MT443 :"c:/users/i63442/desktop/v12.6 updates/smart fusion2/new folder/m2s_dg0568_liberov11p8_sp1_df/sf2_mddr_demo_df/final/m2s_dg0534_df/libero_project/designer/top/synthesis.fdc":18:0:18:0|Timing constraint (through [get_nets { MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORECONFIGP_0.FIC_2_APB_M_PSEL MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORECONFIGP_0.FIC_2_APB_M_PENABLE }] to [get_cells { MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORECONFIGP_0.FIC_2_APB_M_PREADY* MDDR_Demo_top_0.MDDR_Demo_0.MDDR_Demo_sb_0.CORECONFIGP_0.state[0] }]) (max delay 0.000000) was not applied to the design because none of the paths specified by the constraint exist in the design