/*
 * SETUP: Make sure we define everything we will need.
 *
 * We have create three types of pools:
 *   1) MEMPOOL - standard pools
 *   2) MALLOC_MEMPOOL - to be used by mem_malloc in mem.c
 *   3) PBUF_MEMPOOL - a mempool of pbuf's, so include space for the pbuf struct
 *
 * If the include'r doesn't require any special treatment of each of the types
 * above, then will declare #2 & #3 to be just standard mempools.
 */
#ifndef LWIP_MALLOC_MEMPOOL
/* This treats "malloc pools" just like any other pool.
   The pools are a little bigger to provide 'size' as the amount of user data. */
#define LWIP_MALLOC_MEMPOOL(num, size) LWIP_MEMPOOL(POOL_##size, num, (size + sizeof(struct memp_malloc_helper)), "MALLOC_"#size)
#define LWIP_MALLOC_MEMPOOL_START
#define LWIP_MALLOC_MEMPOOL_END
#endif /* LWIP_MALLOC_MEMPOOL */ 

#ifndef LWIP_PBUF_MEMPOOL
/* This treats "pbuf pools" just like any other pool.
 * Allocates buffers for a pbuf struct AND a payload size */
#define LWIP_PBUF_MEMPOOL(name, num, payload, desc) LWIP_MEMPOOL(name, num, (MEMP_ALIGN_SIZE(sizeof(struct pbuf)) + MEMP_ALIGN_SIZE(payload)), desc)
#endif /* LWIP_PBUF_MEMPOOL */


/*
 * A list of internal pools used by LWIP.
 *
 * LWIP_MEMPOOL(pool_name, number_elements, element_size, pool_description)
 *     creates a pool name MEMP_pool_name. description is used in stats.c
 */
#if LWIP_RAW
LWIP_MEMPOOL(RAW_PCB,        MEMP_NUM_RAW_PCB,         sizeof(struct raw_pcb),        "RAW_PCB")
#endif /* LWIP_RAW */

#if LWIP_UDP
LWIP_MEMPOOL(UDP_PCB,        MEMP_NUM_UDP_PCB,         sizeof(struct udp_pcb),        "UDP_PCB")
#endif /* LWIP_UDP */

#if LWIP_TCP
LWIP_MEMPOOL(TCP_PCB,        MEMP_NUM_TCP_PCB,         sizeof(struct tcp_pcb),        "TCP_PCB")
LWIP_MEMPOOL(TCP_PCB_LISTEN, MEMP_NUM_TCP_PCB_LISTEN,  sizeof(struct tcp_pcb_listen), "TCP_PCB_LISTEN")
LWIP_MEMPOOL(TCP_SEG,        MEMP_NUM_TCP_SEG,         sizeof(struct tcp_seg),        "TCP_SEG")
#endif /* LWIP_TCP */

#if IP_REASSEMBLY
LWIP_MEMPOOL(REASSDATA,      MEMP_NUM_REASSDATA,       sizeof(struct ip_reassdata),   "REASSDATA")
#endif /* IP_REASSEMBLY */
#if IP_FRAG && !IP_FRAG_USES_STATIC_BUF && !LWIP_NETIF_TX_SINGLE_PBUF
LWIP_MEMPOOL(FRAG_PBUF,      MEMP_NUM_FRAG_PBUF,       sizeof(struct pbuf_custom_ref),"FRAG_PBUF")
#endif /* IP_FRAG && !IP_FRAG_USES_STATIC_BUF && !LWIP_NETIF_TX_SINGLE_PBUF */

#if LWIP_NETCONN
LWIP_MEMPOOL(NETBUF,         MEMP_NUM_NETBUF,          sizeof(struct netbuf),         "NETBUF")
LWIP_MEMPOOL(NETCONN,        MEMP_NUM_NETCONN,         sizeof(struct netconn),        "NETCONN")
#endif /* LWIP_NETCONN */

#if NO_SYS==0
LWIP_MEMPOOL(TCPIP_MSG_API,  MEMP_NUM_TCPIP_MSG_API,   sizeof(struct tcpip_msg),      "TCPIP_MSG_API")
#if !LWIP_TCPIP_CORE_LOCKING_INPUT
LWIP_MEMPOOL(TCPIP_MSG_INPKT,MEMP_NUM_TCPIP_MSG_INPKT, sizeof(struct tcpip_msg),      "TCPIP_MSG_INPKT")
#endif /* !LWIP_TCPIP_CORE_LOCKING_INPUT */
#endif /* NO_SYS==0 */

#if LWIP_ARP && ARP_QUEUEING
LWIP_MEMPOOL(ARP_QUEUE,      MEMP_NUM_ARP_QUEUE,       sizeof(struct etharp_q_entry), "ARP_QUEUE")
#endif /* LWIP_ARP && ARP_QUEUEING */

#if LWIP_IGMP
LWIP_MEMPOOL(IGMP_GROUP,     MEMP_NUM_IGMP_GROUP,      sizeof(struct igmp_group),     "IGMP_GROUP")
#endif /* LWIP_IGMP */

#if (!NO_SYS || (NO_SYS && !NO_SYS_NO_TIMERS)) /* LWIP_TIMERS */
LWIP_MEMPOOL(SYS_TIMEOUT,    MEMP_NUM_SYS_TIMEOUT,     sizeof(struct sys_timeo),      "SYS_TIMEOUT")
#endif /* LWIP_TIMERS */

#if LWIP_SNMP
LWIP_MEMPOOL(SNMP_ROOTNODE,  MEMP_NUM_SNMP_ROOTNODE,   sizeof(struct mib_list_rootnode), "SNMP_ROOTNODE")
LWIP_MEMPOOL(SNMP_NODE,      MEMP_NUM_SNMP_NODE,       sizeof(struct mib_list_node),     "SNMP_NODE")
LWIP_MEMPOOL(SNMP_VARBIND,   MEMP_NUM_SNMP_VARBIND,    sizeof(struct snmp_varbind),      "SNMP_VARBIND")
LWIP_MEMPOOL(SNMP_VALUE,     MEMP_NUM_SNMP_VALUE,      SNMP_MAX_VALUE_SIZE,              "SNMP_VALUE")
#endif /* LWIP_SNMP */
#if LWIP_DNS && LWIP_SOCKET
LWIP_MEMPOOL(NETDB,          MEMP_NUM_NETDB,           NETDB_ELEM_SIZE,               "NETDB")
#endif /* LWIP_DNS && LWIP_SOCKET */
#if LWIP_DNS && DNS_LOCAL_HOSTLIST && DNS_LOCAL_HOSTLIST_IS_DYNAMIC
LWIP_MEMPOOL(LOCALHOSTLIST,  MEMP_NUM_LOCALHOSTLIST,   LOCALHOSTLIST_ELEM_SIZE,       "LOCALHOSTLIST")
#endif /* LWIP_DNS && DNS_LOCAL_HOSTLIST && DNS_LOCAL_HOSTLIST_IS_DYNAMIC */
#if PPP_SUPPORT && PPPOE_SUPPORT
LWIP_MEMPOOL(PPPOE_IF,      MEMP_NUM_PPPOE_INTERFACES, sizeof(struct pppoe_softc),    "PPPOE_IF")
#endif /* PPP_SUPPORT && PPPOE_SUPPORT */

/*
 * A list of pools of pbuf's used by LWIP.
 *
 * LWIP_PBUF_MEMPOOL(pool_name, number_elements, pbuf_payload_size, pool_description)
 *     creates a pool name MEMP_pool_name. description is used in stats.c
 *     This allocates enough space for the pbuf struct and a payload.
 *     (Example: pbuf_payload_size=0 allocates only size for the struct)
 */
LWIP_PBUF_MEMPOOL(PBUF,      MEMP_NUM_PBUF,            0,                             "PBUF_REF/ROM")
LWIP_PBUF_MEMPOOL(PBUF_POOL, PBUF_POOL_SIZE,           PBUF_POOL_BUFSIZE,             "PBUF_POOL")


/*
 * Allow for user-defined pools; this must be explicitly set in lwipopts.h
 * since the default is to NOT look for lwippools.h
 */
#if MEMP_USE_CUSTOM_POOLS
#include "lwippools.h"
#endif /* MEMP_USE_CUSTOM_POOLS */

/*
 * REQUIRED CLEANUP: Clear up so we don't get "multiply defined" error later
 * (#undef is ignored for something that is not defined)
 */
#undef LWIP_MEMPOOL
#undef LWIP_MALLOC_MEMPOOL
#undef LWIP_MALLOC_MEMPOOL_START
#undef LWIP_MALLOC_MEMPOOL_END
#undef LWIP_PBUF_MEMPOOL