@N: MF248 |Running in 64-bit mode.
@N: MF667 |Clock conversion disabled. (Command "set_option -fix_gated_and_generated_clocks 0" in the project file.)
@N: MO111 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\work\demo\fabosc_0\demo_fabosc_0_osc.v":20:7:20:16|Tristate driver XTLOSC_O2F (in view: work.demo_FABOSC_0_OSC(verilog)) on net XTLOSC_O2F (in view: work.demo_FABOSC_0_OSC(verilog)) has its enable tied to GND.
@N: MO111 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\work\demo\fabosc_0\demo_fabosc_0_osc.v":19:7:19:16|Tristate driver XTLOSC_CCC (in view: work.demo_FABOSC_0_OSC(verilog)) on net XTLOSC_CCC (in view: work.demo_FABOSC_0_OSC(verilog)) has its enable tied to GND.
@N: MO111 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\work\demo\fabosc_0\demo_fabosc_0_osc.v":18:7:18:20|Tristate driver RCOSC_1MHZ_O2F (in view: work.demo_FABOSC_0_OSC(verilog)) on net RCOSC_1MHZ_O2F (in view: work.demo_FABOSC_0_OSC(verilog)) has its enable tied to GND.
@N: MO111 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\work\demo\fabosc_0\demo_fabosc_0_osc.v":17:7:17:20|Tristate driver RCOSC_1MHZ_CCC (in view: work.demo_FABOSC_0_OSC(verilog)) on net RCOSC_1MHZ_CCC (in view: work.demo_FABOSC_0_OSC(verilog)) has its enable tied to GND.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\hdl\blink1.v":33:0:33:5|Removing sequential instance LED3 (in view: work.BLINK_LED(verilog)) of type view:PrimLib.dffre(prim) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\hdl\blink1.v":33:0:33:5|Removing sequential instance LED4 (in view: work.BLINK_LED(verilog)) of type view:PrimLib.dffre(prim) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1089:4:1089:9|Removing sequential instance demo_0.CORERESETP_0.INIT_DONE_int (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1089:4:1089:9|Removing sequential instance demo_0.CORERESETP_0.sm0_state[6] (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1613:4:1613:9|Removing sequential instance demo_0.CORERESETP_0.ddr_settled (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1646:4:1646:9|Removing sequential instance demo_0.CORERESETP_0.ddr_settled_q1 (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":963:4:963:9|Removing sequential instance demo_0.CORERESETP_0.sdif3_spll_lock_q2 (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":929:4:929:9|Removing sequential instance demo_0.CORERESETP_0.CONFIG1_DONE_q1 (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":870:4:870:9|Removing sequential instance demo_0.CORERESETP_0.sdif0_areset_n_rcosc_q1 (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":856:4:856:9|Removing sequential instance demo_0.CORERESETP_0.sm0_areset_n_rcosc (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":755:4:755:9|Removing sequential instance demo_0.CORERESETP_0.sm0_areset_n_q1 (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":755:4:755:9|Removing sequential instance demo_0.CORERESETP_0.sm0_areset_n_clk_base (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1646:4:1646:9|Removing sequential instance demo_0.CORERESETP_0.ddr_settled_clk_base (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1089:4:1089:9|Removing sequential instance demo_0.CORERESETP_0.sm0_state[5] (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1089:4:1089:9|Removing sequential instance demo_0.CORERESETP_0.sm0_state[4] (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1089:4:1089:9|Removing sequential instance demo_0.CORERESETP_0.sm0_state[3] (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1089:4:1089:9|Removing sequential instance demo_0.CORERESETP_0.sm0_state[2] (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1089:4:1089:9|Removing sequential instance demo_0.CORERESETP_0.sm0_state[1] (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: BN362 :"f:\11.8\sf2_isp_using_uart_interface_demo_df\libero\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":1089:4:1089:9|Removing sequential instance demo_0.CORERESETP_0.sm0_state[0] (in view: work.demo_top(verilog)) because it does not drive other instances.
@N: FP130 |Promoting Net demo_0_MSS_READY on CLKINT  I_38 
@N: FX1056 |Writing EDF file: F:\11.8\sf2_isp_using_uart_interface_demo_df\libero\synthesis\demo_top.edn
@N: BW103 |The default time unit for the Synopsys Constraint File (SDC or FDC) is 1ns.
@N: BW107 |Synopsys Constraint File capacitance units using default value of 1pF 
@N: MT320 |This timing report is an estimate of place and route data. For final timing results, use the FPGA vendor place and route report.
@N: MT322 |Clock constraints include only register-to-register paths associated with each individual clock.
@N: MT582 |Estimated period and frequency not reported for given clock unless the clock has at least one timing path which is not a false or a max delay path and that does not have excessive slack