@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":963:4:963:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.sdif3_spll_lock_q1 because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.CONFIG2_DONE_q1. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":946:4:946:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.CONFIG2_DONE_q1 because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.CONFIG1_DONE_q1. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":946:4:946:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.CONFIG2_DONE_clk_base because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.sdif3_spll_lock_q2. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":929:4:929:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.CONFIG1_DONE_clk_base because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.sdif3_spll_lock_q2. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":884:4:884:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.sdif1_areset_n_rcosc_q1 because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.sdif0_areset_n_rcosc_q1. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":912:4:912:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.sdif3_areset_n_rcosc_q1 because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.sdif0_areset_n_rcosc_q1. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":898:4:898:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.sdif2_areset_n_rcosc_q1 because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.sdif0_areset_n_rcosc_q1. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":912:4:912:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.sdif3_areset_n_rcosc because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.sdif2_areset_n_rcosc. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":898:4:898:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.sdif2_areset_n_rcosc because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.sdif1_areset_n_rcosc. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: BN132 :"d:\test\adaptive_fir_filter_demo\component\actel\directcore\coreresetp\7.1.100\rtl\vlog\core\coreresetp.v":884:4:884:9|Removing sequential instance Adaptive_FIR_0.CORERESETP_0.sdif1_areset_n_rcosc because it is equivalent to instance Adaptive_FIR_0.CORERESETP_0.sdif0_areset_n_rcosc. To keep the instance, apply constraint syn_preserve=1 on the instance.
@W: MT246 :"d:\test\adaptive_fir_filter_demo\component\work\adaptive_fir\ccc_0\adaptive_fir_ccc_0_fccc.v":20:36:20:43|Blackbox CCC is missing a user supplied timing model. This may have a negative effect on timing analysis and optimizations (Quality of Results) 
@W: MT420 |Found inferred clock fft_inpl_slowClock|divider_inferred_clock[2] with period 10.00ns. Please declare a user-defined clock on object "n:COREFFT_0.genblk1\.DUT_INPLACE.slowClock_0.divider[2]"
@W: MT447 :"d:/test/adaptive_fir_filter_demo/designer/adaptive_fir_top/synthesis.fdc":9:0:9:0|Timing constraint (through [get_pins { Adaptive_FIR_0.Adaptive_FIR_MSS_0.MSS_ADLIB_INST.CONFIG_PRESET_N }]) (false path) was not applied to the design because none of the paths specified by the constraint exist in the design 
@W: MT447 :"d:/test/adaptive_fir_filter_demo/designer/adaptive_fir_top/synthesis.fdc":10:0:10:0|Timing constraint (through [get_nets { Adaptive_FIR_0.CORERESETP_0.ddr_settled Adaptive_FIR_0.CORERESETP_0.count_ddr_enable Adaptive_FIR_0.CORERESETP_0.release_sdif*_core Adaptive_FIR_0.CORERESETP_0.count_sdif*_enable }]) (false path) was not applied to the design because none of the '-through' objects specified by the constraint exist in the design 
@W: MT447 :"d:/test/adaptive_fir_filter_demo/designer/adaptive_fir_top/synthesis.fdc":11:0:11:0|Timing constraint (from [get_cells { Adaptive_FIR_0.CORERESETP_0.MSS_HPMS_READY_int }] to [get_cells { Adaptive_FIR_0.CORERESETP_0.sm0_areset_n_rcosc Adaptive_FIR_0.CORERESETP_0.sm0_areset_n_rcosc_q1 }]) (false path) was not applied to the design because none of the '-to' objects specified by the constraint exist in the design 
@W: MT447 :"d:/test/adaptive_fir_filter_demo/designer/adaptive_fir_top/synthesis.fdc":12:0:12:0|Timing constraint (from [get_cells { Adaptive_FIR_0.CORERESETP_0.MSS_HPMS_READY_int Adaptive_FIR_0.CORERESETP_0.SDIF*_PERST_N_re }] to [get_cells { Adaptive_FIR_0.CORERESETP_0.sdif*_areset_n_rcosc* }]) (false path) was not applied to the design because none of the '-to' objects specified by the constraint exist in the design 
@W: MT447 :"d:/test/adaptive_fir_filter_demo/designer/adaptive_fir_top/synthesis.fdc":13:0:13:0|Timing constraint (through [get_nets { Adaptive_FIR_0.CORERESETP_0.CONFIG1_DONE Adaptive_FIR_0.CORERESETP_0.CONFIG2_DONE Adaptive_FIR_0.CORERESETP_0.SDIF*_PERST_N Adaptive_FIR_0.CORERESETP_0.SDIF*_PSEL Adaptive_FIR_0.CORERESETP_0.SDIF*_PWRITE Adaptive_FIR_0.CORERESETP_0.SDIF*_PRDATA[*] Adaptive_FIR_0.CORERESETP_0.SOFT_EXT_RESET_OUT Adaptive_FIR_0.CORERESETP_0.SOFT_RESET_F2M Adaptive_FIR_0.CORERESETP_0.SOFT_M3_RESET Adaptive_FIR_0.CORERESETP_0.SOFT_MDDR_DDR_AXI_S_CORE_RESET Adaptive_FIR_0.CORERESETP_0.SOFT_FDDR_CORE_RESET Adaptive_FIR_0.CORERESETP_0.SOFT_SDIF*_PHY_RESET Adaptive_FIR_0.CORERESETP_0.SOFT_SDIF*_CORE_RESET Adaptive_FIR_0.CORERESETP_0.SOFT_SDIF0_0_CORE_RESET Adaptive_FIR_0.CORERESETP_0.SOFT_SDIF0_1_CORE_RESET }]) (false path) was not applied to the design because none of the '-through' objects specified by the constraint exist in the design 
@W: MT447 :"d:/test/adaptive_fir_filter_demo/designer/adaptive_fir_top/synthesis.fdc":14:0:14:0|Timing constraint (through [get_pins { Adaptive_FIR_0.SYSRESET_POR.POWER_ON_RESET_N }]) (false path) was not applied to the design because none of the paths specified by the constraint exist in the design