#Build: Synplify Pro I-2013.09M-SP1 , Build 034R, Jan 17 2014
#install: C:\Microsemi\Libero_v11.3\Synopsys\synplify_I201309MSP1
#OS: Windows 7 6.1
#Hostname: W764-PINNINTIA

#Implementation: synthesis

$ Start of Compile
#Wed Oct 08 11:16:14 2014

Synopsys VHDL Compiler, version comp201309rcp1, Build 078R, built Jan 14 2014
@N: :  | Running in 64-bit mode 
Copyright (C) 1994-2013 Synopsys, Inc. This software and the associated documentation are proprietary to Synopsys, Inc. This software may only be used in accordance with the terms and conditions of a written license agreement with Synopsys, Inc.  All other use or distribution of the software is strictly prohibited.

@N:CD720 : std.vhd(146) | Setting time resolution to ns
@N: : sqmng.vhd(29) | Top entity is set to SQMNG.
Options changed - recompiling
@W:CD134 : pi_controller.vhd(155) | No such identifier, output_y_o, of proper type in current declarative region
@W:CD134 : pi_controller.vhd(156) | No such identifier, acc_out_o, of proper type in current declarative region
VHDL syntax check successful!
@N:CD231 : std1164.vhd(913) | Using onehot encoding for type mvl9plus ('U'="1000000000")
@N:CD630 : sqmng.vhd(29) | Synthesizing work.sqmng.sqmng 
@N:CD233 : sqmng.vhd(91) | Using sequential encoding for type fsm_state
@W:CG296 : sqmng.vhd(150) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(152) | Referenced variable s_reset_state is not in sensitivity list
@W:CG296 : sqmng.vhd(172) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(174) | Referenced variable s_reset_state is not in sensitivity list
@W:CG296 : sqmng.vhd(217) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(219) | Referenced variable s_reset_state is not in sensitivity list
@W:CG296 : sqmng.vhd(265) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(267) | Referenced variable s_reset_state is not in sensitivity list
@W:CG296 : sqmng.vhd(282) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(284) | Referenced variable s_reset_state is not in sensitivity list
@W:CG296 : sqmng.vhd(308) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(310) | Referenced variable s_reset_state is not in sensitivity list
@W:CG296 : sqmng.vhd(330) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(332) | Referenced variable s_reset_state is not in sensitivity list
@W:CD434 : sqmng.vhd(376) | Signal speed_error_abs in the sensitivity list is not used in the process
@W:CG296 : sqmng.vhd(401) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(406) | Referenced variable w_cl_abs is not in sensitivity list
@W:CG296 : sqmng.vhd(469) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(471) | Referenced variable s_reset_state is not in sensitivity list
@W:CG296 : sqmng.vhd(487) | Incomplete sensitivity list - assuming completeness
@W:CG290 : sqmng.vhd(489) | Referenced variable s_reset_state is not in sensitivity list
@W:CD638 : sqmng.vhd(97) | Signal s_r_angle is undriven 
@W:CD638 : sqmng.vhd(98) | Signal s_r_coef_a is undriven 
@W:CD638 : sqmng.vhd(99) | Signal s_r_coef_b is undriven 
@W:CD638 : sqmng.vhd(100) | Signal s_ca_mul_inp is undriven 
@W:CD638 : sqmng.vhd(101) | Signal s_cb_mul_out is undriven 
@W:CD638 : sqmng.vhd(102) | Signal s_ca_mul_ang is undriven 
@W:CD638 : sqmng.vhd(103) | Signal speed_o_sig is undriven 
@W:CD638 : sqmng.vhd(104) | Signal speed_prv is undriven 
@W:CD638 : sqmng.vhd(105) | Signal sub is undriven 
@W:CD638 : sqmng.vhd(107) | Signal s_mas_en_o is undriven 
@W:CD638 : sqmng.vhd(119) | Signal speed_act_i_abs is undriven 
@W:CD638 : sqmng.vhd(121) | Signal speed_ref_in_by_2 is undriven 
Post processing for work.sqmng.sqmng
@W:CL169 : sqmng.vhd(152) | Pruning register s_start_d1_2  
@W:CL111 : sqmng.vhd(219) | All reachable assignments to sub_o assign '0'; register removed by optimization
@W:CL190 : sqmng.vhd(310) | Optimizing register bit theta_scale_val_limit(17) to a constant 0
@W:CL260 : sqmng.vhd(310) | Pruning register bit 17 of theta_scale_val_limit(17 downto 0)  
@W:CL260 : sqmng.vhd(284) | Pruning register bit 17 of theta_scale_val(17 downto 0)  
@N:CL201 : sqmng.vhd(174) | Trying to extract state machine for register state
Extracted state machine for register state
State machine has 3 reachable states with original encodings of:
   00
   01
   10
@W:CL279 : sqmng.vhd(267) | Pruning register bits 35 to 22 of s_omega_scl_reg(35 downto 0)  
@W:CL279 : sqmng.vhd(219) | Pruning register bits 35 to 22 of add_c_o(35 downto 0)  
@W:CL159 : sqmng.vhd(52) | Input speed_act_i is unused
@END

At c_vhdl Exit (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 88MB peak: 89MB)

Process took 0h:00m:01s realtime, 0h:00m:01s cputime
# Wed Oct 08 11:16:14 2014

###########################################################]
Pre-mapping Report

Synopsys Generic Technology Pre-mapping, Version mapact, Build 1154R, Built Jan 20 2014 10:24:19
Copyright (C) 1994-2013, Synopsys, Inc. This software and the associated documentation are proprietary to Synopsys, Inc. This software may only be used in accordance with the terms and conditions of a written license agreement with Synopsys, Inc.  All other use or distribution of the software is strictly prohibited.
Product Version I-2013.09M-SP1 

Mapper Startup Complete (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 99MB peak: 99MB)

Reading constraint file: C:\SK1ASTSL10_3_0_multi_axis\synthesis\MC_System_top_sdc.sdc
Linked File: MC_System_top_scck.rpt
Printing clock  summary report in "C:\SK1ASTSL10_3_0_multi_axis\synthesis\MC_System_top_scck.rpt" file 
@N:MF248 :  | Running in 64-bit mode. 
@N:MF667 :  | Clock conversion disabled  

Design Input Complete (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 100MB peak: 102MB)


Mapper Initialization Complete (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 100MB peak: 102MB)


Start loading timing files (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 100MB peak: 102MB)


Finished loading timing files (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 101MB peak: 103MB)

syn_allowed_resources : blockrams=21  set on top level netlist SQMNG


Clock Summary
**************

Start                                                Requested     Requested     Clock        Clock              
Clock                                                Frequency     Period        Type         Group              
-----------------------------------------------------------------------------------------------------------------
MC_System_0/CCC_0/CCC_INST/INST_CCC_IP:GL0           50.0 MHz      20.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock          100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1        100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_0      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_1      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_2      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_3      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_4      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_5      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_6      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_7      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_8      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_9      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_10     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_11     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_12     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_13     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_14     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_15     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_16     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_17     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_18     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_19     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_20     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_21     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_22     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_23     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_24     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_25     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_26     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_27     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_28     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_29     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_30     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_31     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_32     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_33     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_34     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_35     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_36     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_37     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_38     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_39     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_40     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_41     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_42     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_43     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_44     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_45     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_46     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_47     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_48     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_49     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_50     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_51     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_52     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_53     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_54     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_55     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_56     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_57     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_58     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_59     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_60     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_61     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_62     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_63     100.0 MHz     10.000        declared     group_55_166       
MC_System_CCC_0_FCCC|GL1_net_inferred_clock          100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1        100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_0      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_1      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_2      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_3      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_4      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_5      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_6      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_7      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_8      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_9      100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_10     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_11     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_12     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_13     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_14     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_15     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_16     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_17     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_18     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_19     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_20     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_21     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_22     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_23     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_24     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_25     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_26     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_27     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_28     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_29     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_30     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_31     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_32     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_33     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_34     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_35     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_36     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_37     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_38     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_39     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_40     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_41     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_42     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_43     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_44     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_45     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_46     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_47     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_48     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_49     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_50     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_51     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_52     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_53     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_54     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_55     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_56     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_57     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_58     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_59     100.0 MHz     10.000        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_60     100.0 MHz     10.000        declared     group_55_165       
SQMNG|sys_clk_i                                      100.0 MHz     10.000        inferred     Inferred_clkgroup_0
=================================================================================================================

@W:MT530 : sqmng.vhd(489) | Found inferred clock SQMNG|sys_clk_i which controls 140 sequential elements including init_theta_s. This clock has no specified timing constraint which may adversely impact design performance. 

Finished Pre Mapping Phase.
@N:BN225 :  | Writing default property annotation file C:\SK1ASTSL10_3_0_multi_axis\synthesis\MC_System_top.sap. 
Pre-mapping successful!

At Mapper Exit (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 69MB peak: 133MB)

Process took 0h:00m:01s realtime, 0h:00m:01s cputime
# Wed Oct 08 11:16:16 2014

###########################################################]
Map & Optimize Report

Synopsys Generic Technology Mapper, Version mapact, Build 1154R, Built Jan 20 2014 10:24:19
Copyright (C) 1994-2013, Synopsys, Inc. This software and the associated documentation are proprietary to Synopsys, Inc. This software may only be used in accordance with the terms and conditions of a written license agreement with Synopsys, Inc.  All other use or distribution of the software is strictly prohibited.
Product Version I-2013.09M-SP1 

Mapper Startup Complete (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 99MB peak: 99MB)

@N:MF248 :  | Running in 64-bit mode. 
@N:MF667 :  | Clock conversion disabled  

Design Input Complete (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 99MB peak: 100MB)


Mapper Initialization Complete (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 99MB peak: 100MB)


Start loading timing files (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 100MB peak: 101MB)


Finished loading timing files (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 100MB peak: 103MB)



Starting Optimization and Mapping (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 131MB peak: 132MB)


Available hyper_sources - for debug and ip models
	None Found


Finished RTL optimizations (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 131MB peak: 132MB)

Encoding state machine state[0:2] (view:work.SQMNG(sqmng))
original code -> new code
   00 -> 00
   01 -> 01
   10 -> 10
@N:FX404 : sqmng.vhd(399) | Found addmux in view:work.SQMNG(sqmng) inst inf_abs2[17:0] from inf_abs2_a_2[17:0] 
@N:FX404 : sqmng.vhd(361) | Found addmux in view:work.SQMNG(sqmng) inst inf_abs1[17:0] from inf_abs1_a_1[17:0] 
@N:FX404 : sqmng.vhd(360) | Found addmux in view:work.SQMNG(sqmng) inst inf_abs0[17:0] from inf_abs0_a_0[17:0] 
@N:FX404 : sqmng.vhd(435) | Found addmux in view:work.SQMNG(sqmng) inst init_speedpi_o_1[18:1] from un3_init_speedpi_o[17:0] 
@N:FX404 : sqmng.vhd(460) | Found addmux in view:work.SQMNG(sqmng) inst init_iqpi_o[17:0] from un4_init_iqpi_o[17:0] 

Finished factoring (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 133MB peak: 133MB)


Finished gated-clock and generated-clock conversion (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 132MB peak: 133MB)


Finished generic timing optimizations - Pass 1 (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 132MB peak: 133MB)


Starting Early Timing Optimization (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 133MB peak: 133MB)


Finished Early Timing Optimization (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 133MB peak: 133MB)


Finished generic timing optimizations - Pass 2 (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 132MB peak: 133MB)


Finished preparing to map (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 133MB peak: 134MB)


Finished technology mapping (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 133MB peak: 134MB)

Pass		 CPU time		Worst Slack		Luts / Registers
------------------------------------------------------------
Pass		 CPU time		Worst Slack		Luts / Registers
------------------------------------------------------------
------------------------------------------------------------

@N:FP130 :  | Promoting Net reset_i_c on CLKINT  I_172  
@N:FP130 :  | Promoting Net sys_clk_i_c on CLKINT  I_173  

Added 0 Buffers
Added 0 Cells via replication
	Added 0 Sequential Cells via replication
	Added 0 Combinational Cells via replication

Finished technology timing optimizations and critical path resynthesis (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 133MB peak: 134MB)


Finished restoring hierarchy (Real Time elapsed 0h:00m:00s; CPU Time elapsed 0h:00m:00s; Memory used current: 133MB peak: 134MB)



#### START OF CLOCK OPTIMIZATION REPORT #####[

Clock optimization not enabled
1 non-gated/non-generated clock tree(s) driving 139 clock pin(s) of sequential element(s)
0 gated/generated clock tree(s) driving 0 clock pin(s) of sequential element(s)
0 instances converted, 0 sequential instances remain driven by gated/generated clocks

=========================== Non-Gated/Non-Generated Clocks ============================
Clock Tree ID     Driving Element     Drive Element Type     Fanout     Sample Instance
---------------------------------------------------------------------------------------
ClockId0001        sys_clk_i           port                   139        s_start_d      
=======================================================================================


##### END OF CLOCK OPTIMIZATION REPORT ######]

Writing Analyst data base C:\SK1ASTSL10_3_0_multi_axis\synthesis\MC_System_top.srm

Finished Writing Netlist Databases (Real Time elapsed 0h:00m:01s; CPU Time elapsed 0h:00m:00s; Memory used current: 132MB peak: 134MB)

Writing EDIF Netlist and constraint files
@W:MT558 : mc_system_top_sdc.sdc(5) | Unable to locate source for clock MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_60. Clock will not be forward annotated
@W:MT558 : mc_system_top_sdc.sdc(6) | Unable to locate source for clock MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_63. Clock will not be forward annotated
@N:BW103 :  | Synopsys Constraint File time units using default value of 1ns  
@N:BW107 :  | Synopsys Constraint File capacitance units using default value of 1pF  
@W:BW152 : mc_system_top_sdc.sdc(165) | Cannot forward annotate set_clock_groups command because clock MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_60 is not referenced
@W:BW152 : mc_system_top_sdc.sdc(166) | Cannot forward annotate set_clock_groups command because clock MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_63 is not referenced
I-2013.09M-SP1 

Finished Writing EDIF Netlist and constraint files (Real Time elapsed 0h:00m:01s; CPU Time elapsed 0h:00m:01s; Memory used current: 133MB peak: 135MB)

@W:MT420 :  | Found inferred clock SQMNG|sys_clk_i with period 10.00ns. Please declare a user-defined clock on object "p:sys_clk_i" 



##### START OF TIMING REPORT #####[
# Timing Report written on Wed Oct 08 11:16:18 2014
#


Top view:               SQMNG
Requested Frequency:    50.0 MHz
Wire load mode:         top
Paths requested:        5
Constraint File(s):    C:\SK1ASTSL10_3_0_multi_axis\synthesis\MC_System_top_sdc.sdc
                       
@N:MT320 :  | Timing report estimates place and route data. Please look at the place and route timing report for final timing. 

@N:MT322 :  | Clock constraints cover only FF-to-FF paths associated with the clock. 



Performance Summary 
*******************


Worst slack in design: 7.033

                                                     Requested     Estimated     Requested     Estimated               Clock        Clock              
Starting Clock                                       Frequency     Frequency     Period        Period        Slack     Type         Group              
-------------------------------------------------------------------------------------------------------------------------------------------------------
MC_System_0/CCC_0/CCC_INST/INST_CCC_IP:GL0           50.0 MHz      NA            20.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock          100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1        100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_0      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_1      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_2      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_3      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_4      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_5      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_6      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_7      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_8      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_9      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_10     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_11     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_12     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_13     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_14     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_15     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_16     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_17     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_18     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_19     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_20     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_21     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_22     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_23     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_24     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_25     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_26     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_27     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_28     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_29     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_30     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_31     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_32     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_33     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_34     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_35     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_36     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_37     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_38     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_39     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_40     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_41     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_42     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_43     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_44     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_45     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_46     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_47     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_48     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_49     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_50     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_51     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_52     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_53     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_54     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_55     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_56     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_57     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_58     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_59     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_60     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_61     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_62     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_63     100.0 MHz     NA            10.000        NA            NA        declared     group_55_166       
MC_System_CCC_0_FCCC|GL1_net_inferred_clock          100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1        100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_0      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_1      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_2      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_3      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_4      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_5      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_6      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_7      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_8      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_9      100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_10     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_11     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_12     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_13     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_14     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_15     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_16     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_17     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_18     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_19     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_20     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_21     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_22     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_23     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_24     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_25     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_26     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_27     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_28     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_29     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_30     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_31     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_32     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_33     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_34     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_35     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_36     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_37     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_38     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_39     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_40     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_41     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_42     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_43     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_44     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_45     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_46     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_47     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_48     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_49     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_50     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_51     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_52     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_53     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_54     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_55     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_56     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_57     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_58     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_59     100.0 MHz     NA            10.000        NA            NA        virtual      default_clkgroup   
MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_60     100.0 MHz     NA            10.000        NA            NA        declared     group_55_165       
SQMNG|sys_clk_i                                      100.0 MHz     337.0 MHz     10.000        2.967         7.033     inferred     Inferred_clkgroup_0
=======================================================================================================================================================
@W:MT548 : mc_system_top_sdc.sdc(5) | Source for clock MC_System_CCC_0_FCCC|GL1_net_inferred_clock_1_60 not found in netlist
@W:MT548 : mc_system_top_sdc.sdc(6) | Source for clock MC_System_CCC_0_FCCC|GL0_net_inferred_clock_1_63 not found in netlist





Clock Relationships
*******************

Clocks                            |    rise  to  rise   |    fall  to  fall   |    rise  to  fall   |    fall  to  rise 
------------------------------------------------------------------------------------------------------------------------
Starting         Ending           |  constraint  slack  |  constraint  slack  |  constraint  slack  |  constraint  slack
------------------------------------------------------------------------------------------------------------------------
SQMNG|sys_clk_i  SQMNG|sys_clk_i  |  10.000      7.033  |  No paths    -      |  No paths    -      |  No paths    -    
========================================================================================================================
 Note: 'No paths' indicates there are no paths in the design for that pair of clock edges.
       'Diff grp' indicates that paths exist but the starting clock and ending clock are in different clock groups.



Interface Information 
*********************

No IO constraint found



====================================
Detailed Report for Clock: SQMNG|sys_clk_i
====================================



Starting Points with Worst Slack
********************************

                             Starting                                                          Arrival          
Instance                     Reference           Type     Pin     Net                          Time        Slack
                             Clock                                                                              
----------------------------------------------------------------------------------------------------------------
state[0]                     SQMNG|sys_clk_i     SLE      Q       state[0]                     0.094       7.033
state[1]                     SQMNG|sys_clk_i     SLE      Q       state[1]                     0.094       7.524
s_start_d                    SQMNG|sys_clk_i     SLE      Q       s_start_d                    0.094       8.080
init_theta_s                 SQMNG|sys_clk_i     SLE      Q       init_theta_s                 0.094       8.141
theta_scale_val_limit[4]     SQMNG|sys_clk_i     SLE      Q       theta_scale_val_limit[4]     0.076       8.405
theta_scale_val_limit[5]     SQMNG|sys_clk_i     SLE      Q       theta_scale_val_limit[5]     0.076       8.405
theta_scale_val_limit[6]     SQMNG|sys_clk_i     SLE      Q       theta_scale_val_limit[6]     0.076       8.405
theta_scale_val_limit[7]     SQMNG|sys_clk_i     SLE      Q       theta_scale_val_limit[7]     0.076       8.405
theta_scale_val_limit[8]     SQMNG|sys_clk_i     SLE      Q       theta_scale_val_limit[8]     0.076       8.405
theta_scale_val_limit[9]     SQMNG|sys_clk_i     SLE      Q       theta_scale_val_limit[9]     0.076       8.405
================================================================================================================


Ending Points with Worst Slack
******************************

                       Starting                                                   Required          
Instance               Reference           Type     Pin     Net                   Time         Slack
                       Clock                                                                        
----------------------------------------------------------------------------------------------------
s_omega_scl_reg[0]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[1]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[2]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[3]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[4]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[5]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[6]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[7]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[8]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
s_omega_scl_reg[9]     SQMNG|sys_clk_i     SLE      EN      mas_en_o_0_sqmuxa     9.707        7.033
====================================================================================================



Worst Path Information
View Worst Path in Analyst
***********************


Path information for path number 1: 
      Requested Period:                      10.000
    - Setup time:                            0.293
    + Clock delay at ending point:           0.000 (ideal)
    = Required time:                         9.707

    - Propagation time:                      2.674
    - Clock delay at starting point:         0.000 (ideal)
    = Slack (critical) :                     7.033

    Number of logic level(s):                1
    Starting point:                          state[0] / Q
    Ending point:                            s_omega_scl_reg[0] / EN
    The start point is clocked by            SQMNG|sys_clk_i [rising] on pin CLK
    The end   point is clocked by            SQMNG|sys_clk_i [rising] on pin CLK

Instance / Net                      Pin      Pin               Arrival     No. of    
Name                       Type     Name     Dir     Delay     Time        Fan Out(s)
-------------------------------------------------------------------------------------
state[0]                   SLE      Q        Out     0.094     0.094       -         
state[0]                   Net      -        -       1.518     -           62        
mas_en_o_0_sqmuxa_0_a3     CFG2     A        In      -         1.612       -         
mas_en_o_0_sqmuxa_0_a3     CFG2     Y        Out     0.076     1.688       -         
mas_en_o_0_sqmuxa          Net      -        -       0.986     -           22        
s_omega_scl_reg[0]         SLE      EN       In      -         2.674       -         
=====================================================================================
Total path delay (propagation time + setup) of 2.967 is 0.463(15.6%) logic and 2.504(84.4%) route.
Path delay compensated for clock skew. Clock skew is added to clock-to-out value, and is subtracted from setup time value



##### END OF TIMING REPORT #####]

---------------------------------------
Resource Usage Report for SQMNG 

Mapping to part: m2s010fbga484-1
Cell usage:
CLKINT          2 uses
CFG2           32 uses
CFG3           37 uses
CFG4           43 uses

Carry primitives used for arithmetic functions:
ARI1           177 uses


Sequential Cells: 
SLE            139 uses

DSP Blocks:    0

I/O ports: 356
I/O primitives: 338
INBUF          187 uses
OUTBUF         151 uses


Global Clock Buffers: 2


Total LUTs:    289

Mapper successful!

At Mapper Exit (Real Time elapsed 0h:00m:01s; CPU Time elapsed 0h:00m:01s; Memory used current: 50MB peak: 135MB)

Process took 0h:00m:01s realtime, 0h:00m:01s cputime
# Wed Oct 08 11:16:18 2014

###########################################################]