/*
    FreeRTOS V6.0.1 - Copyright (C) 2009 Real Time Engineers Ltd.

    ***************************************************************************
    *                                                                         *
    * If you are:                                                             *
    *                                                                         *
    *    + New to FreeRTOS,                                                   *
    *    + Wanting to learn FreeRTOS or multitasking in general quickly       *
    *    + Looking for basic training,                                        *
    *    + Wanting to improve your FreeRTOS skills and productivity           *
    *                                                                         *
    * then take a look at the FreeRTOS eBook                                  *
    *                                                                         *
    *        "Using the FreeRTOS Real Time Kernel - a Practical Guide"        *
    *                  http://www.FreeRTOS.org/Documentation                  *
    *                                                                         *
    * A pdf reference manual is also available.  Both are usually delivered   *
    * to your inbox within 20 minutes to two hours when purchased between 8am *
    * and 8pm GMT (although please allow up to 24 hours in case of            *
    * exceptional circumstances).  Thank you for your support!                *
    *                                                                         *
    ***************************************************************************

    This file is part of the FreeRTOS distribution.

    FreeRTOS is free software; you can redistribute it and/or modify it under
    the terms of the GNU General Public License (version 2) as published by the
    Free Software Foundation AND MODIFIED BY the FreeRTOS exception.
    ***NOTE*** The exception to the GPL is included to allow you to distribute
    a combined work that includes FreeRTOS without being obliged to provide the
    source code for proprietary components outside of the FreeRTOS kernel.
    FreeRTOS is distributed in the hope that it will be useful, but WITHOUT
    ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
    FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License for
    more details. You should have received a copy of the GNU General Public
    License and the FreeRTOS license exception along with FreeRTOS; if not it
    can be viewed here: http://www.freertos.org/a00114.html and also obtained
    by writing to Richard Barry, contact details for whom are available on the
    FreeRTOS WEB site.

    1 tab == 4 spaces!

    http://www.FreeRTOS.org - Documentation, latest information, license and
    contact details.

    http://www.SafeRTOS.com - A version that is certified for use in safety
    critical systems.

    http://www.OpenRTOS.com - Commercial support, development, porting,
    licensing and training services.
*/

#ifndef FREERTOS_CONFIG_H
#define FREERTOS_CONFIG_H

/* Library includes. */
/*#include "stm32f10x_lib.h"*/

/*-----------------------------------------------------------
 * Application specific definitions.
 *
 * These definitions should be adjusted for your particular hardware and
 * application requirements.
 *
 * THESE PARAMETERS ARE DESCRIBED WITHIN THE 'CONFIGURATION' SECTION OF THE
 * FreeRTOS API DOCUMENTATION AVAILABLE ON THE FreeRTOS.org WEB SITE.
 *
 * See http://www.freertos.org/a00110.html.
 *----------------------------------------------------------*/

#define configUSE_PREEMPTION		1
#define configUSE_IDLE_HOOK			0
#define configUSE_TICK_HOOK			0
/* F1 is running at 40MHz = 0.025 us clk
1/0.025  --- 1 millisec = 40000.
10 ms = 400000.
*/
#define configCPU_CLOCK_HZ			( ( unsigned long ) 20000000 )
#define configTICK_RATE_HZ			( ( portTickType ) 100 )
#define configMAX_PRIORITIES		( ( unsigned portBASE_TYPE ) 5 )
#define configMINIMAL_STACK_SIZE	( ( unsigned short ) 512 )
#define configTOTAL_HEAP_SIZE		( ( size_t ) ( 17 * 1024 ) )
#define configMAX_TASK_NAME_LEN		( 16 )
#define configUSE_TRACE_FACILITY	0
#define configUSE_16_BIT_TICKS		1
#define configIDLE_SHOULD_YIELD		1
#define configUSE_MUTEXES			0

#define configUSE_COUNTING_SEMAPHORES 1

/* Co-routine definitions. */
#define configUSE_CO_ROUTINES 		1
#define configMAX_CO_ROUTINE_PRIORITIES ( 2 )

/* Set the following definitions to 1 to include the API function, or zero
to exclude the API function. */

#define INCLUDE_vTaskPrioritySet		1
#define INCLUDE_uxTaskPriorityGet		1
#define INCLUDE_vTaskDelete				1
#define INCLUDE_vTaskCleanUpResources	1
#define INCLUDE_vTaskSuspend			1
#define INCLUDE_vTaskDelayUntil			1
#define INCLUDE_vTaskDelay				1

#define INCLUDE_vResumeFromISR              1
#define INCLUDE_uxTaskGetStackHighWaterMark         1


/* This is the raw value as per the Cortex-M3 NVIC.  Values can be 255
(lowest) to 0 (1?) (highest). */
#define configKERNEL_INTERRUPT_PRIORITY 		255
//#define configKERNEL_INTERRUPT_PRIORITY 		149
#define configMAX_SYSCALL_INTERRUPT_PRIORITY 	191 /* equivalent to 0xb0, or priority 11. */


/* This is the value being used as per the ST library which permits 16
priority values, 0 to 15.  This must correspond to the
configKERNEL_INTERRUPT_PRIORITY setting.  Here 15 corresponds to the lowest
NVIC value of 255. */
//#define configLIBRARY_KERNEL_INTERRUPT_PRIORITY	15

#endif /* FREERTOS_CONFIG_H */