#include "ff.h"
#include "integer.h"
#include "mss_uart.h"
#include "mss_rtc.h"

unsigned long year_in_reference;
unsigned long month_in_reference;
unsigned long days_in_reference;
unsigned long hours_in_reference;
unsigned long mins_in_reference;
unsigned long secs_in_reference;


int xatoi (			/* 0:Failed, 1:Successful */
	char **str,		/* Pointer to pointer to the string */
	long *res		/* Pointer to the valiable to store the value */
)
{
	unsigned long val;
	unsigned char c, r, s = 0;


	*res = 0;

	while ((c = **str) == ' ') (*str)++;	/* Skip leading spaces */

	if (c == '-') {		/* negative? */
		s = 1;
		c = *(++(*str));
	}

	if (c == '0') {
		c = *(++(*str));
		switch (c) {
		case 'x':		/* hexdecimal */
			r = 16; c = *(++(*str));
			break;
		case 'b':		/* binary */
			r = 2; c = *(++(*str));
			break;
		default:
			if (c <= ' ') return 1;	/* single zero */
			if (c < '0' || c > '9') return 0;	/* invalid char */
			r = 8;		/* octal */
		}
	} else {
		if (c < '0' || c > '9') return 0;	/* EOL or invalid char */
		r = 10;			/* decimal */
	}

	val = 0;
	while (c > ' ') {
		if (c >= 'a') c -= 0x20;
		c -= '0';
		if (c >= 17) {
			c -= 7;
			if (c <= 9) return 0;	/* invalid char */
		}
		if (c >= r) return 0;		/* invalid char for current radix */
		val = val * r + c;
		c = *(++(*str));
	}
	if (s) val = 0 - val;			/* apply sign if needed */

	*res = val;
	return 1;
}


/*----------------------------------------------*/
/* Get a line from the input                    */
/*----------------------------------------------*/

int get_line (		/* 0:End of stream, 1:A line arrived */
	char* buff,		/* Pointer to the buffer */
	int len			/* Buffer length */
)
{
	int rv, i, rx_size, size = 0;
    uint8_t rx_buff[1]={0};
    
	rv = i = 0;
//	for (;;) {
//		c = xfunc_in();				/* Get a char from the incoming stream */
		  while(*rx_buff!= '\n')
		  {
			rx_size = MSS_UART_get_rx ( &g_mss_uart0, rx_buff, sizeof(rx_buff) );
			
			if( rx_size > 0 )
			{
				buff[size] = *rx_buff;
				size++;
			}	
		  }
#if 0
		while(! MSS_UART_get_rx ( &g_mss_uart0, &c, 1 ))
			;
		if (!c) return 0;			/* End of stream? */
		if (c == '\r') 
			break;		/* End of line? */
		if (c == '\b' && i) {		/* Back space? */
			i--;
			xputc(c);
			continue;
		}
		if (c >= ' ' && i < len - 1) {	/* Visible chars */
			buff[i++] = c;
//			xputc(c);
		}
	}
#endif	
	buff[size] = 0;	/* Terminate with zero */
//	xputc('\n');
	return 1;
}


/*---------------------------------------------------------*/
/* User Provided Timer Function for FatFs module           */
/*---------------------------------------------------------*/
/* This is a real time clock service to be called from     */
/* FatFs module. Any valid time must be returned even if   */
/* the system does not support a real time clock.          */
int isLeapYear(int year)
{
	if(year%400 ==0 || (year%100 != 0 && year%4 == 0))
	{
	    return 1;
	}
	else
	{
	    return 0;
    }
}

int set_fattime()
{
    unsigned int num_of_days_in_non_leap_year[]={31,28,31,30,31,30,31,31,30,31,30,31};
    unsigned int num_of_days_in_leap_year[]={31,29,31,30,31,30,31,31,30,31,30,31};
    unsigned long tm_sec = 0, tm_min = 0, tm_hour = 0, tm_yday = 0, tm_year = 0;
    unsigned long month;
    unsigned long noOfLeapYears;
    long p1;
    char * ptr;
    
    char Line[80];
    
    int isLeapFlag = 0, ii;
    //uint64_t rtcCount = 0;
    unsigned long time_in_sec =0;

    iprintf("Enter the RTC time in: <M D YYYY Hr Min > Format\n\r");

	get_line(Line, sizeof(Line));

	ptr = Line;

	if (xatoi(&ptr, &p1)) {
        
		month = p1;
        if( xatoi(&ptr, &p1))
		    tm_yday = p1;
		else
		{
				iprintf(" Please enter the correct time for RTC \n\r");
				set_fattime();
		}

        if( xatoi(&ptr, &p1))
		  tm_year = p1;
    	else
    	{
    		iprintf(" Please enter the correct time for RTC \n");
    		set_fattime();
    	}

        if( (month >=1)&&(month<=12) &&
        	((tm_yday>= 1) && (tm_yday <=31)) &&
        	((tm_year>= 1980) && (tm_year<=2080)))
        {
        
        
        isLeapFlag = isLeapYear(tm_year);
	    tm_year -= 1980;				
		//rtcYear = p1 - 1900;
        noOfLeapYears = tm_year/4;
        
	    //xatoi(&ptr, &p1);
        //month = p1;

        for( ii = 0; ii < (month -1); ii++ )
	  	{
        	if( isLeapFlag )
	   	    {
	            tm_yday += num_of_days_in_leap_year[ii];
	   	    }
	   	    else
	   	    {
	   	    	tm_yday += num_of_days_in_non_leap_year[ii];
	   	    }
	  	}
		
		//rtcMon = p1;
		//xatoi(&ptr, &p1);
		//tm_yday += p1;
		//Adding Leap Year Days
		tm_yday += noOfLeapYears;
		//Totoal No of Dyas
		tm_yday += tm_year * 365;

		// rtcMday = p1;
		if(xatoi(&ptr, &p1))
		   tm_hour = p1;
		else
		{
			iprintf(" Please enter the correct time for RTC \n");
			set_fattime();
		}

		//rtcHour = p1;
		if( xatoi(&ptr, &p1))
		   tm_min = p1;
		else
		{
			iprintf(" Please enter the correct time for RTC \n");
			set_fattime();
		}

		tm_sec = 0;
		
		time_in_sec = tm_sec + tm_min*60 + tm_hour*3600 + tm_yday*86400;
		MSS_RTC_set_seconds_count(time_in_sec);
        }
        else
		{
			iprintf(" Please enter the correct time for RTC \n");
			set_fattime();
		}

	}
	else
	{
		iprintf(" Please enter the correct time for RTC \n");
		set_fattime();
	}
		//printf("RTC Secs SET  %d\n", time_in_sec);
}

uint32_t get_fattime ()
{
	uint32_t tmr, ii;
    unsigned int num_of_days_in_year[]={31,28,31,30,31,30,31,31,30,31,30,31};
//    unsigned int num_of_days_in_leap_year[]={31,29,31,30,31,30,31,31,30,31,30,31};
	uint32_t  noOfYears, noOfMonths, noOfDays,noOfHours, noOfMins, noOfSecs, residue;


	//set_imask_ccr(1);
	//tmr =	(uint32_t)MSS_RTC_get_rtc_count();
	tmr =	(uint32_t)MSS_RTC_get_seconds_count();
	

	//printf("RTC Secs Get %d\n", tmr);
	
    /* Calculating the Number of Days from the Seconds Value */
    noOfDays = (tmr / 86400);
    residue = (tmr % 86400);

	    /* Calculating the Number of Hours */
	    noOfHours = (residue / 3600);
	    noOfSecs = (residue % 3600);

	    /* Calculating the Number of Minutes */
	    noOfMins = (noOfSecs / 60);
	    noOfSecs = (noOfSecs % 60);


	noOfYears = noOfDays /365 ;
	noOfDays = ((noOfDays % 365) - (noOfYears / 4));
	
	if ((noOfYears % 4) == 0)
	{
		num_of_days_in_year[1] += 1;
	}
	/*Months */
	for (ii= 0; ii < 12; ii++)
	{
        if (noOfDays > num_of_days_in_year[ii] )
        {
        	noOfDays -= num_of_days_in_year[ii];
        }
        else
        {

        	break;
        }
        
	}
	noOfMonths = ++ii;
	tmr =    ( ((noOfYears) << 25 ) |
	           ((noOfMonths) << 21) |
	           ((noOfDays) << 16) |
	           ((noOfHours) << 11) |
	           ((noOfMins) << 5) |
	           ((noOfSecs) >> 1));

	return tmr;
}