This section
provides information on the PFSOC_CONTROL_SCB Module Instance. Each of the
module registers is described below.
Register Lock Bits
can prevent the XCVR configuration registers from being overwritten by hosts
that have access to these registers. The lock bits can be managed using the
Configure Register Lock Bits utility in the Libero SoC. The following registers
can be locked.
· PFSOC_CONTROL_SCB_SOFT_RESET
· PFSOC_CONTROL_SCB_TVS_CONTROL
· PFSOC_CONTROL_SCB_TVS_TRIGGER
· PFSOC_CONTROL_SCB_VDETECTOR
Return to mpfs_ioscb_memmap_dri
|
Register Name |
Type |
Register Width (Bits)
|
Register Reset |
Address Offset |
Physical Address |
|
RW |
32 |
0x0710 0100 |
0x00 |
0x0702 0000 |
|
|
RW |
32 |
0x0000 0007 |
0x04 |
0x0702 0004 |
|
|
RW |
32 |
0x0000 0000 |
0x08 |
0x0702 0008 |
|
|
RW |
32 |
0x0000 0000 |
0x0C |
0x0702 000C |
|
|
RW |
32 |
0x0000 0000 |
0x10 |
0x0702 0010 |
|
|
RW |
32 |
0x0000 0000 |
0x14 |
0x0702 0014 |
|
|
RO |
32 |
0x0000 0000 |
0x18 |
0x0702 0018 |
|
|
RW |
32 |
0x0000 0000 |
0x1C |
0x0702 001C |
|
|
RW |
32 |
0x0000 0000 |
0x20 |
0x0702 0020 |
|
|
RO |
32 |
0x0000 0000 |
0x24 |
0x0702 0024 |
|
|
RO |
32 |
0x0000 0000 |
0x28 |
0x0702 0028 |
|
|
RW |
32 |
0x0000 0000 |
0x2C |
0x0702 002C |
|
|
RW |
32 |
0x0000 4040 |
0x30 |
0x0702 0030 |
|
|
RW |
32 |
0x0000 0D10 |
0x34 |
0x0702 0034 |
|
|
RW |
32 |
0x0000 1010 |
0x38 |
0x0702 0038 |
|
|
RW |
32 |
0x0000 0010 |
0x3C |
0x0702 003C |
|
|
RW |
32 |
0x0000 0000 |
0x40 |
0x0702 0040 |
|
|
RW |
32 |
0x0000 0000 |
0x50 |
0x0702 0050 |
|
|
RO |
32 |
0x0000 0000 |
0x54 |
0x0702 0054 |
|
|
RW |
32 |
0x0000 0000 |
0x58 |
0x0702 0058 |
|
|
RW |
32 |
0x0000 0000 |
0x5C |
0x0702 005C |
|
|
RW |
32 |
0x0000 0000 |
0x60 |
0x0702 0060 |
|
Address offset |
0x00 |
||
|
Physical address |
0x0702 0000 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
System Reset Register. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
|
31:16 |
BLOCKID |
This returns the block type and chip location. |
RO |
0x0710 |
|
|
|
|
Read 0x0000 |
[block_address_PFSOC_CONTROL_SCB] Indicates the Block chip
location. |
|
|
|
15:9 |
Reserved |
|
RO |
0x00 |
|
|
8 |
PERIPH |
This asserts the functional reset of the block. It is
asserted and left asserted at power up. |
WO |
1 |
|
|
|
|
Write 0 |
[scb_periph_not_in_soft_reset_PFSOC_CONTROL_SCB] Resets
not asserted |
|
|
|
|
|
Write 1 |
[scb_periph_reset_PFSOC_CONTROL_SCB] SCB registers reset
pulsed |
|
|
|
7:2 |
Reserved |
|
RO |
0x00 |
|
|
1 |
V_MAP |
This when asserted resets all the register bits apart from
the non-volatile registers |
WO |
0 |
|
|
|
|
Write 0 |
[scb_v_regs_not_in_soft_reset_PFSOC_CONTROL_SCB] Resets
not asserted |
|
|
|
|
|
Write 1 |
[scb_v_regs_reset_PFSOC_CONTROL_SCB] SCB Volitile reset
i.e RW-P registers are reset |
|
|
|
0 |
NV_MAP |
This when asserted resets all the non-volatile register
bits e.g. RW-P bits |
WO |
0 |
|
|
|
|
Write 0 |
[scb_nv_regs_not_in_soft_reset_PFSOC_CONTROL_SCB] Resets
not asserted |
|
|
|
|
|
Write 1 |
[scb_nv_regs_reset_PFSOC_CONTROL_SCB] SCB Non-Volitile
reset i.e RW-X registers are reset |
|
|
|
Address offset |
0x04 |
||
|
Physical address |
0x0702 0004 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:3 |
Reserved |
|
RO |
0x0000 0000 |
|
2 |
enable_2p5 |
|
RW |
1 |
|
1 |
enable_1p8 |
|
RW |
1 |
|
0 |
enable_1p05 |
|
RW |
1 |
|
Address offset |
0x08 |
||
|
Physical address |
0x0702 0008 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:22 |
Reserved |
|
RO |
0x000 |
|
21 |
over_temp |
Indicates temperature is below the set value |
RO |
0 |
|
20 |
under_temp |
Indicates temperature is over the set value |
RO |
0 |
|
19:16 |
valid |
Indicates Channel value is valid, once set will stay set
until channel is disabled. |
RO |
0x0 |
|
15:8 |
rate |
Time to wait once all enabled channels converted |
RW |
0x00 |
|
7 |
Reserved |
|
RO |
0 |
|
6 |
running |
FSM is doing a conversion |
RO |
0 |
|
5 |
poweroff |
Between conversions power the TVS down, adds 50us to the
overall conversion rate |
RW |
0 |
|
4 |
abort |
Abort operation, and restart if enables are nonzero |
RW |
0 |
|
3:0 |
enable |
Enables each of the channels. |
RW |
0x0 |
|
Address offset |
0x0C |
||
|
Physical address |
0x0702 000C |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
sign |
Sets the y=ax2+bx+c Temperature correction |
RW |
0 |
|
30:20 |
integ |
Sets the y=ax2+bx+c Temperature correction |
RW |
0x000 |
|
19:0 |
fract |
Sets the y=ax2+bx+c Temperature correction |
RW |
0x0 0000 |
|
Address offset |
0x10 |
||
|
Physical address |
0x0702 0010 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
sign |
Sets the y=ax2+bx+c Temperature correction |
RW |
0 |
|
30:20 |
integ |
Sets the y=ax2+bx+c Temperature correction |
RW |
0x000 |
|
19:0 |
fract |
Sets the y=ax2+bx+c Temperature correction |
RW |
0x0 0000 |
|
Address offset |
0x14 |
||
|
Physical address |
0x0702 0014 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
sign |
Sets the y=ax2+bx+c Temperature correction, only applies
to 1.05 conversion |
RW |
0 |
|
30:20 |
integ |
Sets the y=ax2+bx+c Temperature correction, only applies
to 1.05 conversion |
RW |
0x000 |
|
19:15 |
fract |
Sets the y=ax2+bx+c Temperature correction, only applies
to 1.05 conversion |
RW |
0x00 |
|
14:0 |
Reserved |
Sets the y=ax2+bx+c
Temperature correction, only applies to 1.05 conversion |
RO |
0x0000 |
|
Address offset |
0x18 |
||
|
Physical address |
0x0702 0018 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
sign |
Sets the y=ax2+bx+c Voltage correction |
RO |
0 |
|
30:20 |
integ |
Sets the y=ax2+bx+c Voltage correction |
RO |
0x000 |
|
19:0 |
fract |
Sets the y=ax2+bx+c Voltage correction |
RO |
0x0 0000 |
|
Address offset |
0x1C |
||
|
Physical address |
0x0702 001C |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
sign |
Sets the y=ax2+bx+c Voltage correction |
RW |
0 |
|
30:20 |
integ |
Sets the y=ax2+bx+c Voltage correction |
RW |
0x000 |
|
19:0 |
fract |
Sets the y=ax2+bx+c Voltage correction |
RW |
0x0 0000 |
|
Address offset |
0x20 |
||
|
Physical address |
0x0702 0020 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
sign |
Sets the y=ax2+bx+c Voltage correction |
RW |
0 |
|
30:20 |
integ |
Sets the y=ax2+bx+c Voltage correction |
RW |
0x000 |
|
19:15 |
fract |
Sets the y=ax2+bx+c Voltage correction |
RW |
0x00 |
|
14:0 |
Reserved |
Sets the y=ax2+bx+c
Voltage correction |
RO |
0x0000 |
|
Address offset |
0x24 |
||
|
Physical address |
0x0702 0024 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:16 |
volt1p8 |
|
RO |
0x0000 |
|
15:0 |
volt1p05 |
|
RO |
0x0000 |
|
Address offset |
0x28 |
||
|
Physical address |
0x0702 0028 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:16 |
temp |
|
RO |
0x0000 |
|
15:0 |
volt2p5 |
|
RO |
0x0000 |
|
Address offset |
0x2C |
||
|
Physical address |
0x0702 002C |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
temperature trigger levels |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:16 |
HIGH |
|
RW |
0x0000 |
|
15:0 |
LOW |
|
RW |
0x0000 |
|
Address offset |
0x30 |
||
|
Physical address |
0x0702 0030 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:15 |
Reserved |
|
RO |
0x0 0000 |
|
14:8 |
progl |
|
RW |
0x40 |
|
7 |
Reserved |
|
RO |
0 |
|
6:0 |
progh |
|
RW |
0x40 |
|
Address offset |
0x34 |
||
|
Physical address |
0x0702 0034 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:13 |
Reserved |
|
RO |
0x0 0000 |
|
12:8 |
progl |
|
RW |
0x0D |
|
7:5 |
Reserved |
|
RO |
0x0 |
|
4:0 |
progh |
|
RW |
0x10 |
|
Address offset |
0x38 |
||
|
Physical address |
0x0702 0038 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:13 |
Reserved |
|
RO |
0x0 0000 |
|
12:8 |
progl |
|
RW |
0x10 |
|
7:5 |
Reserved |
|
RO |
0x0 |
|
4:0 |
progh |
|
RW |
0x10 |
|
Address offset |
0x3C |
||
|
Physical address |
0x0702 003C |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:5 |
Reserved |
|
RO |
0x000 0000 |
|
4 |
deltavbe |
|
RW |
1 |
|
3:0 |
caltrim |
|
RW |
0x0 |
|
Address offset |
0x40 |
||
|
Physical address |
0x0702 0040 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:10 |
Reserved |
|
RO |
0x00 0000 |
|
9:8 |
rate |
|
RW |
0x0 |
|
7:6 |
width |
|
RW |
0x0 |
|
5:4 |
threshold |
|
RW |
0x0 |
|
3:2 |
negtrim |
|
RW |
0x0 |
|
1:0 |
postrim |
|
RW |
0x0 |
|
Address offset |
0x50 |
||
|
Physical address |
0x0702 0050 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:16 |
command |
The 16-bit command value |
RW |
0x0000 |
|
15:4 |
Reserved |
|
RO |
0x000 |
|
3 |
notify |
Tells G5C to notify the MSS via a MSS interrupt when
complete |
RW |
0 |
|
2 |
abort |
When written to '1' requests a system service is aborted. |
RW |
0 |
|
1 |
busy |
Is set whist a the system service is being processed |
RO |
0 |
|
0 |
request |
When written to '1' requests a system servide as specified
in the command field. Will stay set until G5C starts processing the command |
RW |
0 |
|
Address offset |
0x54 |
||
|
Physical address |
0x0702 0054 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
|||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:16 |
status |
returned services status, is valid when BUSY=0; |
RO |
0x0000 |
|
15:4 |
Reserved |
|
RO |
0x000 |
|
3 |
notify |
read of services control register |
RO |
0 |
|
2 |
abort |
read of services control register |
RO |
0 |
|
1 |
busy |
read of services control register |
RO |
0 |
|
0 |
request |
read of services control register |
RO |
0 |
|
Address offset |
0x58 |
||
|
Physical address |
0x0702 0058 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
Indicates that an alarm condition has happened. Register
is intended for MSS use. Is cleared by writing a '1' |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:10 |
Reserved |
|
RO |
0x00 0000 |
|
9 |
temp_low_fall |
Latched value from TVS block, writing 1 clears |
RW |
0 |
|
8 |
temp_low_rise |
Latched value from TVS block, writing 1 clears |
RW |
0 |
|
7 |
temp_high_fall |
Latched value from TVS block, writing 1 clears |
RW |
0 |
|
6 |
temp_high_rise |
Latched value from TVS block, writing 1 clears |
RW |
0 |
|
5 |
high_p5 |
Latched value from user detector, writing 1 clears |
RW |
0 |
|
4 |
low_p5 |
Latched value from user detector, writing 1 clears |
RW |
0 |
|
3 |
high_p8 |
Latched value from user detector, writing 1 clears |
RW |
0 |
|
2 |
low_p8 |
Latched value from user detector, writing 1 clears |
RW |
0 |
|
1 |
high_p05 |
Latched value from user detector, writing 1 clears |
RW |
0 |
|
0 |
low_p05 |
Latched value from user detector, writing 1 clears |
RW |
0 |
|
Address offset |
0x5C |
||
|
Physical address |
0x0702 005C |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
Enables the detector to set the MSS alarm signal routed
from G5C to the MSS. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:10 |
Reserved |
|
RO |
0x00 0000 |
|
9 |
temp_low_fall |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
8 |
temp_low_rise |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
7 |
temp_high_fall |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
6 |
temp_high_rise |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
5 |
high_p5 |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
4 |
low_p5 |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
3 |
high_p8 |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
2 |
low_p8 |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
1 |
high_p05 |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
0 |
low_p05 |
Enables the generation of the MSS user alarm on this event
|
RW |
0 |
|
Address offset |
0x60 |
||
|
Physical address |
0x0702 0060 |
Instance |
PFSOC_CONTROL_SCB |
|
Description |
Reset Controls for the MSS SPI Core |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:2 |
Reserved |
|
RO |
0x0000 0000 |
|
1 |
mask_auto_reset |
When asserted prevents the MSS reset request from
resetting the MSS SCB SPI Core |
RW |
0 |
|
0 |
reset |
When asserted holds the MSS SCB SPI Core in reset. |
RW |
0 |
PFSOC_CONTROL_SCB
has no common memories.