This section
provides information on the PF_MSS_TOP_SCB_REGS Module Instance. Each of the
module registers is described below.
Return to mpfs_ioscb_memmap_dri
|
Register Name |
Type |
Register Width (Bits)
|
Register Reset |
Address Offset |
Physical Address |
|
RW |
32 |
0x0720 0000 |
0x000 |
0x0704 0000 |
|
|
RW |
32 |
0x0000 0000 |
0x010 |
0x0704 0010 |
|
|
RW |
32 |
0x0000 0000 |
0x014 |
0x0704 0014 |
|
|
RW |
32 |
0x0000 0000 |
0x018 |
0x0704 0018 |
|
|
RW |
32 |
0x0000 0000 |
0x01C |
0x0704 001C |
|
|
RW |
32 |
0x0000 0000 |
0x020 |
0x0704 0020 |
|
|
RW |
32 |
0x0000 0000 |
0x024 |
0x0704 0024 |
|
|
RW |
32 |
0x0000 0000 |
0x028 |
0x0704 0028 |
|
|
RW |
32 |
0x0000 0000 |
0x02C |
0x0704 002C |
|
|
RW |
32 |
0x0000 0002 |
0x030 |
0x0704 0030 |
|
|
RW |
32 |
0x0000 0001 |
0x050 |
0x0704 0050 |
|
|
RW |
32 |
0x0000 0000 |
0x054 |
0x0704 0054 |
|
|
RW |
32 |
0x0000 2000 |
0x058 |
0x0704 0058 |
|
|
RW |
32 |
0x0000 0107 |
0x100 |
0x0704 0100 |
|
|
RW |
32 |
0x0000 0000 |
0x104 |
0x0704 0104 |
|
|
RW |
32 |
0x2000 3120 |
0x108 |
0x0704 0108 |
|
|
RW |
32 |
0x2000 3120 |
0x10C |
0x0704 010C |
|
|
RW |
32 |
0x2000 3120 |
0x110 |
0x0704 0110 |
|
|
RW |
32 |
0x2000 3120 |
0x114 |
0x0704 0114 |
|
|
RW |
32 |
0x2000 3120 |
0x118 |
0x0704 0118 |
|
|
RW |
32 |
0x0000 0513 |
0x120 |
0x0704 0120 |
|
|
RW |
32 |
0x3445 1073 |
0x124 |
0x0704 0124 |
|
|
RW |
32 |
0x1050 0073 |
0x128 |
0x0704 0128 |
|
|
RW |
32 |
0xFF5F F06F |
0x12C |
0x0704 012C |
|
|
RW |
32 |
0xFF1F F06F |
0x130 |
0x0704 0130 |
|
|
RW |
32 |
0xFEDF F06F |
0x134 |
0x0704 0134 |
|
|
RW |
32 |
0xFE9F F06F |
0x138 |
0x0704 0138 |
|
|
RW |
32 |
0xFE5F F06F |
0x13C |
0x0704 013C |
|
|
RW |
32 |
0x0000 0000 |
0x180 |
0x0704 0180 |
|
|
RW |
32 |
0x0000 0000 |
0x184 |
0x0704 0184 |
|
|
RW |
32 |
0x0000 0000 |
0x188 |
0x0704 0188 |
|
|
RW |
32 |
0x0000 0000 |
0x18C |
0x0704 018C |
|
|
RW |
32 |
0x0000 0000 |
0x190 |
0x0704 0190 |
|
|
RW |
32 |
0x0000 0000 |
0x194 |
0x0704 0194 |
|
|
RW |
32 |
0x0000 0000 |
0x198 |
0x0704 0198 |
|
|
RW |
32 |
0x0000 0000 |
0x19C |
0x0704 019C |
|
|
RW |
32 |
0x0000 0004 |
0x1A0 |
0x0704 01A0 |
|
|
RW |
32 |
0x0000 0000 |
0x1A4 |
0x0704 01A4 |
|
|
RW |
32 |
0x4005 0003 |
0x1A8 |
0x0704 01A8 |
|
|
RW |
32 |
0x0000 007F |
0x1AC |
0x0704 01AC |
|
|
RW |
32 |
0x0000 3FFF |
0x1B0 |
0x0704 01B0 |
|
|
RW |
32 |
0x0000 0000 |
0x1B4 |
0x0704 01B4 |
|
|
RW |
32 |
0x0000 0000 |
0x1B8 |
0x0704 01B8 |
|
|
RW |
32 |
0x0000 0720 |
0x1BC |
0x0704 01BC |
|
|
RO |
32 |
0x0000 0000 |
0x1C0 |
0x0704 01C0 |
|
|
RW |
32 |
0x0000 3F3F |
0x1C4 |
0x0704 01C4 |
|
|
RW |
32 |
0x0000 3F3F |
0x1C8 |
0x0704 01C8 |
|
|
RW |
32 |
0x8800 000F |
0x200 |
0x0704 0200 |
|
|
RW |
32 |
0x0000 0000 |
0x204 |
0x0704 0204 |
|
|
RW |
32 |
0x0000 1003 |
0x208 |
0x0704 0208 |
|
|
RO |
32 |
0x0001 0000 |
0x20C |
0x0704 020C |
|
|
RO |
32 |
0x0000 0000 |
0x210 |
0x0704 0210 |
|
|
RW |
32 |
0x0000 0000 |
0x214 |
0x0704 0214 |
|
|
RW |
32 |
0x8800 000F |
0x220 |
0x0704 0220 |
|
|
RW |
32 |
0x0000 0000 |
0x224 |
0x0704 0224 |
|
|
RW |
32 |
0x0000 1003 |
0x228 |
0x0704 0228 |
|
|
RO |
32 |
0x0001 0000 |
0x22C |
0x0704 022C |
|
|
RO |
32 |
0x0000 0000 |
0x230 |
0x0704 0230 |
|
|
RW |
32 |
0x0000 0000 |
0x234 |
0x0704 0234 |
|
|
RW |
32 |
0x8800 000F |
0x240 |
0x0704 0240 |
|
|
RW |
32 |
0x0000 0000 |
0x244 |
0x0704 0244 |
|
|
RW |
32 |
0x0000 1003 |
0x248 |
0x0704 0248 |
|
|
RO |
32 |
0x0001 0000 |
0x24C |
0x0704 024C |
|
|
RO |
32 |
0x0000 0000 |
0x250 |
0x0704 0250 |
|
|
RW |
32 |
0x0000 0000 |
0x254 |
0x0704 0254 |
|
|
RW |
32 |
0x8800 000F |
0x260 |
0x0704 0260 |
|
|
RW |
32 |
0x0000 0000 |
0x264 |
0x0704 0264 |
|
|
RW |
32 |
0x0000 1003 |
0x268 |
0x0704 0268 |
|
|
RO |
32 |
0x0001 0000 |
0x26C |
0x0704 026C |
|
|
RO |
32 |
0x0000 0000 |
0x270 |
0x0704 0270 |
|
|
RW |
32 |
0x0000 0000 |
0x274 |
0x0704 0274 |
|
|
RW |
32 |
0x0000 0828 |
0x278 |
0x0704 0278 |
|
|
RW |
32 |
0x0000 0828 |
0x27C |
0x0704 027C |
|
Address offset |
0x000 |
||
|
Physical address |
0x0704 0000 |
Instance |
MSS |
|
Description |
System Reset Register. This MSS soft reset register is not
readable or writeable by the MSS or user or DRI. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:16 |
BLOCKID |
This returns the block type and chip location. |
RO |
0x0720 |
|
15:9 |
Reserved |
|
RO |
0x00 |
|
8 |
PERIPH |
This asserts the functional reset of the block. It is
asserted at power up, the bit self clears i.e. is
similar to a W1P bit. This bit is activated global_periph_reset
|
WO |
0 |
|
7:2 |
Reserved |
|
RO |
0x00 |
|
1 |
V_MAP |
This when asserted resets all the register bits apart from
the non-volatile registers, the bit self clears i.e.
is similar to a W1P bit. This bit is activated global_map_reset.
|
WO |
0 |
|
0 |
NV_MAP |
This when asserted resets all the non-volatile register
bits e.g. RW-P bits, the bit self clears i.e. is
similar to a W1P bit. This bit is activated global_map_reset.
|
WO |
0 |
|
Address offset |
0x010 |
||
|
Physical address |
0x0704 0010 |
Instance |
MSS |
|
Description |
Axi Write
Setup. Not accesible from MSS or user or DRI. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
SYSTEM |
0: AXI transaction uses ID 0 and passes through MPU block |
RW |
0 |
|
30:27 |
QOS |
Sets the AXI QOS value, higher values have higher priority
in the switch |
RW |
0x0 |
|
26:24 |
PROT |
Sets the AXI protection value |
RW |
0x0 |
|
23:20 |
CACHE |
Sets the AXI Cache value |
RW |
0x0 |
|
19 |
LOCK |
Sets the AXI lock |
RW |
0 |
|
18:16 |
SIZE |
Set the AXI size (width) |
RW |
0x0 |
|
15:8 |
LENGTH |
Sets the AXI burst length |
RW |
0x00 |
|
7:6 |
BURST |
Sets the AXi burst type |
RW |
0x0 |
|
5:0 |
ADDR |
Sets the upper 6-bits of the address bus |
RW |
0x00 |
|
Address offset |
0x014 |
||
|
Physical address |
0x0704 0014 |
Instance |
MSS |
|
Description |
AXI Write Address. Not accesible
from MSS or user or DRI. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
ADDR |
This sets the AXI write address. A write to this register
triggers the AXI AW cycle |
RW |
0x0000 0000 |
|
Address offset |
0x018 |
||
|
Physical address |
0x0704 0018 |
Instance |
MSS |
|
Description |
AXI Write Data. This is write
only register, reads will return zero. Not accesible
from MSS or user or DRI. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
DATA |
Write Data, when written will initiate a AHB write
transfer through the write data FIFO.Data must be written
using word operations. If AWSIZE<=2 then a AXI Write data cycle will be
started every cycle, if AWSIZE=3 a AXI Write data cycle will be started every
other cycle. |
RW |
0x0000 0000 |
|
Address offset |
0x01C |
||
|
Physical address |
0x0704 001C |
Instance |
MSS |
|
Description |
AXI Read Setup. Not accesible
from MSS or user or DRI. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
SYSTEM |
0: AXI transaction uses ID 0 and passes through MPU block |
RW |
0 |
|
30:27 |
QOS |
Sets the AXI QOS value, higher values have higher priority
in the switch |
RW |
0x0 |
|
26:24 |
PROT |
Sets the AXI protection value |
RW |
0x0 |
|
23:20 |
CACHE |
Sets the AXI Cache value |
RW |
0x0 |
|
19 |
LOCK |
Sets the AXI lock |
RW |
0 |
|
18:16 |
SIZE |
Set the AXI size (width) |
RW |
0x0 |
|
15:8 |
LENGTH |
Sets the AXI burst length |
RW |
0x00 |
|
7:6 |
BURST |
Sets the AXi burst type |
RW |
0x0 |
|
5:0 |
ADDR |
Sets the upper 6-bits of the address bus |
RW |
0x00 |
|
Address offset |
0x020 |
||
|
Physical address |
0x0704 0020 |
Instance |
MSS |
|
Description |
AXI Read Address. Not accesible
from MSS or user or DRI. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
ADDR |
This sets the AXI read address. A write to this register
triggers the AXI AR cycle |
RW |
0x0000 0000 |
|
Address offset |
0x024 |
||
|
Physical address |
0x0704 0024 |
Instance |
MSS |
|
Description |
AHB Read data. This is a read only register, writes will be have no effect. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
DATA |
Read data from the AXI read FIFO |
RW |
0x0000 0000 |
|
Address offset |
0x028 |
||
|
Physical address |
0x0704 0028 |
Instance |
MSS |
|
Description |
AXI Master Status. Not accessible from MSS or user or DRI.
This register provides status information and writes only supported on bits
28:24 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:29 |
Reserved |
|
RO |
0x0 |
|
28 |
INT_ENABLE_SYSREG |
Enable SCB interrupt from the SCB Interrupt register |
RW |
0 |
|
27 |
INT_ENABLE_WRESP |
Enable SCB interrupt on write response error |
RW |
0 |
|
26 |
INT_ENABLE_RRESP |
Enable SCB interrupt on read response error |
RW |
0 |
|
25 |
INT_ENABLE_WRITE_ORUN |
Enable SCB interrupt on write overrun |
RW |
0 |
|
24 |
INT_ENABLE_READ_ORUN |
Enable SCB interrupt on read overrun |
RW |
0 |
|
23:21 |
Reserved |
|
RO |
0x0 |
|
20 |
MSS_RESET |
Indicates that the MSS has been reset and the SCB transfer
may have failed. Is the internal MSS sticky_reset
signal |
RW |
0 |
|
19:18 |
READ_RESPONSE |
Indicates the read response. When a non-zero value is detected the register will hold the value until the read_error bit is cleared or abort asserted |
RW |
0x0 |
|
17:16 |
WRITE_RESPONSE |
Indicates the write response. When a non-zero value is detected the register will hold the value until the write_error bit is cleared or abort asserted |
RW |
0x0 |
|
15 |
WRITE_OVERRUN |
Indicates the SCB bus wrote the write FIFO when empty. Is
cleared by writing a ‘1’ |
RW |
0 |
|
14 |
READ_OVERRUN |
Indicates the SCB bus read the read FIFO when empty. Is
cleared by writing a ‘1’ |
RW |
0 |
|
13:9 |
READ_COUNT |
Indicates how many 32-bit words are stored in the read
FIFO |
RW |
0x00 |
|
8:4 |
WRITE_COUNT |
Indicates how many 32-bit words are stored in the write
FIFO |
RW |
0x00 |
|
3 |
READ_ERROR |
Set when a read error response is received. Is cleared by
writing a ‘1’ |
RW |
0 |
|
2 |
WRITE_ERROR |
Set when a write error response is received. Is cleared by
writing a ‘1’ |
RW |
0 |
|
1 |
READ_BUSY |
Set during arvalid cycle and
cleared on the last read response |
RW |
0 |
|
0 |
WRITE_BUSY |
Set during awvalid cycle and cleared
on the write response |
RW |
0 |
|
Address offset |
0x02C |
||
|
Physical address |
0x0704 002C |
Instance |
MSS |
|
Description |
AXI Cycle Controls. Not accesible
from MSS or user or DRI. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:17 |
Reserved |
|
RO |
0x0000 |
|
16 |
START_WRITE |
Starts AXI transfer when STALL_WRITE is set, reads as zero
|
RW |
0 |
|
15:9 |
Reserved |
|
RO |
0x00 |
|
8 |
STALL_WRITE |
When set prevents the logic initiating AW cycle
automatically. Write is started by START_WRITE. Allows up to 16 words
(32-bits) of data to be queued allowing AXI to run more efficiently. |
RW |
0 |
|
7:1 |
Reserved |
|
RO |
0x00 |
|
0 |
ABORT |
Abort current transfer and reset the FSMS. May cause AXI
protocol violations |
RW |
0 |
|
Address offset |
0x030 |
||
|
Physical address |
0x0704 0030 |
Instance |
MSS |
|
Description |
Used to program MSS RAM redundancy system during system
startup |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:3 |
Reserved |
|
RO |
0x0000 0000 |
|
2 |
NOCLOCK |
When set stops the SCB clock creating the Redundancy
clock. To allow for large recovery times on the redundancy ISOLATE and RESET
inputs this bit should be set prior to toggling the reset/isolate bits and
cleared afterwards. |
RW |
0 |
|
1 |
ISOLATE |
Asserts the Redundacy isolate,
interface isolated when 1 (can be accessed by MSS in factory mode) |
RW |
1 |
|
0 |
RESET |
Asserts the Redundacy reset (can
be accessed by MSS in factory mode) |
RW |
0 |
|
Address offset |
0x050 |
||
|
Physical address |
0x0704 0050 |
Instance |
MSS |
|
Description |
Used to access the BIST systems |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:19 |
Reserved |
|
RO |
0x0000 |
|
18:16 |
margin |
Set the BIST memory margin, factory mode only |
RW |
0x0 |
|
15:13 |
Reserved |
|
RO |
0x0 |
|
12:8 |
select |
Select the BIST engine 0-15 |
RW |
0x00 |
|
7:4 |
Reserved |
|
RO |
0x0 |
|
3 |
diag_select |
Assert the DIAG select |
RW |
0 |
|
2 |
reset |
Assert the BIST reset |
RW |
0 |
|
1 |
enable |
Enable the CPU BIST system |
RW |
0 |
|
0 |
enabled |
Indicates that CPU may use BIST system, UFS bit may
disable this interface, available when factory mode set |
RO |
1 |
|
Address offset |
0x054 |
||
|
Physical address |
0x0704 0054 |
Instance |
MSS |
|
Description |
Data value to be shifted into BIST system |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
Writes sets the data value to shifted, LSB shifted out
first. Reads returns the shifted in value, MSB is last bit shifted in. |
RW |
0x0000 0000 |
|
Address offset |
0x058 |
||
|
Physical address |
0x0704 0058 |
Instance |
MSS |
|
Description |
BIST Shift Controls |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:15 |
Reserved |
|
RO |
0x0 0000 |
|
14:8 |
length |
Number of bits to shift 1-127. If set to >32 the outgoing
shift data for bits 33 upwards will be zero. This allows MBIST with CSR
registers greater than 32 to be started with valid data loaded into bits 23:0
off the CSR register as specified in the data register. When >32 incoming
data is not captured in the shift register, if the read data is to extracted then each shift operation should be <=32
bits. To read a 88 bit register will require 3 shift
operatiosn of 32, 32 and 24 bits |
RW |
0x20 |
|
7:4 |
Reserved |
|
RO |
0x0 |
|
3 |
busy |
Indicates that the shift is in progress. |
RO |
0 |
|
2 |
shift |
Perform the specified number off shift cycles. |
RW |
0 |
|
1 |
capture |
Do a shift cycle, may be asserted at the same time as shift,
capture is asserted before shift operations start. |
RW |
0 |
|
0 |
update |
Do an update cycle |
RW |
0 |
|
Address offset |
0x100 |
||
|
Physical address |
0x0704 0100 |
Instance |
MSS |
|
Description |
MSS reset Controls |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:25 |
Reserved |
|
RO |
0x00 |
|
24:16 |
REASON |
This provides a read off the main SYSREG reset reason
register |
RO |
0x000 |
|
15:9 |
Reserved |
|
RO |
0x00 |
|
8 |
SGMII |
Asserts a reset the SGMII block containing the MSS
reference clock input. |
RW |
1 |
|
7:4 |
Reserved |
|
RO |
0x0 |
|
3 |
REBOOT_REQUEST |
Reading returns the value of reboot_request. |
RW |
0 |
|
2 |
CPUINRESET |
Indicates that the CPU's are being help in reset. Will
stay active for sixteen CPU clocks after the CPU resets are released |
RO |
1 |
|
1 |
MSS |
Holds the MSS system (i.e.
AXI/AHB/APB resets) in reset. When asserted the CPU's
are also held in reset. The Trace UDB reset is not asserted by this bit. |
RW |
1 |
|
0 |
CPU |
Holds the CPUS (corplex) in
reset. |
RW |
1 |
|
Address offset |
0x104 |
||
|
Physical address |
0x0704 0104 |
Instance |
MSS |
|
Description |
MSS Status |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:17 |
Reserved |
|
RO |
0x0000 |
|
16 |
ecc_error_other |
|
RO |
0 |
|
15 |
ecc_error_l2 |
|
RO |
0 |
|
14 |
halt_cpu4 |
|
RO |
0 |
|
13 |
halt_cpu3 |
|
RO |
0 |
|
12 |
halt_cpu2 |
|
RO |
0 |
|
11 |
halt_cpu1 |
|
RO |
0 |
|
10 |
halt_cpu0 |
|
RO |
0 |
|
9 |
debug_active |
|
RO |
0 |
|
8:4 |
watchdog |
|
RO |
0x00 |
|
3:0 |
boot_status |
|
RW |
0x0 |
|
Address offset |
0x108 |
||
|
Physical address |
0x0704 0108 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
address |
Boot Address i.e. reset vector
for the coreplex |
RW |
0x2000 3120 |
|
Address offset |
0x10C |
||
|
Physical address |
0x0704 010C |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
address |
Boot Address i.e. reset vector
for the coreplex |
RW |
0x2000 3120 |
|
Address offset |
0x110 |
||
|
Physical address |
0x0704 0110 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
address |
Boot Address i.e. reset vector
for the coreplex |
RW |
0x2000 3120 |
|
Address offset |
0x114 |
||
|
Physical address |
0x0704 0114 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
address |
Boot Address i.e. reset vector
for the coreplex |
RW |
0x2000 3120 |
|
Address offset |
0x118 |
||
|
Physical address |
0x0704 0118 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
address |
Boot Address i.e. reset vector
for the coreplex |
RW |
0x2000 3120 |
|
Address offset |
0x120 |
||
|
Physical address |
0x0704 0120 |
Instance |
MSS |
|
Description |
32-byte ROM for CPU booting |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
li a0,0 |
RW |
0x0000 0513 |
|
Address offset |
0x124 |
||
|
Physical address |
0x0704 0124 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
csrw mip,a0 |
RW |
0x3445 1073 |
|
Address offset |
0x128 |
||
|
Physical address |
0x0704 0128 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
wfi |
RW |
0x1050 0073 |
|
Address offset |
0x12C |
||
|
Physical address |
0x0704 012C |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
j 20003120 <_start> |
RW |
0xFF5F F06F |
|
Address offset |
0x130 |
||
|
Physical address |
0x0704 0130 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
j 20003120 <_start> |
RW |
0xFF1F F06F |
|
Address offset |
0x134 |
||
|
Physical address |
0x0704 0134 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
j 20003120 <_start> |
RW |
0xFEDF F06F |
|
Address offset |
0x138 |
||
|
Physical address |
0x0704 0138 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
j 20003120 <_start> |
RW |
0xFE9F F06F |
|
Address offset |
0x13C |
||
|
Physical address |
0x0704 013C |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
j 20003120 <_start> |
RW |
0xFE5F F06F |
|
Address offset |
0x180 |
||
|
Physical address |
0x0704 0180 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:1 |
Reserved |
|
RO |
0x0000 0000 |
|
0 |
in_progress |
Set by PFC when FF in progress |
RW |
0 |
|
Address offset |
0x184 |
||
|
Physical address |
0x0704 0184 |
Instance |
MSS |
|
Description |
Register bit that may drive IOMUX |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:1 |
Reserved |
|
RO |
0x0000 0000 |
|
0 |
ioout |
Allows PFC to drive an IO pad[4] when
IOMUX is configured in MISC mode. This is provided to aid device validation alloing an IO to be easily controlleed
by PF-control. |
RW |
0 |
|
Address offset |
0x188 |
||
|
Physical address |
0x0704 0188 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:20 |
Reserved |
|
RO |
0x000 |
|
19:16 |
idv |
|
RW |
0x0 |
|
15:0 |
idp |
|
RW |
0x0000 |
|
Address offset |
0x18C |
||
|
Physical address |
0x0704 018C |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:1 |
Reserved |
|
RO |
0x0000 0000 |
|
0 |
active |
Writing to this bit sets the pfc_message
interrupt to the Coreplex, interrupt is cleared by coreplex writing a '0'. It is required that the MSS
clears this bit proir to requesting a system
service from PFC, on completion PFC will set the MESSAGE register and this
bit casuing an interrupt to the MSS indicating the
system service is complete. |
RW |
0 |
|
Address offset |
0x190 |
||
|
Physical address |
0x0704 0190 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:0 |
data |
Data value associated with Message interrupt, used for
system service return status |
RW |
0x0000 0000 |
|
Address offset |
0x194 |
||
|
Physical address |
0x0704 0194 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:1 |
Reserved |
|
RO |
0x0000 0000 |
|
0 |
active |
Writing to this bit sets the DEVRST interrupt to the Coreplex via the maintence
register, interrupt is cleared by coreplex writing
a '0' to this bit |
RW |
0 |
|
Address offset |
0x198 |
||
|
Physical address |
0x0704 0198 |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:1 |
Reserved |
|
RO |
0x0000 0000 |
|
0 |
active |
Writing to this bit sets the SCB interrupt signal,
interrupt is cleared by PFC writing a '0' to this bit |
RW |
0 |
|
Address offset |
0x19C |
||
|
Physical address |
0x0704 019C |
Instance |
MSS |
|
Description |
|||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:1 |
Reserved |
|
RO |
0x0000 0000 |
|
0 |
active |
Writing to this bit sets the MSS to PFC interrupt,
interrupt is cleared by PFC writing a '0' to this bit |
RW |
0 |
|
Address offset |
0x1A0 |
||
|
Physical address |
0x0704 01A0 |
Instance |
MSS |
|
Description |
This register configures the |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:17 |
Reserved |
|
RO |
0x0000 |
|
16 |
DISABLE_XIP |
When set prevents the QSPI module from operating in XIP
mode preventinmg direct execution from the QSPI
device |
RW |
0 |
|
15:9 |
Reserved |
|
RO |
0x00 |
|
8 |
CPU_BIST_DISABLE |
When set the CPU's may not initiate MBIST of the RAMS |
RW |
0 |
|
7:6 |
Reserved |
|
RO |
0x0 |
|
5 |
CPU_DISABLE |
When '1' dissables the SIFIVE
CPUs and holds them in reset. |
RW |
0 |
|
4 |
CPU_ALLOWED |
When '1' allows the SIFIVE CPUs to operate. When '0' the
CPUS (E51 and U54s) are held in reset. This bit is intended to be set via a
factory configuration bit by PF-Control allowing the RiscV
cores to be de-featured |
RW |
0 |
|
3 |
CAN_ALLOWED |
When '1' indicates CAN is enabled When '0' the CAN block
is held in reset. This bit is intended to be set via a factory configuration
bit by PF-Control allowing the CAN core to be de-featured |
RW |
0 |
|
2 |
CRYPTO_DISABLE |
When '1' disables the Crypto block and the Athena block is
held in reset. This bit is intended to be set via a factory configuration bit
by PF-Control allowing the CAN core to be de-featured |
RW |
1 |
|
1 |
Reserved |
|
RO |
0 |
|
0 |
FACTORY_TEST_MODE |
Indicates the device is in manufacturing test mode. |
RW |
0 |
|
Address offset |
0x1A4 |
||
|
Physical address |
0x0704 01A4 |
Instance |
MSS |
|
Description |
Sets the Athena owners. Not writeable by the MSS or user. ATHERA_CR configuration is
provided as part of Libero SoC configuration and setting is integrated in stp file. User cannot change configuration dynamically. |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:5 |
Reserved |
|
RO |
0x000 0000 |
|
4 |
stream_enable |
Allow Streaming Interface to operate |
RW |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2:0 |
mss_mode |
0xx: Crypto block not available to fabric or MSS |
RW |
0x0 |
|
Address offset |
0x1A8 |
||
|
Physical address |
0x0704 01A8 |
Instance |
MSS |
|
Description |
Applies to AHB Controllers when NVM override set |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
timer |
Sets the duration of the timer used to detect a non response of slow response
from the PNVM on C and R bus accesses. |
RW |
0x40 |
|
23:19 |
Reserved |
|
RO |
0x00 |
|
18 |
interrupt_enable |
Enable the PNVM interrupt |
RW |
1 |
|
17 |
slowread |
When '1' the controller will initate
separate PNVM reads for all reads. No buffering or speculative operations
will be carried out. When performing word reads incrementing through PNVM
each location will be read twice (intended for test use) |
RW |
0 |
|
16 |
readahead |
Enables "readahead" on the PNVM controller. The
controller will automatically read the next PNVM location as soon as possible
ahead of the AHB request. This will improve read performance when
incrementing though memory as the NVM reads and AHB cycles are pipelined.
When set non incrementing accesses will take longer as the controller may be
in the process of reading the next address and the PNVM cycle needs to
complete prior to starting the required read |
RW |
1 |
|
15:10 |
Reserved |
|
RO |
0x00 |
|
9 |
clock_suppress |
When set suppresses clock edge between C-Bus access cycles
so that they appear as consecutive access cycles. |
RW |
0 |
|
8 |
clock_continuous |
When '1' the PNVM clock will be always generated, and not
stopped between access cycles. Setting this will increase access latency but
mean that the PNVM clock operates at a stable rate. |
RW |
0 |
|
7:6 |
Reserved |
|
RO |
0x0 |
|
5:0 |
clock_period |
Sets the number of AHB cycles used to generate the PNVM
clock, |
RW |
0x03 |
|
Address offset |
0x1AC |
||
|
Physical address |
0x0704 01AC |
Instance |
MSS |
|
Description |
Applies to the eNVM controller |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:9 |
Reserved |
|
RO |
0x00 0000 |
|
8 |
override |
Enable PFC overrides |
RW |
0 |
|
7 |
Reserved |
|
RO |
0 |
|
6 |
sleep |
Controls the PNVM sleep input |
RW |
1 |
|
5 |
iso |
Controls the PNVM iso (isolate) input |
RW |
1 |
|
4 |
pd4 |
Controls the PNVM pd4 (powerdown)
input |
RW |
1 |
|
3 |
pd3 |
Controls the PNVM pd3 (powerdown)
input |
RW |
1 |
|
2 |
pd2 |
Controls the PNVM pd2 (powerdown)
input |
RW |
1 |
|
1 |
pd1 |
Controls the PNVM pd1 (powerdown)
input |
RW |
1 |
|
0 |
reset |
Asserts the PNVM reset input (inverted version to PNVM) |
RW |
1 |
|
Address offset |
0x1B0 |
||
|
Physical address |
0x0704 01B0 |
Instance |
MSS |
|
Description |
Puts all the RAMS in that block into shut down mode. RAM
contents not preserved. Powers down the RAM and periphery circuits. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:14 |
Reserved |
|
RO |
0x0 0000 |
|
13 |
l2 |
|
RW |
1 |
|
12 |
u54_4 |
|
RW |
1 |
|
11 |
u54_3 |
|
RW |
1 |
|
10 |
u54_2 |
|
RW |
1 |
|
9 |
u54_1 |
|
RW |
1 |
|
8 |
e51 |
|
RW |
1 |
|
7 |
ddrc |
|
RW |
1 |
|
6 |
athena |
|
RW |
1 |
|
5 |
mmc |
|
RW |
1 |
|
4 |
gem1 |
|
RW |
1 |
|
3 |
gem0 |
|
RW |
1 |
|
2 |
usb |
|
RW |
1 |
|
1 |
can1 |
|
RW |
1 |
|
0 |
can0 |
|
RW |
1 |
|
Address offset |
0x1B4 |
||
|
Physical address |
0x0704 01B4 |
Instance |
MSS |
|
Description |
Controls the RAM margin inputs on the RAMS. Should not be changeld without explicity
guidance from Silicon Engineering |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:27 |
Reserved |
|
RO |
0x00 |
|
26:25 |
l2 |
|
RW |
0x0 |
|
24:23 |
u54_4 |
|
RW |
0x0 |
|
22:21 |
u54_3 |
|
RW |
0x0 |
|
20:19 |
u54_2 |
|
RW |
0x0 |
|
18:17 |
u54_1 |
|
RW |
0x0 |
|
16:15 |
e51 |
|
RW |
0x0 |
|
14:13 |
ddrc |
|
RW |
0x0 |
|
12:11 |
mmc |
|
RW |
0x0 |
|
10:9 |
gem1 |
|
RW |
0x0 |
|
8:7 |
gem0 |
|
RW |
0x0 |
|
6:5 |
usb |
|
RW |
0x0 |
|
4:3 |
can1 |
|
RW |
0x0 |
|
2:1 |
can0 |
|
RW |
0x0 |
|
0 |
enable |
|
RW |
0 |
|
Address offset |
0x1B8 |
||
|
Physical address |
0x0704 01B8 |
Instance |
MSS |
|
Description |
Configures the trace and debug connectivity |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:9 |
Reserved |
|
RO |
0x00 0000 |
|
8 |
ULTRASOC_FABRIC |
When set the Utrasoc JTAG
interface is connected to fabric EIP connections allowing the JTAG to be
directly accessed through fabric IO pins. This also connects the RiscV debugger to the fabric as it passed through the UltraSoc JPAM module |
RW |
0 |
|
7:3 |
Reserved |
|
RO |
0x00 |
|
2 |
ULTRASOC_DISABLE_AXI |
When set the Utrasoc module is dissabled and will not respond to AXI accesses from
PF-Control or the fabric. The JTAG end point will be in bypass mode. |
RW |
0 |
|
1 |
ULTRASOC_DISABLE_JTAG |
When set the Utrasoc module is dissabled and will not respond to JTAG accesses from
PF-Control or the fabric. The JTAG end point will be in bypass mode. |
RW |
0 |
|
0 |
CPU_DEBUG_DISABLE |
When set the RiscV debug module
is dissabled and will not respond to JTAG accesses
from either PF-Control or the fabric. The JTAG end point will be in bypass
mode. |
RW |
0 |
|
Address offset |
0x1BC |
||
|
Physical address |
0x0704 01BC |
Instance |
MSS |
|
Description |
Controls the MSS Corner IO control signals |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:16 |
Reserved |
|
RO |
0x0000 |
|
15 |
mss_sel_hw_def |
Sets the value driven out on mss_sel_hw_def_out
|
RW |
0 |
|
14 |
mss_sel_hw_dyn |
Sets the value driven out on mss_sel_hw_dyn_out
|
RW |
0 |
|
13 |
mss_io_en |
Sets the value driven out on mss_io_en
(before gating) |
RW |
0 |
|
12 |
mss_flash_valid |
Sets the value driven out on mss_flash_valid_out
|
RW |
0 |
|
11 |
mss_core_up |
Sets the value driven out on mss_core_up_out
|
RW |
0 |
|
10:8 |
mss_dce |
Sets the value driven out on mss_dce_out
unless PFC asserts its overrides |
RW |
0x7 |
|
7 |
lp_stop_clocks_done_mss |
Read back of lp_stop_clocks_done
input of MSS Corner LP state control |
RO |
0 |
|
6 |
lp_stop_clocks_out_mss |
Direct control of MSS Corner LP state control |
RW |
0 |
|
5 |
lp_pll_locked_mss |
Direct control of MSS Corner LP state control |
RW |
1 |
|
4 |
lp_state_bypass_mss |
Direct control of MSS Corner LP state control |
RW |
0 |
|
3 |
lp_state_persist_mss |
Direct control of MSS Corner LP state control |
RW |
0 |
|
2 |
lp_state_op_mss |
Direct control of MSS Corner LP state control |
RW |
0 |
|
1 |
lp_state_ip_mss |
Direct control of MSS Corner LP state control |
RW |
0 |
|
0 |
lp_state_mss |
Direct control of MSS Corner LP state control (before
gating) |
RW |
0 |
|
Address offset |
0x1C0 |
||
|
Physical address |
0x0704 01C0 |
Instance |
MSS |
|
Description |
Controls the lockdown enable for the MSS-related IO banks |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:4 |
Reserved |
|
RO |
0x000 0000 |
|
3 |
ddr_io_lockdn_en |
Enable lockdown of DDR-related IO if global lockdown
asserted |
RO |
0 |
|
2 |
sgmii_io_lockdn_en |
Enable lockdown of SGMII-related IO if global lockdown
asserted |
RO |
0 |
|
1 |
mssio_b4_lockdn_en |
Enable lockdown of MSSIO bank 4 if global lockdown
asserted |
RO |
0 |
|
0 |
mssio_b2_lockdn_en |
Enable lockdown of MSSIO bank 2 if global lockdown
asserted |
RO |
0 |
|
Address offset |
0x1C4 |
||
|
Physical address |
0x0704 01C4 |
Instance |
MSS |
|
Description |
Configures the MSSIO block |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:20 |
Reserved |
|
RO |
0x000 |
|
19:16 |
vs |
Sets the voltage controls for bank 2 |
RW |
0x0 |
|
15:14 |
Reserved |
|
RO |
0x0 |
|
13:8 |
bank_ncode |
Sets the NCODE value for bank 2 |
RW |
0x3F |
|
7:6 |
Reserved |
|
RO |
0x0 |
|
5:0 |
bank_pcode |
Sets the PCODE value for bank 2 |
RW |
0x3F |
|
Address offset |
0x1C8 |
||
|
Physical address |
0x0704 01C8 |
Instance |
MSS |
|
Description |
Configures the MSSIO block |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:20 |
Reserved |
|
RO |
0x000 |
|
19:16 |
vs |
Sets the voltage controls for bank 4 |
RW |
0x0 |
|
15:14 |
Reserved |
|
RO |
0x0 |
|
13:8 |
bank_ncode |
Sets the NCODE value for bank 4 |
RW |
0x3F |
|
7:6 |
Reserved |
|
RO |
0x0 |
|
5:0 |
bank_pcode |
Sets the PCODE value for bank 4 |
RW |
0x3F |
|
Address offset |
0x200 |
||
|
Physical address |
0x0704 0200 |
Instance |
MSS |
|
Description |
DLL control register 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:28 |
lock_low |
|
RW |
0x8 |
|
27:24 |
lock_high |
|
RW |
0x8 |
|
23:22 |
Reserved |
|
RO |
0x0 |
|
21:20 |
lock_flt |
|
RW |
0x0 |
|
19 |
lock_frc |
|
RW |
0 |
|
18:16 |
Reserved |
|
RO |
0x0 |
|
15:14 |
alu_upd |
|
RW |
0x0 |
|
13:11 |
Reserved |
|
RO |
0x0 |
|
10 |
div_sel |
|
RW |
0 |
|
9 |
fb_sel |
|
RW |
0 |
|
8 |
ref_sel |
|
RW |
0 |
|
7:6 |
sel_s |
|
RW |
0x0 |
|
5:4 |
sel_p |
|
RW |
0x0 |
|
3:2 |
phase_s |
|
RW |
0x3 |
|
1:0 |
phase_p |
All thes eregisters
follow the standard allocation for DLL blocks used in PF. Please refer to the
DLL SAC specification for details of register functions. |
RW |
0x3 |
|
Address offset |
0x204 |
||
|
Physical address |
0x0704 0204 |
Instance |
MSS |
|
Description |
DLL control register 1 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
Reserved |
|
RO |
0 |
|
30 |
relock_fast |
|
RW |
0 |
|
29:24 |
init_code |
|
RW |
0x00 |
|
23 |
test_ring |
|
RW |
0 |
|
22:16 |
Reserved |
|
RO |
0x00 |
|
15 |
test_s |
|
RW |
0 |
|
14:8 |
adj_del4 |
|
RW |
0x00 |
|
7:0 |
set_alu |
|
RW |
0x00 |
|
Address offset |
0x208 |
||
|
Physical address |
0x0704 0208 |
Instance |
MSS |
|
Description |
DLL status register 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
Reserved |
|
RO |
0x00 |
|
23:16 |
Reserved |
|
RO |
0x00 |
|
15:14 |
Reserved |
|
RO |
0x0 |
|
13 |
Reserved |
|
RO |
0 |
|
12 |
phase_move_clk |
|
RW |
1 |
|
11 |
Reserved |
|
RO |
0 |
|
10 |
Reserved |
|
RO |
0 |
|
9 |
Reserved |
|
RO |
0 |
|
8 |
Reserved |
|
RO |
0 |
|
7:5 |
Reserved |
|
RO |
0x0 |
|
4 |
Reserved |
|
RO |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2 |
Reserved |
|
RO |
0 |
|
1 |
bypass |
|
RW |
1 |
|
0 |
reset |
|
RW |
1 |
|
Address offset |
0x20C |
||
|
Physical address |
0x0704 020C |
Instance |
MSS |
|
Description |
DLL status register 1 |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:30 |
Reserved |
|
RO |
0x0 |
|
29:28 |
Reserved |
|
RO |
0x0 |
|
27:26 |
Reserved |
|
RO |
0x0 |
|
25 |
Reserved |
|
RO |
0 |
|
24:16 |
sro_alu_cnt |
|
RO |
0x001 |
|
15:8 |
Reserved |
|
RO |
0x00 |
|
7 |
Reserved |
|
RO |
0 |
|
6:0 |
sro_del4 |
|
RO |
0x00 |
|
Address offset |
0x210 |
||
|
Physical address |
0x0704 0210 |
Instance |
MSS |
|
Description |
DLL status register 2 |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
Reserved |
|
RO |
0x00 |
|
23:16 |
Reserved |
|
RO |
0x00 |
|
15:7 |
Reserved |
|
RO |
0x000 |
|
6 |
Reserved |
|
RO |
0 |
|
5 |
Reserved |
|
RO |
0 |
|
4 |
Reserved |
|
RO |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2 |
sro_lock |
|
RO |
0 |
|
1 |
Reserved |
|
RO |
0 |
|
0 |
Reserved |
|
RO |
0 |
|
Address offset |
0x214 |
||
|
Physical address |
0x0704 0214 |
Instance |
MSS |
|
Description |
Enables test modes on the DLL |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:4 |
Reserved |
|
RO |
0x000 0000 |
|
3 |
reserved |
To aid synthesis - reads as zero |
RO |
0 |
|
2 |
ref_select |
When '1' the sb clock input is fed to the DLL reference |
RW |
0 |
|
1 |
cfm_select |
Feeds the MBIST clock rather than DLL clock to the CFM
block |
RW |
0 |
|
0 |
cfm_enable |
When set enables the DLL output to the frequency meter
inside the PF-Controller for test use |
RW |
0 |
|
Address offset |
0x220 |
||
|
Physical address |
0x0704 0220 |
Instance |
MSS |
|
Description |
DLL control register 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:28 |
lock_low |
|
RW |
0x8 |
|
27:24 |
lock_high |
|
RW |
0x8 |
|
23:22 |
Reserved |
|
RO |
0x0 |
|
21:20 |
lock_flt |
|
RW |
0x0 |
|
19 |
lock_frc |
|
RW |
0 |
|
18:16 |
Reserved |
|
RO |
0x0 |
|
15:14 |
alu_upd |
|
RW |
0x0 |
|
13:11 |
Reserved |
|
RO |
0x0 |
|
10 |
div_sel |
|
RW |
0 |
|
9 |
fb_sel |
|
RW |
0 |
|
8 |
ref_sel |
|
RW |
0 |
|
7:6 |
sel_s |
|
RW |
0x0 |
|
5:4 |
sel_p |
|
RW |
0x0 |
|
3:2 |
phase_s |
|
RW |
0x3 |
|
1:0 |
phase_p |
All these registers follow the standard allocation for DLL
blocks used in PF. Please refer to the DLL SAC specification for details of
register functions. |
RW |
0x3 |
|
Address offset |
0x224 |
||
|
Physical address |
0x0704 0224 |
Instance |
MSS |
|
Description |
DLL control register 1 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
Reserved |
|
RO |
0 |
|
30 |
relock_fast |
|
RW |
0 |
|
29:24 |
init_code |
|
RW |
0x00 |
|
23 |
test_ring |
|
RW |
0 |
|
22:16 |
Reserved |
|
RO |
0x00 |
|
15 |
test_s |
|
RW |
0 |
|
14:8 |
adj_del4 |
|
RW |
0x00 |
|
7:0 |
set_alu |
|
RW |
0x00 |
|
Address offset |
0x228 |
||
|
Physical address |
0x0704 0228 |
Instance |
MSS |
|
Description |
DLL status register 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
Reserved |
|
RO |
0x00 |
|
23:16 |
Reserved |
|
RO |
0x00 |
|
15:14 |
Reserved |
|
RO |
0x0 |
|
13 |
Reserved |
|
RO |
0 |
|
12 |
phase_move_clk |
|
RW |
1 |
|
11 |
Reserved |
|
RO |
0 |
|
10 |
Reserved |
|
RO |
0 |
|
9 |
Reserved |
|
RO |
0 |
|
8 |
Reserved |
|
RO |
0 |
|
7:5 |
Reserved |
|
RO |
0x0 |
|
4 |
Reserved |
|
RO |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2 |
Reserved |
|
RO |
0 |
|
1 |
bypass |
|
RW |
1 |
|
0 |
reset |
|
RW |
1 |
|
Address offset |
0x22C |
||
|
Physical address |
0x0704 022C |
Instance |
MSS |
|
Description |
DLL status register 1 |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:30 |
Reserved |
|
RO |
0x0 |
|
29:28 |
Reserved |
|
RO |
0x0 |
|
27:26 |
Reserved |
|
RO |
0x0 |
|
25 |
Reserved |
|
RO |
0 |
|
24:16 |
sro_alu_cnt |
|
RO |
0x001 |
|
15:8 |
Reserved |
|
RO |
0x00 |
|
7 |
Reserved |
|
RO |
0 |
|
6:0 |
sro_del4 |
|
RO |
0x00 |
|
Address offset |
0x230 |
||
|
Physical address |
0x0704 0230 |
Instance |
MSS |
|
Description |
DLL status register 2 |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
Reserved |
|
RO |
0x00 |
|
23:16 |
Reserved |
|
RO |
0x00 |
|
15:7 |
Reserved |
|
RO |
0x000 |
|
6 |
Reserved |
|
RO |
0 |
|
5 |
Reserved |
|
RO |
0 |
|
4 |
Reserved |
|
RO |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2 |
sro_lock |
|
RO |
0 |
|
1 |
Reserved |
|
RO |
0 |
|
0 |
Reserved |
|
RO |
0 |
|
Address offset |
0x234 |
||
|
Physical address |
0x0704 0234 |
Instance |
MSS |
|
Description |
Enables test modes on the DLL |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:4 |
Reserved |
|
RO |
0x000 0000 |
|
3 |
reserved |
To aid synthesis - reads as zero |
RO |
0 |
|
2 |
ref_select |
When '1' the sb clock input is fed to the DLL reference |
RW |
0 |
|
1 |
cfm_select |
Feeds the MBIST clock rather than DLL clock to the CFM
block |
RW |
0 |
|
0 |
cfm_enable |
When set enables the DLL output to the frequency meter
inside the PF-Controller for test use |
RW |
0 |
|
Address offset |
0x240 |
||
|
Physical address |
0x0704 0240 |
Instance |
MSS |
|
Description |
DLL control register 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:28 |
lock_low |
|
RW |
0x8 |
|
27:24 |
lock_high |
|
RW |
0x8 |
|
23:22 |
Reserved |
|
RO |
0x0 |
|
21:20 |
lock_flt |
|
RW |
0x0 |
|
19 |
lock_frc |
|
RW |
0 |
|
18:16 |
Reserved |
|
RO |
0x0 |
|
15:14 |
alu_upd |
|
RW |
0x0 |
|
13:11 |
Reserved |
|
RO |
0x0 |
|
10 |
div_sel |
|
RW |
0 |
|
9 |
fb_sel |
|
RW |
0 |
|
8 |
ref_sel |
|
RW |
0 |
|
7:6 |
sel_s |
|
RW |
0x0 |
|
5:4 |
sel_p |
|
RW |
0x0 |
|
3:2 |
phase_s |
|
RW |
0x3 |
|
1:0 |
phase_p |
All these registers follow the standard allocation for DLL
blocks used in PF. Please refer to the DLL SAC specification for details of
register functions. |
RW |
0x3 |
|
Address offset |
0x244 |
||
|
Physical address |
0x0704 0244 |
Instance |
MSS |
|
Description |
DLL control register 1 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
Reserved |
|
RO |
0 |
|
30 |
relock_fast |
|
RW |
0 |
|
29:24 |
init_code |
|
RW |
0x00 |
|
23 |
test_ring |
|
RW |
0 |
|
22:16 |
Reserved |
|
RO |
0x00 |
|
15 |
test_s |
|
RW |
0 |
|
14:8 |
adj_del4 |
|
RW |
0x00 |
|
7:0 |
set_alu |
|
RW |
0x00 |
|
Address offset |
0x248 |
||
|
Physical address |
0x0704 0248 |
Instance |
MSS |
|
Description |
DLL status register 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
Reserved |
|
RO |
0x00 |
|
23:16 |
Reserved |
|
RO |
0x00 |
|
15:14 |
Reserved |
|
RO |
0x0 |
|
13 |
Reserved |
|
RO |
0 |
|
12 |
phase_move_clk |
|
RW |
1 |
|
11 |
Reserved |
|
RO |
0 |
|
10 |
Reserved |
|
RO |
0 |
|
9 |
Reserved |
|
RO |
0 |
|
8 |
Reserved |
|
RO |
0 |
|
7:5 |
Reserved |
|
RO |
0x0 |
|
4 |
Reserved |
|
RO |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2 |
Reserved |
|
RO |
0 |
|
1 |
bypass |
|
RW |
1 |
|
0 |
reset |
|
RW |
1 |
|
Address offset |
0x24C |
||
|
Physical address |
0x0704 024C |
Instance |
MSS |
|
Description |
DLL status register 1 |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:30 |
Reserved |
|
RO |
0x0 |
|
29:28 |
Reserved |
|
RO |
0x0 |
|
27:26 |
Reserved |
|
RO |
0x0 |
|
25 |
Reserved |
|
RO |
0 |
|
24:16 |
sro_alu_cnt |
|
RO |
0x001 |
|
15:8 |
Reserved |
|
RO |
0x00 |
|
7 |
Reserved |
|
RO |
0 |
|
6:0 |
sro_del4 |
|
RO |
0x00 |
|
Address offset |
0x250 |
||
|
Physical address |
0x0704 0250 |
Instance |
MSS |
|
Description |
DLL status register 2 |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
Reserved |
|
RO |
0x00 |
|
23:16 |
Reserved |
|
RO |
0x00 |
|
15:7 |
Reserved |
|
RO |
0x000 |
|
6 |
Reserved |
|
RO |
0 |
|
5 |
Reserved |
|
RO |
0 |
|
4 |
Reserved |
|
RO |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2 |
sro_lock |
|
RO |
0 |
|
1 |
Reserved |
|
RO |
0 |
|
0 |
Reserved |
|
RO |
0 |
|
Address offset |
0x254 |
||
|
Physical address |
0x0704 0254 |
Instance |
MSS |
|
Description |
Enables test modes on the DLL |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:4 |
Reserved |
|
RO |
0x000 0000 |
|
3 |
reserved |
To aid synthesis - reads as zero |
RO |
0 |
|
2 |
ref_select |
When '1' the sb clock input is fed to the DLL reference |
RW |
0 |
|
1 |
cfm_select |
Feeds the MBIST clock rather than DLL clock to the CFM
block |
RW |
0 |
|
0 |
cfm_enable |
When set enables the DLL output to the frequency meter
inside the PF-Controller for test use |
RW |
0 |
|
Address offset |
0x260 |
||
|
Physical address |
0x0704 0260 |
Instance |
MSS |
|
Description |
DLL control register 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:28 |
lock_low |
|
RW |
0x8 |
|
27:24 |
lock_high |
|
RW |
0x8 |
|
23:22 |
Reserved |
|
RO |
0x0 |
|
21:20 |
lock_flt |
|
RW |
0x0 |
|
19 |
lock_frc |
|
RW |
0 |
|
18:16 |
Reserved |
|
RO |
0x0 |
|
15:14 |
alu_upd |
|
RW |
0x0 |
|
13:11 |
Reserved |
|
RO |
0x0 |
|
10 |
div_sel |
|
RW |
0 |
|
9 |
fb_sel |
|
RW |
0 |
|
8 |
ref_sel |
|
RW |
0 |
|
7:6 |
sel_s |
|
RW |
0x0 |
|
5:4 |
sel_p |
|
RW |
0x0 |
|
3:2 |
phase_s |
|
RW |
0x3 |
|
1:0 |
phase_p |
All these registers follow the standard allocation for DLL
blocks used in PF. Please refer to the DLL SAC specification for details of
register functions. |
RW |
0x3 |
|
Address offset |
0x264 |
||
|
Physical address |
0x0704 0264 |
Instance |
MSS |
|
Description |
DLL control register 1 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31 |
Reserved |
|
RO |
0 |
|
30 |
relock_fast |
|
RW |
0 |
|
29:24 |
init_code |
|
RW |
0x00 |
|
23 |
test_ring |
|
RW |
0 |
|
22:16 |
Reserved |
|
RO |
0x00 |
|
15 |
test_s |
|
RW |
0 |
|
14:8 |
adj_del4 |
|
RW |
0x00 |
|
7:0 |
set_alu |
|
RW |
0x00 |
|
Address offset |
0x268 |
||
|
Physical address |
0x0704 0268 |
Instance |
MSS |
|
Description |
DLL status register 0 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
Reserved |
|
RO |
0x00 |
|
23:16 |
Reserved |
|
RO |
0x00 |
|
15:14 |
Reserved |
|
RO |
0x0 |
|
13 |
Reserved |
|
RO |
0 |
|
12 |
phase_move_clk |
|
RW |
1 |
|
11 |
Reserved |
|
RO |
0 |
|
10 |
Reserved |
|
RO |
0 |
|
9 |
Reserved |
|
RO |
0 |
|
8 |
Reserved |
|
RO |
0 |
|
7:5 |
Reserved |
|
RO |
0x0 |
|
4 |
Reserved |
|
RO |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2 |
Reserved |
|
RO |
0 |
|
1 |
bypass |
|
RW |
1 |
|
0 |
reset |
|
RW |
1 |
|
Address offset |
0x26C |
||
|
Physical address |
0x0704 026C |
Instance |
MSS |
|
Description |
DLL status register 1 |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:30 |
Reserved |
|
RO |
0x0 |
|
29:28 |
Reserved |
|
RO |
0x0 |
|
27:26 |
Reserved |
|
RO |
0x0 |
|
25 |
Reserved |
|
RO |
0 |
|
24:16 |
sro_alu_cnt |
|
RO |
0x001 |
|
15:8 |
Reserved |
|
RO |
0x00 |
|
7 |
Reserved |
|
RO |
0 |
|
6:0 |
sro_del4 |
|
RO |
0x00 |
|
Address offset |
0x270 |
||
|
Physical address |
0x0704 0270 |
Instance |
MSS |
|
Description |
DLL status register 2 |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:24 |
Reserved |
|
RO |
0x00 |
|
23:16 |
Reserved |
|
RO |
0x00 |
|
15:7 |
Reserved |
|
RO |
0x000 |
|
6 |
Reserved |
|
RO |
0 |
|
5 |
Reserved |
|
RO |
0 |
|
4 |
Reserved |
|
RO |
0 |
|
3 |
Reserved |
|
RO |
0 |
|
2 |
sro_lock |
|
RO |
0 |
|
1 |
Reserved |
|
RO |
0 |
|
0 |
Reserved |
|
RO |
0 |
|
Address offset |
0x274 |
||
|
Physical address |
0x0704 0274 |
Instance |
MSS |
|
Description |
Enables test modes on the DLL |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:4 |
Reserved |
|
RO |
0x000 0000 |
|
3 |
reserved |
To aid synthesis - reads as zero |
RO |
0 |
|
2 |
ref_select |
When '1' the sb clock input is fed to the DLL reference |
RW |
0 |
|
1 |
cfm_select |
Feeds the MBIST clock rather than DLL clock to the CFM
block |
RW |
0 |
|
0 |
cfm_enable |
When set enables the DLL output to the frequency meter
inside the PF-Controller for test use |
RW |
0 |
|
Address offset |
0x278 |
||
|
Physical address |
0x0704 0278 |
Instance |
MSS |
|
Description |
dpc values
for MSSIO bank 2 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:15 |
Reserved |
|
RO |
0x0 0000 |
|
14 |
dpc_io_cfg_lp_bypass_en |
|
RW |
0 |
|
13 |
dpc_io_cfg_lp_persist_en |
|
RW |
0 |
|
12 |
dpc_io_cfg_atp_en |
|
RW |
0 |
|
11 |
dpc_io_cfg_wpu |
|
RW |
1 |
|
10 |
dpc_io_cfg_wpd |
|
RW |
0 |
|
9 |
dpc_io_cfg_lockdn_en |
|
RW |
0 |
|
8 |
dpc_io_cfg_enhyst |
|
RW |
0 |
|
7 |
dpc_io_cfg_clamp |
|
RW |
0 |
|
6 |
dpc_io_cfg_drv_3 |
|
RW |
0 |
|
5 |
dpc_io_cfg_drv_2 |
|
RW |
1 |
|
4 |
dpc_io_cfg_drv_1 |
|
RW |
0 |
|
3 |
dpc_io_cfg_drv_0 |
|
RW |
1 |
|
2 |
dpc_io_cfg_ibufmd_2 |
|
RW |
0 |
|
1 |
dpc_io_cfg_ibufmd_1 |
|
RW |
0 |
|
0 |
dpc_io_cfg_ibufmd_0 |
|
RW |
0 |
|
Address offset |
0x27C |
||
|
Physical address |
0x0704 027C |
Instance |
MSS |
|
Description |
dpc values
for MSSIO bank 4 |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
|
31:15 |
Reserved |
|
RO |
0x0 0000 |
|
14 |
dpc_io_cfg_lp_bypass_en |
|
RW |
0 |
|
13 |
dpc_io_cfg_lp_persist_en |
|
RW |
0 |
|
12 |
dpc_io_cfg_atp_en |
|
RW |
0 |
|
11 |
dpc_io_cfg_wpu |
|
RW |
1 |
|
10 |
dpc_io_cfg_wpd |
|
RW |
0 |
|
9 |
dpc_io_cfg_lockdn_en |
|
RW |
0 |
|
8 |
dpc_io_cfg_enhyst |
|
RW |
0 |
|
7 |
dpc_io_cfg_clamp |
|
RW |
0 |
|
6 |
dpc_io_cfg_drv_3 |
|
RW |
0 |
|
5 |
dpc_io_cfg_drv_2 |
|
RW |
1 |
|
4 |
dpc_io_cfg_drv_1 |
|
RW |
0 |
|
3 |
dpc_io_cfg_drv_0 |
|
RW |
1 |
|
2 |
dpc_io_cfg_ibufmd_2 |
|
RW |
0 |
|
1 |
dpc_io_cfg_ibufmd_1 |
|
RW |
0 |
|
0 |
dpc_io_cfg_ibufmd_0 |
|
RW |
0 |
PF_MSS_TOP_SCB_REGS
has no common memories.