.. _INCLUDE_INST_IN_FSM_DOT_GRAPH: INCLUDE_INST_IN_FSM_DOT_GRAPH ------------- This constraint enables including instruction labels in the state node labels in the FSM's generated dot graph. Category +++++++++ Miscellaneous Value Type +++++++++++ Integer Valid Values +++++++++++++ 0, 1 Default Value ++++++++++++++ unset (0) Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Untested Examples +++++++++ ``set_parameter INCLUDE_INST_IN_FSM_DOT_GRAPH 1`` --------------------------------------------------------------------------------