.. _DFG_SHOW_DUMMY_CALLS: DFG_SHOW_DUMMY_CALLS -------------------- Show dummy calls such as printf in the dataflow dot graphs. Category +++++++++ Debugging Value Type +++++++++++ Integer Valid Values +++++++++++++ 0, 1 Default Value ++++++++++++++ unset (0, dummy calls ignored) Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ :ref:`NO_DFG_DOT_FILES` should be disabled Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Actively in-use Examples +++++++++ ``set_parameter DFG_SHOW_DUMMY_CALLS 1`` --------------------------------------------------------------------------------