.. _DEBUG_SDC_CONSTRAINTS: DEBUG_SDC_CONSTRAINTS ---------------------- This parameter prints all the SDC constraints during modulo scheduling into the pipelining.legup.rpt file. Category +++++++++ Debugging Value Type +++++++++++ Integer Valid Values +++++++++++++ 0, 1 Default Value ++++++++++++++ 0 Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Actively in-use Examples +++++++++ ``set_parameter DEBUG_SDC_CONSTRAINTS 1`` --------------------------------------------------------------------------------