.. highlight:: c .. _hwarch: Hardware Architecture ====================== This section describes the hardware architecture produced by LegUp. Circuit Topology ---------------- Each C/C++ function corresponds to a hardware module in Verilog. For instance, if we have a software program with the following call graph: .. image:: /images/callgraph_new.* :scale: 75 % :align: center where ``main`` calls ``a`` and ``b``, which in turn call ``c`` and ``d``. Notice that function ``c`` is called by both ``a`` and ``b``. One way to create this system in hardware is to instantiate one module within another module, in a nested hierarchy, following how the functions are called in software: .. image:: /images/circuit_arch_nested.* :scale: 75 % :align: center This architecture is employed by some of the other HLS tools, but it can create an unnecessary replication of hardware. Notice how module ``c`` has to be created twice, since the function ``c`` is called from different parent functions. In LegUp, we instantiate all module at the same level of hierarchy, and automatically create the necessary interconnect to connect them together. .. image:: /images/circuit_arch_flat.* :align: center This prevents modules from being unnecessarily replicated, saving area. The hardware system may also use a functional unit (denoted as ``FU`` in the figure), such as a floating-point unit, which is also created at the same level. This architecture also allows such units, which typically consume a lot of area, to be shared between different modules. .. NOTE:: For a small function, or for a function that is only called once in software, LegUp may decide to ``inline`` the function into its parent function to improve performance. Any inlined function is included as part of its parent function, so there will not be a separate module in the Verilog for the inlined function. Thus you may not find all the software functions in the generated hardware. Threaded Hardware Modules ^^^^^^^^^^^^^^^^^^^^^^^^^ When Pthreads are used in software, LegUp automatically compiles them to concurrently executing modules. This is synonymous to how multiple threads are compiled to execute on multiple processor cores in software. By default, each thread in software becomes an independent hardware module. For example, forking three threads of function ``a`` in software creates three concurrently executing instances of module ``a`` in hardware. .. In a processor-accelerator hybrid system, each thread is compiled to a concurrently executing hardware accelerator. .. _mem_arch: Memory Architecture -------------------- LegUp stores any arrays (local or global) and global variables in a memory. We describe below what type of memories they are, as well as where the memories are stored. .. In LegUp, there exists four hierarchies of memories: 1) Local memory, 2) shared-local memory, 3) aliased memory, and 4) processor memory. In LegUp, there exists four hierarchies of memories: 1) Local memory, 2) shared-local memory, 3) aliased memory, and 4) I/O memory. Local, shared-local, and aliased memories exist in the generated hardware. .. In a hardware-only system, only the first three levels of memories exist. .. In a processor-accelerator hybrid system, all four levels of memories exist. I/O memories are used data that are inputs/output to/from the generated hardware. They exist outside of the generated hardware (LegUp does not instantiate memories for them), where top-level memory interfaces are created for them. .. Any data that is only accessed by an accelerator is stored on the accelerator side. .. Any data that is only accessed by the processor, or is shared between multiple accelerators, .. or is shared between an accelerator and the processor, is stored in processor memory. .. The processor memory consists of an off-chip memory and on-chip cache. .. The processor and all hardware accelerators have access to the on-chip cache. .. For the processor-accelerator hybrid architecture, see the `ARM Processor-Accelerator Hybrid Architecture`_ section below. Local Memory ^^^^^^^^^^^^^^^^^ LegUp uses points-to analysis to determine which memories are used by which functions. If a memory is determined to be used by a single function, where the function is to be compiled to hardware, that array is implemented as a local memory. A local memory is created and connected directly inside the module that accesses it. Local memories have a latency of 1 clock cycle by default. The local memory latency can be changed with the :ref:`set_operation_latency` Tcl parameter. Shared-Local Memory ^^^^^^^^^^^^^^^^^^^ If a memory is accessed by multiple functions, where all the functions that access it are to be compiled to hardware, the memory is designated as a shared-local memory. A shared-local memory is instantiated outside the modules (at the same level of hierarchy as the modules themselves, as shown above), and memory ports are created for the modules to connect to the memory. Arbitration is automatically created to handle contention for a shared-local memory. LegUp automatically optimizes the arbitration logic, so that if the modules that access the memory are executing sequentially, a simple ``OR`` gate is used for arbitration (which consumes only a small amount of area), but if the accessing modules are executing concurrently (with the use of ``Pthreads``), a round-robin arbiter is automatically created to handle contention. Shared-local memories have a latency of 1 clock cycle. The shared-local memory latency can be changed with the :ref:`set_operation_latency` Tcl parameter. Aliased Memory ^^^^^^^^^^^^^^^^^ There can be cases where a pointer can point to multiple arrays, causing pointer aliasing. These pointers need to be resolved at runtime. We designate the memories that such a pointer can refer to as aliased memories, which are stored in a memory controller (described below). A memory controller contains all memories that can alias to each other, and allows memory accesses to be steered to the correct memory at runtime. There can be multiple memory controllers in a system, each containing a set of memories that alias to each other. Aliased memories have a latency of 2 clock cycles. The aliased memory latency can be changed with the :ref:`set_operation_latency` Tcl parameter. Memory Controller ~~~~~~~~~~~~~~~~~ The purpose of the memory controller is to automatically resolve pointer ambiguity at runtime. The memory controller is only created if there are aliased memories. The architecture of the memory controller is shown below: .. image:: /images/memory_controller.* :align: center For clarity, some of the signals are combined together in the figure. Even though the figure depicts a single-ported memory, all memories are dual-ported by default, unless only a single memory access is needed per cycle, in which case it will be single-ported memory. The memory controller steers memory accesses to the correct RAM, by using a tag, which is assigned to each aliased memory by LegUp. At runtime, the tag is used to determine which memory block to enable, with all other memory blocks disabled. The same tag is used to select the correct output data between all memory blocks. .. Processor Memory .. ^^^^^^^^^^^^^^^^^ The processor memory consists of the on-chip cache and off-chip memory in the processor-accelerator hybrid flow. Any memories which are accessed by functions running on the processor are stored in off-chip memory and can be brought into the on-chip cache during program execution. Memories that are shared between multiple accelerators are also stored in this shared memory space. In case of aliased memories, if a pointer that aliases points to a memory that is accessed by the processor, then all of the memories that the pointer aliases to are stored in this shared memory space. .. _io_memory: I/O Memory ^^^^^^^^^^^^^^^^^ Any memory that is accessed by both the software testbench (parent functions of the top-level function) and hardware functions (the top-level functions and its descendants) becomes an I/O memory. These are any non-constant arguments for top-level function or global variables that are accessed by both the software testbench and hardware functions. I/O memories become memory interfaces of the top-level module for the generated hardware, where no actual memories are instantiated within the generated hardware for them. For more information on interfaces, please refer to :ref:`rtl_interface`. Memory Storage ^^^^^^^^^^^^^^^^^ By default, each local, shared-local, and aliased memories are stored in a separate dual-ported on-chip RAM, where each RAM allows two accesses per clock cycle. All local memories can be accessed in parallel. All shared-local memories can be accessed concurrently when there are no accesses to same memory in the same clock cycle. If there are concurrent accesses to the same RAM, our arbitration logic handles the contention automatically and stalls the appropriate modules. All independent memory controllers can also be accessed in parallel, but aliased memories which belong to the same memory controller must be accessed sequentially. Memory Optimizations ~~~~~~~~~~~~~~~~~~~~ LegUp automatically stores each single-element global variable (non-array) in a set of registers, rather than a block RAM, to reduce memory usage and improve performance. A block RAM has a minimum read latency of 1 clock cycle, where a register can be read in the same clock cycle (0 cycle latency). For small arrays, LegUp may decide to split them up and store individual elements in separate registers. This allows all elements to be accessed at the same time. If an array is accessed in a loop, and the loop is unrolled, LegUp also may decide to split up the array. If only up to a single memory accessed is needed per cycle for a memory, LegUp will instantiate a single-ported RAM, otherwise a dual-ported RAM will be used. If a memory is only ever read from, LegUp will convert the memory to a read-only memory (ROM), even if the corresponding array is not declared as a constant in software. If a memory is not accessed at all, LegUp will automatically optimize away the memory. .. For constant arrays, which are stored in read-only memories (ROM), the user can choose to replicate them for each function that accesses them. This can be beneficial when the constant array is accessed frequently by multiple threads (in Pthreads/OpenMP). By creating a dedicated memory for each thread, it localizes the memory to each thread, making the constant array a local memory of each threaded module. This can improve performance by reducing stalls due to contention, and also save the resource of arbitration logic. This feature can be enabled with the ``Replicate ROM to each accessing module`` constraint in LegUp. The figure below shows an example architecture with Pthread modules and all of the memories that we have described for a hardware-only system. The ``main`` function forks two threads of function ``d``, hence two instances of ``d`` are created. ``main``, ``d0``, and ``d`` all execute in parallel, and they share the memory controller, shared-local memories 0 and 1, a register module, as well as a hardware lock module. The hardware lock module is automatically created when a mutex is used in software. All arbitration logic shown are round-robin arbiters, as all of the modules execute in parallel. A local memory that is used only by ``main`` is instantiated inside the module, and ``d0`` and ``d1`` have replicated constant memories instantiated inside. .. image:: /images/architecture_with_all_memories.* :align: center Interfaces ----------- Please refer to the :ref:`rtl_interface` section for a detailed description on the interfaces that are created by LegUp. .. comment LegUp generates a number different interfaces for functions and memories. For instance, if we have the following C prototypes:: int FunctionA(int a, int *mem, legupFIFO &fifo); void FunctionB(FIFO &fifo); where FunctionA calls FunctionB, with a FIFO being written to in FunctionA and read from in FunctionB, LegUp can generate the following module interfaces. .. code-block:: v module FunctionA ( // default interface input clk, input reset, input start, output reg finish, input memory_controller_waitrequest, // for return value output reg [31:0] return_val, // for argument input [31:0] arg_a, // for calling FunctionB output FunctionB_start, input FunctionB_finish, // for accessing mem pointer output reg [7:0] mem_address_a, output reg mem_enable_a, output reg mem_write_enable_a, output reg [31:0] mem_in_a, input [31:0] mem_out_a, output reg [7:0] mem_address_b, output reg mem_enable_b, output reg mem_write_enable_b, output reg [31:0] mem_in_b, input [31:0] mem_out_b, // for writing to fifo input fifo_ready_from_sink, output fifo_valid_to_sink, output [31:0] fifo_data_to_sink ) module FunctionB ( // default interface input clk, input reset, input start, output reg finish, input memory_controller_waitrequest, // for reading from fifo input fifo_ready_to_source, output fifo_valid_from_source, output [31:0] fifo_data_from_source ) As seen above, each module contains a number of default interface signals, ``clk``, ``reset``, ``start,`` and ``finish``. The start/reset signals are used by the first state of the state machine: .. image:: /images/first_state.* :align: center The finish signal is kept low until the last state of the state machine, where finish is set to 1. The ``memory_controller_waitrequest`` signal is the stall signal for the module, which when asserted, stalls the entire module. Since FunctionA has a return type of ``int``, it has a 32-bit ``return_val`` output. Each scalar argument becomes an input to the module. The ``int a`` argument creates the 32-bit ``arg_a`` input. In the C program, FunctionA calls FunctionB, hence LegUp creates handshaking signals between the two modules. When the output signal ``FunctionB_start`` is asserted, FunctionB starts executing. FunctionA then waits until the input signal ``FunctionB_finish`` is asserted. This is in line with the sequential executing behavior of software. However, when Pthreads is used, the caller module continues to execute after forking its threaded modules. In FunctionA, memory signals for the ``mem`` pointer argument are also shown. In this case, mem is designated as a shared-local memory and created outside the module, hence memory ports are created to access the memory. Two ports are created for the memory to allow two accesses per clock cycle. Note that if a pointer is passed into a function, but LegUp determines that the array the pointer refers to is only accessed by the function, the memory will be designated as a local memory and be instantiated within the module (removing the need for memory ports). The following memory signals are shown: ================== ============================= Memory Signal Type Description ================== ============================= address Address of memory. enable 1 if reading or writing in this clock cycle write_enable 1 for write, 0 for read in Data being read from memory out Data being written to memory ================== ============================= The width of the address bus is determined by the depth of the memory. The ``fifo`` argument is given to both FunctionA and FunctionB, where FunctionA writes to the FIFO and FunctionB reads from the FIFO. LegUp currently does not allow the same function to both write to and read from the same FIFO. In this case, the sink (reader) is FunctionB and the source (writer) is FunctionA. ================== ============================= FIFO Signal Type Description ================== ============================= ready Indicates whether the sink is ready to receive data valid Indicates whether this data is valid data Data being sent ================== ============================= Register Interface ^^^^^^^^^^^^^^^^^^^^^^^^^^ If a memory is a single element (a single-element global variable or an array with a single element), LegUp will simply the memory interface to a register interface. A register interface has the following signals: ==================== ============================= Register Signal Type Description ==================== ============================= write_enable 1 for write readdata Data being read writedata Data being written ==================== ============================= If the single-element memory is only ever read from (read-only), LegUp will further simply the interface by default to the following: ==================== ============================= Register Signal Type Description ==================== ============================= readdata Data being read ==================== ============================= If the single-element memory is only ever written to (write-only), LegUp will simply the interface by default to the following: ==================== ============================= Register Signal Type Description ==================== ============================= write_enable 1 for write writedata Data being written ==================== ============================= If the single-element memory is only ever written to (write-only), and the user only wants the writedata port at the top-level, user can use ``set_argument_interface_type wire -always_valid`` Tcl command. This will create the following port at the top-level: ==================== ============================= Register Signal Type Description ==================== ============================= writedata Data being written ==================== ============================= User may want the written data to be stored and held constant when written to the top-level interface. If the single-element memory is only ever written to (write-only), user can use ``set_argument_interface_type register`` Tcl command. This will instantiate a register inside the top-level module where the single-element will be written to and stored, and the output of the register will be connected to the top-level interface, so that the data outputted is held constant. The top-level will only have the following port: ==================== ============================= Register Signal Type Description ==================== ============================= writedata Data being written ==================== ============================= AXI Slave Interface (Beta) ^^^^^^^^^^^^^^^^^^^^^^^^^^ LegUp currently provides Beta support for AXI Slave Interface. Please refer to the user guide for more details.