Instantiating LegUp IP Core in Libero SmartDesign ------------------------------------------------- After we use LegUp HLS to design a hardware IP component, we will want to instantiate the component into Libero SmartDesign and integrate this core into our larger system. When LegUp HLS generates the hardware, LegUp will also generate a ``create_hdl_plus.tcl`` script to easily instantiate the LegUp-generated IP core into Libero SmartDesign. You will see the log message in the console which includes the full path to the script like this: .. code-block:: text Info: Generating HDL+ Tcl script to be imported in SmartDesign: /cygdrive/c/LegUp-9.0/workspace/sobel_part3/create_hdl_plus.tcl. This is a Cygwin path. You can replace ``/cygdrive/c/`` with ``C:\\``, so the Windows path in the above example is: .. code-block:: text C:\LegUp-9.0\workspace\sobel_part3\create_hdl_plus.tcl. Now we can open Libero and create a new SmartDesign (or open an existing SmartDesign) as shown in the figure below. .. image:: /images/create_SmartDesign_in_Libero.png :scale: 100 % :align: center We now go to the Libero ``Projects`` menu and select ``Execute Script`` and give the path to the generated ``create_hdl_plus.tcl`` script as shown in the figures below. Then click ``Run``. Running the Tcl script will add the LegUp-generated HDL+ component (``sobel_filter_top`` in this example), all required Verilog files, memory initialization files, and other dependencies to the Libero project. .. image:: /images/projects_execute_script.png :scale: 100 % :align: center .. image:: /images/execute_script.png :scale: 100 % :align: center As shown in the figures below, we can now instantiate the component in SmartDesign by right-clicking on the HDL+ component (``sobel_filter_top`` in this example) in the ``Design Hiearchy`` panel on the left and selecting ``Instantiate in system``. In the SmartDesign system we will now see the new IP component (``sobel_filter_top_0`` in this example). .. image:: /images/instantiate_in_system.png :scale: 100 % :align: center .. image:: /images/new_IP_component.png :scale: 100 % :align: center The generated ``create_hdl_plus.tcl`` script will automatically group ports as AXI4-Master, AXI4-Slave or AXI4-Stream interfaces if they match the corresponding AXI4 specifications. In this example, since the ``sobel_filter_top`` IP component used LegUp FIFOs as top-level arguments and they match AXI4-Stream specifications, LegUp has automatically grouped the ``output_fifo`` and ``input_fifo`` data/ready/valid ports as AXI4-Stream interfaces.