.. _set_memory_local: set_memory_local ----------------- This parameter can be used to force a particular array to be placed in local memory instead of global memory. Category +++++++++ HLS Constraints Value Type +++++++++++ String Valid Values +++++++++++++ Array name Default Value ++++++++++++++ None Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ LOCAL_RAMS Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ No longer in-use Examples +++++++++ ``set_memory_local JpegFileBuf`` --------------------------------------------------------------------------------