.. _set_legup_output_path: set_legup_output_path --------------------- This parameter sets the output path for all LegUp generated files. Only subdirectories of the current path are allowed. The makefile will create the full path, while the clean target will remove it. Category +++++++++ Miscellaneous Value Type +++++++++++ String Valid Values +++++++++++++ All alphanumeric strings Default Value ++++++++++++++ ``output`` Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Actively in-use Examples +++++++++ ``set_legup_output_path output`` --------------------------------------------------------------------------------