.. _TEST_WAITREQUEST: TEST_WAITREQUEST ------------- Test handling of the waitrequest signal by setting waitrequest high of 5 cycles at the beginning of every transfer. This should have no impact on circuit functionality but just make the total cycle count about 5x higher. Category +++++++++ Debugging Value Type +++++++++++ Integer Valid Values +++++++++++++ 0, 1 Default Value ++++++++++++++ unset (0) Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Untested Examples +++++++++ ``set_parameter TEST_WAITREQUEST 1`` --------------------------------------------------------------------------------