.. _SYSTEM_PROJECT_NAME: SYSTEM_PROJECT_NAME ------------- The name of the directory containing the project and system to be used by the software and hybrid makefile targets. The directory must also include a legup.tcl file that describes the Qsys system. This constraint is set in the set_project function and should not be set independently. Category +++++++++ Board and Device Specification Value Type +++++++++++ String Valid Values +++++++++++++ Any valid directory name Default Value ++++++++++++++ Tiger_SDRAM Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ Software and hybrid flows Test Status ++++++++++++ Actively in-use Examples +++++++++ ``set_parameter SYSTEM_PROJECT_NAME Tiger_SDRAM`` --------------------------------------------------------------------------------