.. _NO_ROMS: NO_ROMS ------------- This parameter places constant arrays into RAMs instead of the default read-only memory. Category +++++++++ HLS Constraints Value Type +++++++++++ Integer Valid Values +++++++++++++ 0, 1 Default Value ++++++++++++++ 0 Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Actively in-use Examples +++++++++ ``set_parameter NO_ROMS 1`` --------------------------------------------------------------------------------