.. _loop_pipeline: loop_pipeline ------------- This parameter enables pipelining for a given loop in the code. Loop pipelining allows a new iteration of the loop to begin before the current one has completed, achieving higher throughput. Optional arguments: +--------------------+-----------------------------------------------------------------------+ | Parameter | Description | +====================+=======================================================================+ | -ii | Specify a pipeline initiation interval (default = 1) | +--------------------+-----------------------------------------------------------------------+ | -ignore-mem-deps | Ignore loop carried dependencies for all memory accesses in the loop | +--------------------+-----------------------------------------------------------------------+ Category +++++++++ HLS Constraints Value Type +++++++++++ +--------------------+------------+ | Parameter | Value Type | +====================+============+ | loop_pipeline | String | +--------------------+------------+ | -ii | Integer | +--------------------+------------+ | -ignore-mem-deps | None | +--------------------+------------+ Valid Values +++++++++++++ See Examples Default Value ++++++++++++++ N/A Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Actively in-use Examples +++++++++ ``loop_pipeline "loop1"`` ``loop_pipeline "loop2" -ii 1`` ``loop_pipeline "loop3" -ignore-mem-deps`` --------------------------------------------------------------------------------