.. _PRINT_STATES: PRINT_STATES ------------- When this parameter is enabled, the cur_state of each function will be displayed at every clock cycle in simulation. Category +++++++++ Simulation Value Type +++++++++++ Integer Valid Values +++++++++++++ 0, 1 Default Value ++++++++++++++ unset (0) Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Actively in-use Examples +++++++++ ``set_parameter PRINT_STATES 1`` --------------------------------------------------------------------------------