.. _PATTERN_SHARE_SUB PATTERN_SHARE_SUB ------------- Select which instructions to share in pattern sharing. Choices are: Adders / Subtractors Bitwise operations (AND, OR, XOR) Shifts (logical shift Left/Right and arithmetic shift Right) If set, these instructions will be included in patterns and shared with 2-1 muxing. Note that multipliers, dividers and remainders are not shared in patterns because they should be shared with more than 2-1 muxing (if at all). The bipartite binding algorithm is used for those instructions while pattern sharing is used for the smaller instructions above. This particular parameter pertains to sharing subtract. This parameter does NOTHING unless ENABLE_PATTERN_SHARING is 1. Paper: Stefan Hadjis, Andrew Canis, Jason Helge Anderson, Jongsok Choi, Kevin Nam, Stephen Dean Brown, Tomasz S. Czajkowski, "Impact of FPGA architecture on resource sharing in high-level synthesis," FPGA 2012: 111-114 Category +++++++++ HLS Constraints Value Type +++++++++++ Integer Valid Values +++++++++++++ 0 or 1 Default Value ++++++++++++++ 0 (for Cyclone II); 1 (for all other archs with 6-LUTs) Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ ENABLE_PATTERN_SHARING Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Actively in-use Examples +++++++++ ``set_parameter PATTERN_SHARE_SUB 1'' --------------------------------------------------------------------------------