.. _DUAL_PORT_BINDING: DUAL_PORT_BINDING ----------------- Enabling this parameter results in use of the dual-ported on-chip memories, allowing up to two memory accesses per clock cycle. Category +++++++++ HLS Constraints Value Type +++++++++++ Integer Valid Values +++++++++++++ 0, 1 Default Value ++++++++++++++ 1 (On) Location Where Default is Specified +++++++++++++++++++++++++++++++++++ ``examples/legup.tcl`` Dependencies +++++++++++++ None Applicable Flows +++++++++++++++++ All devices and flows Test Status ++++++++++++ Actively in-use Example +++++++++ ``set_parameter DUAL_PORT_BINDING 1`` -----------------------------------------------------------------------------------------------------