README for Mircochip XC8-AVR GNU Toolchain v2.40 Sources 
              =========================================================


This directory contains the complete modified source code of various open source
software that was used for building the Microchip XC8 AVR GNU Toolchain v2.40.


CONTENTS
========

1. avr-binutils.tar.bz2

   Binutils 2.26.20160125 with the modifications in AVR target

2. avr-gcc.tar.bz2

   GCC 5.4.0 with the modifications in AVR target

3. avr-libc.tar.bz2

   AVR libc "2.0.0" with the modifications

4. avr8-headers.zip

   Header files for AVR 8 bit devices

6. build-avr8-gnu-toolchain-git.sh

   Script to build the toolchain



HOW TO BUILD?
=============

Preparation:

1. Create directories for build <bld>, source <src>, and install <install>
  

2. Extract the source tarballs for binutils, gcc and avr-libc 
   to <src>, and copy the avr8-headers zip to <src>/headers/.


3. Building the toolchain has following dependencies:

   gmp-5.0.2
   mpfr-3.0.0
   mpc-0.9
   ncurses-5.9

   They may be obtained from their respective project websites. The tarballs
   of these should be copied to the following directories:

   - gmp tar.gz file to <src>/gmp/
   - mpfr tar.gz file to <src>/mpfr/
   - mpc tar file to <src>/mpc/
   - ncurses tar file to <src>/ncurses/

   libxml2-2.9.7
   - This should be installed, library and include path should be in CXXFLAGS


4. In order to build, issue the following command


   bash build-avr8-gnu-toolchain-git.sh -b <bld> -p <install> -s <src> 


   Note 1: If the binaries are required to be installed in the default 
           directories, one may use  -P <root-passwd>  option to pass the root 
           password.

   Note 2: This current version assumes that the build environment has the 
           following present and available:

           - automake-1.11.1
           - autoconf-2.64
           - texinfo-4.13


--------------------------------------------------------------------------------