The Dialog gets invoked by selecting Example Project… from the File->New menu. It can also be invoked using the shortcut: Ctrl+Shift+E

Or by invoking the icon from the Atmel Studio toolbar shown below :

ASF distributes more than one release versions. To create an example project for a specific version, user can select the appropriate ASF Version form the ComboBox shown in above diagram, and proceed.

The Dialog proposes different categories for choosing the ready to use Atmel Software Framework projects. These projects are listed under following categories.