• Body Electronics 
  • Chassis
  • Drivers Assistance
  • Instrumentation
  • Lighting Control
  • Powertrain
  • Safety/Security

Electronic Compass System

Auto dimming rear view mirrors not only increase driving safety but provide the car OEM with a cost effective way to deliver value added features, such as electronic compass, to the driver. The electronic compass system determines the direction in which the car is heading as it senses the absolute position and the change in direction of the car using the earth’s magnetic field as a reference. The direction can be displayed using a low end segmented LCD integrated with the auto dimming rear view mirror or in conjunction with the vehicle’s on board navigation display. The sensor technology utilized is commonly either magnetoresistive or inductive sensors.

Design Considerations:

  • Robust, General Purpose performance oriented microcontroller with small footprint.
  • Flexible Sensor Interface
  • Signal Conditioning Hardware

Design Solutions:

  • PIC16, PIC18 and PIC24 microcontrollers enable a broad array of diverse on-chip peripherals from IIC to CCP to ADC to SR Latch to CTMU to provide the system designer with an opportunity to match the appropriate peripheral set with the sensing methodology utilized within the electronic compass system. Even with on-chip ADC of the microcontroller, the output signal generated by magnetoresistive sensors generally has a low level requiring amplification using either on-chip operational amplifiers or standalone differential amplifiers, depending on available board space.
  • Whereas when inductive sensors are used they are connected to a known resistance value in order to create a LR oscillator circuit. When the car changes position, the inductance of the system changes. As a result the frequency of the circuit changes.
  • The output signal generated by the Magnetoresistive sensors is generally of a low magnitude, which needs to be amplified for before being fed into the ADC module. Microchip provides the user with the option of using stand alone differential amplifiers or using integrated amplifiers, which saves external component cost and board space. (Most?) Microchip microcontrollers also have on board ADC modules, providing the user greater control and flexibility to use the signal data.
  • The Inductive Sensors are connected to a known resistance value in order to create a LR oscillator circuit. With change in position, the inductance of the system changes, hence the frequency of the circuit changes. Timing algorithms developed for the PICmicrocontrollers enable the system to measure the change in frequency of the circuit, to measure the change in inductance value, and process the data to determine the direction of change.
  • The on-chip EEPROM peripheral of PICmicrocontrollers or standalone SEE provide the system designer with a non-volatile memory array to store system variables that may be recovered to identify the last known settings / conditions.
  • Utilizing PICmicrocontrollers with on-chip LCD modules support the direct drive of the LCD display eliminating the need for a incremental LCD driver chip. A Graphics library is readily available to support the system designer’s code development efficiency.
  • With on-chip peripherals to support LIN and CAN communication protocols, the system designer is able to choose the appropriate PICmicrocontroller that matches the overall system requirements. Plus CAN and LIN transceivers options are available to the system designer for the physical layers interface requirements.