LED Applications
The benefits of LED lighting can be appreciated in many types of lighting applications:
• Automotive and aircraft cabin lighting
• Automotive and aircraft instrument panel lighting
• Architectural emergency exit lighting
• Architectural color effect lighting
• Industrial and outdoor lighting
• Traffic and railway signals Automotive Brake Lights
• Dot matrix signs and video displays
• LCD display backlighting
• Personal flashlights
• Medical instrument and tool lighting
• Digital camera flash and video light
Efficient LED Control
LEDs must be driven with a source of constant current. Most LEDs have a specified current level that will achieve the maximum brightness for that LED without premature failures. LEDs could be driven with a linear voltage regulator configured as a constant current source. However, this approach is not practical for higher power LEDs due to power dissipation in the regulator circuit.
A switch-mode power supply (SMPS) provides a much more efficient solution to drive the LED. An LED will have a forward voltage drop across its terminals for a given current drive level. The input supply voltage and the LED forward voltage characteristics determine the SMPS topology that is required.
Multiple LEDs can be connected in series to increase the forward voltage drop at the chosen drive current level. The SMPS circuit topologies adopted to regulate current in LED lighting applications are the same used to control voltage in a power supply application. Each type of SMPS topology has its advantages and disadvantages as presented in the table below.
|