Introduction to Ethernet
Functional Overview
TCP/IP Download & Support
Application Ideas
Development Tools
Recommended Parts
Frequently Asked Questions (FAQs)
  Featured Products
 

  ENC624J600
 
 
 
 

  PIC18F97J60 Family
 
 
 
 

  ENC28J60
 
 
 
 

  MAC Address Chips
 
 
 

This section describes some application examples that can make use of Microchip’s Ethernet solution. The examples include IP Security Camera, Vending Machine, Internet Radio and Ethernet Gateway.

IP Security Camera

In this example, a video camera is connected via Ethernet to the Internet. Real time video can be streamed to any location with an IP address. It is also possible to control the camera remotely, to pan and zoom on new subjects. Applications include home surveillance while at work, or surveillance of a second home, boat, or other remote location.

Figure 3

Vending Machine

In this example, a vending machine is connected via Ethernet to the Internet. Real time information, such as the amount of money, inventory status, or operating condition of the machine video can be streamed to any location with an IP address. The added cost is more than compensated by the improved efficiency made possible by reporting made possible through the IP connection. Price changes could also be done remotely.

Figure 4

Internet Radio

In this example, streaming audio is received via Ethernet from the Internet. Radio channels become IP addresses, and the service can be free or by paid subscription. The quality of service (reception) can be greatly improved, and the content controlled via use of Ethernet.

    Figure 5

Ethernet Gateway

In this example, a thermostat is connected via Ethernet to the Internet. Real time information, such as the current temperature and humidity, can be streamed to any location with an IP address. The settings can be changed remotely – settings for new cycle time and temperatures can be updated easily thru the Internet

Figure 6

Back to TCP/IP, Continue to Tools