AN650 - Designing a Transponder Coil for the HCS410 - Application Notes - Details
  Application Notes/
Technical Brief
Application Notes
Application Notes by Release Date
Application Notes (alphabetical)
Application Notes - Source Code
SPICE Models
AN650
Title: Designing a Transponder Coil for the HCS410
Name: AN650
Date: 6/9/11
Author: Mike Sonnabend, Janvan Niekerk
Description: This application note explains the design of transponder coils. An Excel spreadsheet is used to automate the update of values, depending on the specified parameters. The spreadsheet file name is transpnd.xls. A zip file containing this spreadsheet and a copy of this application note can be downloaded from Microchip?s web site at www.microchip.com. The basic approach is to choose the transponder coil external dimensions, since volume will usually be the primary constraint for a coil as it will need to fit into a keyfob, credit card or other small volume. Secondly, properties of the core, coil windings as well as the equivalent load placed across the coil are entered. This fixes the Initial Coil Specification. Once the initial coil is built, measurements are made on this coil to determine the coil quality factor. These measurements are used to calculate the Optimum Coil Specification for a second coil.
Keywords: HCS540
 Related Information
 
 App Notes and Source Code
  AN650
  AN650 Source Code