dsPIC33E USB Starter Kit
Buy/Sample Options DM330012
Contact Microchip
Development Tool Selector
Microchip Advanced Parts Selector (MAPS)
CiSAR (Service Request)
dsPIC33E USB Starter Kit 
Part Number: DM330012

The dsPIC33E USB Starter Kit provides a low cost method for the development and testing of USB OTG, Host and Device applications on the 60 MIPS dsPIC33E DSC family. The board contains an on-board programming/debugger, standard A USB and micro A/B connectors, three user-programmable LEDs, three push button switches and an expansion header compatible with the Multimedia Expansion Board (DM320005) and I/O Expansion Board (DM320002). The starter kit comes preloaded with basic Communication Device Class (CDC) demonstration software.

The starter kit contains the following items:

1. dsPIC33E USB Starter Kit Development Board with a dsPIC33EP512MU810-I/PT DSC

2. dsPIC33E USB Starter Kit Information Sheet

3. USB mini-B to standard cable - USB debug cable to debug and power the board

4. USB micro-B to standard cable - USB cable to communicate with the dsPIC33E USB

5.

Programming, Running and Debugging Applications

Use the following procedure for programming/debugging your application programs (the dsPIC33E Start Kit CDC USB Device Demo software available from the link below is mentioned here as an example):

1. Using MPLAB IDE, open the project C:\dsPIC33E PIC24E USB Starter Kit Demo\Firmware\ USB Device - CDC - Basic Demo - dsPIC33E USB Starter Kit.mcp. (This assumes that the demo was installed in the default location)

2. Connect the starter kit to your PC using the provided USB mini-B to full-sized A cable. Note that the jumper in J5 should not be installed.

3. Choose “Starter Kit On Board” as the debugger tool in MPLAB IDE by selecting Debugger > Select Tool> Starter Kit On Board.

4. Choose the debug build configuration by selecting Project > Build Configuration > Debug.

5. Build the project by selecting Project > Build All.

6. Download the code into the starter kit by selecting Debugger > Program.

7. Run the downloaded application software by selecting Debugger > Run. At this time LED2 on the starter kit should turn on.

8. This demo allows the Starter Kit to appear as a serial (COM) port to the host. The instructions for this demo can be found at C:\dsPIC33E PIC24E USB Starter Kit Demo\Documentation\Getting Started\Getting Started - Running the Device - CDC - Basic Demo. See the Running the Demo section.

Downloads