[FAQ]Flying with Explorer 16 Favorites Gallery List

Page: 12 > Showing page 1 of 2
Author
Neiwiertz
Super Member
  • Total Posts : 2093
  • Reward points : 0
  • Joined: 2004/09/01 02:58:52
  • Status: offline
2008/05/17 09:59:25 (permalink)
5 (2)

Flying with Explorer 16 Favorites Gallery List

I was supriced recently to read the breaking news of unlocking the at 18LF4550
as a Pickit II by Rafalw.

Instantly i had the idea to create a collection thread of links for the Explorer 16 any aspect,
enhancement and ideas. Feel free to extend the overview of this list.
post edited by Neiwiertz - 2008/09/07 03:50:32
#1

32 Replies Related Threads

    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/05/17 10:00:57 (permalink)
    0
    -------------------------------------------------------------------
    [ Favorites and Tools                                             ]
    -------------------------------------------------------------------

     
    AVIX-RT RTOS Viewer Plugin for AVIX

    AVIX RTOS AVIX-16 and AVIX-32  for 16-bit and 32-bit microchip mcu's
    AVIX-RT unique Zero-latency and fastest RTOS: www.avix-rt.com

    Intronix 34 Channel LA1034 Logicport

    NirSoft USBDeview

    Eflightworks of Eric (Ohmite)

    MPLAB tab switching addon
     
    Preprocessor calculation of constants
     
    Request Microchip make a Linux compatible 1GHz+ CPU
     

    Problems with AC244005 isolator
     
    Is it possible to use two Pickit 3(or Pickit 2) units from the same
     
    Adjusting Speed of Programmer
    post edited by Neiwiertz - 2013/01/03 16:00:21

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #2
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/05/17 10:02:01 (permalink)
    0
    -------------------------------------------------------------------
    [ Unlocking ICSP (Pickit II) functionality at the 18LF4550 of E16 ]
    -------------------------------------------------------------------


    Explorer 16, 18F4550 (U2) is a PICkit 2?

    Firmware for Explorer 16, 18F4550 (U2) (unofficial)

    Hacking the Microchip Explorer 16 Development Board

    Performing row earse using ICSP

    Operating system support

    Explorer 16 and USB port
    post edited by Neiwiertz - 2010/09/24 10:12:49
    #3
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/05/17 10:03:12 (permalink)
    5 (1)
    -------------------------------------------------------------------
    [ Generic-HID at the 18LF4550 of E16 and USB subject's            ]
    -------------------------------------------------------------------

     
    Question(s) about USB Stack v2013-02-15
     
    USB external transceiver interface
     
    USB HID communication with the PIC18LF4550 on Explorer 16 board

    generic HID transfer-size in Windows (and alternatives)

    PIC USB related web sites from Xiaofan

    USB Firmware Framework Confirmed and Potential Anomalies from Xiaofan

    USB OTG

    HID boot-keyboard & mouse on same device?

    HID Keyboard Without 6 Key Limit?

    posting full code for people to use

    PIC32 USB Embedded Host for Barcode scanner

    UBW32 (32 bit PIC32 based USB Bit Whacker)

    How to get maximum USB throughput

    MCHPUSB driver INF problem in Vista - fixed

    USB Printer Class(Client, not Host)

    How to eject properly the MDD -SD Card Reader example under MAC OSX

    USB Mass Storage Floppy Drive

    Receive Vendor-Specific control commands on 18F4550

    Maximizing USB bulk transfer throughput
     
    Open source USB 1.1 stack running on PIC16F628/628A
     
    USB Composite Device(HID and MIDI)
     
    HID keyboard + mouse using 1 HID report with 2 IDs
     
    host wants string index 0xEE

    host always wants more

    What is meant by DATA0 and DATA1?

    setup transaction not working
     
    PIC32MX USB zero-byte transfers
     
    HID samples for dsPIC33E Demo Board
     
    Interface an USB to dsPIC33EP512MU814 microcontroller
     
    USB PID managed POOl
     
    hid joystick/keyboard multimedia key
     
    USB Ehternet Emulation, RNDIS Question
     
    USB HID report size greater than 64 bytes with Microchip Stack

    Changing from Mouse to Generic HID
     
    Building USB stack projects with XC8 compiler
     
    USB Smart Card reader
     
    restart computer from USB port
     
    U1SOF value (USB_SOF_THRESHOLD_xx) is too short on host
     
    Wired Xbox 360 Controller USB Emulation

    I need MCP2210 dll header file for C/C++
    post edited by Neiwiertz - 2013/09/17 15:57:50
    #4
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/05/17 10:03:51 (permalink)
    0
    -------------------------------------------------------------------
    [ Introducing JTAG functionality at the 18LF4550 of E16           ]
    -------------------------------------------------------------------


    Firmware and Windows application with support JTAG PIC32. At: Firmware for Explorer 16, 18F4550 (U2) (unofficial)

    PIC32 JTAG

    JTAG and PIC
     
    JTAG programmer for PIC32MX795F512L

    Jtag pinning versus ICSP
    post edited by Neiwiertz - 2012/12/30 07:05:38
    #5
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/05/17 10:05:28 (permalink)
    #6
    xiaofan
    Super Member
    • Total Posts : 6247
    • Reward points : 0
    • Joined: 2005/04/14 07:05:25
    • Location: Singapore
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/05/17 22:02:03 (permalink)
    0
    -------------------------------------------------------------------
    [  Microchip Resources for Explorer 16                                          ]
    -------------------------------------------------------------------

    Explorer 16 page:
    http://www.microchip.com/stellent/idcplg?IdcService=SS_GET_PAGE&nodeId=1406&dDocName=en024858&part=DM240001

    PICTail+ page:
    http://www.microchip.com/stellent/idcplg?IdcService=SS_GET_PAGE&nodeId=2519¶m=en530893

    USB stack:
    http://www.microchip.com/usb

    Graphics library:
    http://www.microchip.com/graphics

    TCP/IP stack:
    http://www.microchip.com/tcpip

    TCP/IP Stack V4.50
    http://forum.microchip.com/tm.aspx?m=342759

    TCP/IP Stack V4.51
    http://forum.microchip.com/tm.aspx?m=355202
    post edited by xiaofan - 2008/07/31 05:08:23
    #7
    xiaofan
    Super Member
    • Total Posts : 6247
    • Reward points : 0
    • Joined: 2005/04/14 07:05:25
    • Location: Singapore
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/05/17 22:09:30 (permalink)
    0
    -------------------------------------------------------------------
    [ Demo projects for PIC32                                                          ]
    -------------------------------------------------------------------
    Several examples for PIC32 for the Explorer 16 board
    http://forum.microchip.com/tm.aspx?m=338457
     
    FreeRTOS and AVIX both provide examples for Explorer 16.
    http://www.freertos.org/
    http://www.avix-rt.com/
     

     
    #8
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/05/18 07:31:20 (permalink)
    0
    -------------------------------------------------------------------
    [ Courses and Articles at Explorer 16 board                       ]
    -------------------------------------------------------------------


    How does a real-time operating system (RTOS) work?
    Article at Elektor March 2008 author Leon van Snippenberg, AVIX-RT

    E16 related courses at Elektor
    Elektor Magazine Explorer-16 Project Page Courses: 1 2 3 4

    The Microchip 16-Bit Embedded Control 2007 Design Contest

    Programming 16-Bit PIC Microcontrollers in C: Learning to Fly the PIC 24

    Programming 32-bit Microcontrollers in C: Exploring the PIC32
    post edited by Neiwiertz - 2010/09/24 10:14:35

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #9
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/06/17 00:18:58 (permalink)
    0
    -------------------------------------------------------------------
    [ E16 Interfacing: Graphics PICtail Plus Daughter Board 2         ]
    -------------------------------------------------------------------


    Graphics PICtail™ Plus Daughter Board 2 Errata

    E16 Graphics PICtail Plus Board 2 Compatibility with USB PICtail Plus board FIX

    Collection Graphics related tools by Xiaofan
    Embedded System LCD PC Software Links

    Can i have two shemes in the touchscreen?

    Touchscreen how to input a series numbers to window?

    graphic LCD and graphs

    JPEG decoding

    Widgets

    Progress Bar

    FInding touchscreens compatible to Microchips Graphics Library

    BMP-format

    Graphic LCDs

    Touchscreen Calibration Methods

    gRaphics Library & Touch screen

    Getting the Microchip Graphics Library to work with the SSD1906

    SSD1906 with External TFT

    Graphics Library - SSD1926 2D support?

    Solomon Systech SSD1926 Datasheet

    Graphics Pictail and Explorer 16

    PMP 16 problem & Explorer 16 + Pic32 PIM + Graphics V3 (SSD1926)

    128x64 LCD Interfacing

    HD44780 Hitachi Controller

    Menu driven AN in C

    How to impliment a menu system in LCD?

    scroll down multilevel lcd menu

    Connecting TFT-G240320UTSW-92W-TP-E to SSD1906

    graphic display

    Graphic pictail board Plus pic 32 starter kit

    Bug in Microchip Bitmap and Font converter Utility???

    Getting Problem in Graphic PICtail board

    Graphics Pictail v 1 compatible bug

    PIC24 Animation

    Simple 3D Rendering engine for PIC32

    advice for my first board with a QVGA LCD or alike

    How to use graphics Library

    Best Way to Get a Landscape Display

    Bug in Graphics Library V2.10
     
    Using Mikromedia for PIC32 with Microchip Graphics Library
    post edited by Neiwiertz - 2013/03/04 10:08:59

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #10
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/06/24 11:01:59 (permalink)

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #11
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/08/06 09:46:42 (permalink)

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #14
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/08/30 08:13:47 (permalink)
    0
    -------------------------------------------------------------------
    [ E16 Connect SD MMC PICtail board, FAT and MSD related subject   ]
    -------------------------------------------------------------------


    connecting AC164122 board

    uSD Card Issues

    Please Insert Card

    PICDEM 18 and SPI SD file system problem

    Data corruption in AN1003 Mass Storage code?

    SD card Format

    sd/mmc 18f

    SD Reading CSD trouble resolved

    Royalty free SD Card host implementation

    USB Mass Storage Device not enough bandwidth

    SD card an ENC28J60 on same SPI possible?

    PICtail SD board issue

    SD Card --> SPI Mode

    writing to sd card error

    SD Card Signal Levels

    PIC32 SD/MMC card

    SD card corruption and protection features

    MSD with PIC18F65J50 and Serial Flash

    SD not working

    MMC Interfacing problem

    SD Card SPI Operation

    SDHC ?

    sd-card writing raw without filesystem

    SD Card SPI Init Problem (ACMD41 & CMD1 always return 0x01)

    Bit banging SPI to MMC/SD card problem

    C_SIZE on SD cards - problems...

    SD Card with SDIO

    How to eject properly the MDD -SD Card Reader example under MAC OSX

    How to: Protect SD card against power loss?

    SPI and MMC

    Question about MicroSD Adapter Card Interface with dsPIC33FJ64MC80

    Conceptual question about saving/restoring state.

    SDHC Initialization doesn't respond to ACMD41 (Returns 0x01)

    Kingston 4GB SDHC class 4 cards - multi-block write problems.

    SD CARD intermittent failures

    SD Card Logger - Writing Speed Demos

    PIC32 SD card MSD performance unleashed

    PIC32 SD card reader using DMA?

    Approaching the end of my rope with DMA+SPI
     
    SD Card with SDIO
     
    FSfopen speed
     
    SD Card in SPI Mode
     
    SDC/SDHC/MMC in SPI problem
     
    PIC32 SD card MSD performance unleashed
    post edited by Neiwiertz - 2013/09/17 15:59:02

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #16
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/08/30 08:36:28 (permalink)
    0
    -------------------------------------------------------------------
    [
    E16 Bunch of links: SPI                                         ]
    -------------------------------------------------------------------


    SPI communiction between 2 CPU

    A Problem with SPI Between two PICDEM FS USB boards

    SSPBUF in SPI

    4550 SPI losing first bit

    SPI doing strange things with ICD2

    SPI Interfacing circuit between two microcontrollers

    Have you? SPI in Slave Mode Frame Slave Mode

    spi Chip select

    P24FJ framed SPI slave mode

    SPI framed master

    EDIT: links fixed reported by dan1138
    post edited by Neiwiertz - 2011/01/26 15:15:37

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #17
    dan1138
    Super Member
    • Total Posts : 2770
    • Reward points : 0
    • Joined: 2007/02/21 23:04:16
    • Location: 0
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/09/02 12:52:20 (permalink)
    0
    -------------------------------------------------------------------
    [ E16 MA240014  - PIC24F USB PIM   Manual / Schematic                ]
    -------------------------------------------------------------------

    PIC24FJ256GB110 PIM Manual
    (This was hard to find)

    This link can also be hard to find:
    Explorer 16 Plug-In Modules (PIMs)

    post edited by dan1138 - 2008/09/16 22:51:11
    #18
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/09/17 11:13:03 (permalink)

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #19
    Neiwiertz
    Super Member
    • Total Posts : 2093
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: Flying with Explorer 16 Favorites Gallery List 2008/09/28 13:57:21 (permalink)
    0
    -------------------------------------------------------------------
    [ E16 Maximize Application Reliability Meet IEC 60730 standard’s  ]
    -------------------------------------------------------------------


    Recently i noticed this new Interesting Appnote of Microchip

    Class B Safety Software Library for PIC MCUs and dsPIC DSCs

    Simple RAM test

    MISRA-C and safety code II
     
    Class B Safety Software Library for 8 Bit pics
     
    SWR (software reset) on a PIC24FJ256GB206 device
    post edited by Neiwiertz - 2013/01/03 16:02:53

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #20
    Page: 12 > Showing page 1 of 2
    Jump to:
    © 2018 APG vNext Commercial Version 4.5