Microchip Technology
Welcome to www.microchip.com
Search: Click here to Search Microchip.com
Forums Home Register LoginLog Out Inbox Address Book My Subscription Member List Search My Profile FAQ
RE: PICDEM FS USB bootloader command line application ported to Windows using libusb-win32

RE: PICDEM FS USB bootloader command line application ported to Windows using libusb-win32

 
View related threads: (in this forum | in all forums)

Logged in as: Guest
Users viewing this topic: none
  Printable Version
All Forums >> [Microcontroller Discussion Group] >> USB >> RE: PICDEM FS USB bootloader command line application ported to Windows using libusb-win32 Page: <<   < prev  1 [2]
Login
Message << Older Topic   Newer Topic >>
RE: PICDEM FS USB bootloader command line application p... - Oct. 19, 2007 9:06:03 AM   
tapenot

 

Posts: 7
Joined: Oct. 18, 2007
From: 0
Status: offline
Thanks!
The solution was to change the write functions for the interrupt functions! It's working great!

(in reply to xiaofan)
Post #: 21
RE: PICDEM FS USB bootloader command line application p... - Oct. 19, 2007 6:51:27 PM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
Thanks for the report. I noticed this error when porting the demo application to FreeBSD.

I will contact the original author and tried to get my patch into his archive.

(in reply to tapenot)
Post #: 22
RE: PICDEM FS USB bootloader command line application p... - Oct. 23, 2007 1:27:34 AM   
tapenot

 

Posts: 7
Joined: Oct. 18, 2007
From: 0
Status: offline
Last week i posted that the fsusb_demo code was not working with ubuntu 7.04, and i arranged it fixin the usb_bulk_write/read functions for the usb_interrupt_write/read functions. Today i have updated my ubuntu version to 7.10 and it's not working neither. I guess i have bad luck. Anyway, the error i get when i try to communicate with the Picdem fs usb is:

$ sudo ./fsusb_demo --ledon 3

Locating Microchip(tm) PICDEM(tm) FS USB Demo Board (vendor 0x04d8/product 0x000c)
usb_set_debug: Setting debugging level to 255 (on)
setting USB debug on by adding usb_set_debug(255)
usb_os_init: Found USB VFS at /dev/bus/usb
usb_os_find_busses: Found 005
usb_os_find_busses: Found 001
usb_os_find_busses: Found 002
usb_os_find_busses: Found 003
usb_os_find_busses: Found 004
usb_os_find_devices: Found 001 on 005
usb_os_find_devices: Found 001 on 001
usb_os_find_devices: Found 008 on 002
usb_os_find_devices: Found 001 on 002
error obtaining child information: Inappropriate ioctl for device
usb_os_find_devices: Found 001 on 003
usb_os_find_devices: Found 001 on 004
Found USB PICDEM FS USB Demo Board as device '008' on USB bus 002
USB error: could not set config 1: Device or resource busy
Fatal error> Error setting USB configuration.


Any idea about how can i fix the problem? Thanks.

(in reply to xiaofan)
Post #: 23
RE: PICDEM FS USB bootloader command line application p... - Oct. 23, 2007 1:35:12 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
I just installed Ubuntu 7.10 and I have not tried it (the mirror does not have the packages I need yet).

Have you tried to use my patch?

For the problems, please refer to the following links. Personally I think it is a bad idea to include the demo inside the kernel. Since I have the patch I do not really want to argue for the removal of the kernel patch.

http://www.opensubscriber.com/message/linux-usb-devel@lists.sourceforge.net/7160138.html



/* change by Xiaofan */ 
/* to detach the kernel driver if it is
calimed by some newer kernel ldusb module.
http://www.opensubscriber.com/message/linux-usb-devel@lists.sourceforge.net/7160138.html
*/
#ifdef LINUX

{

int retval;

char dname[32] = {0};

retval = usb_get_driver_np(d, 0, dname, 31);

if (!retval)

usb_detach_kernel_driver_np(d, 0);

}

#endif




(in reply to tapenot)
Post #: 24
RE: PICDEM FS USB bootloader command line application p... - Oct. 23, 2007 2:09:59 AM   
tapenot

 

Posts: 7
Joined: Oct. 18, 2007
From: 0
Status: offline
I've never worked with patches before, so it would be grateful if the explanation could be with more detail.
I understand that i have to add next line to some file, but i don't know which one.
#define USB_VENDOR_ID_MICROCHIP 0x04d8
#define USB_DEVICE_ID_PICDEM 0x000c

Thanks.

(in reply to xiaofan)
Post #: 25
RE: PICDEM FS USB bootloader command line application p... - Oct. 23, 2007 2:19:24 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
http://forum.microchip.com/tm.aspx?m=106426&mpage=1

I've posted my modified version of the code.

(in reply to tapenot)
Post #: 26
RE: PICDEM FS USB bootloader command line application p... - Oct. 23, 2007 2:45:16 AM   
tapenot

 

Posts: 7
Joined: Oct. 18, 2007
From: 0
Status: offline
It's not still working, but as i've noticed you have added the part of code #ifdef LINUX. But where is defined LINUX, this code is not executed.

(in reply to xiaofan)
Post #: 27
RE: PICDEM FS USB bootloader command line application p... - Oct. 23, 2007 2:56:26 AM   
tapenot

 

Posts: 7
Joined: Oct. 18, 2007
From: 0
Status: offline
Yeah, it's working. I guess you just forgot to add #define LINUX at the beggining of the code. I've added it and it's now working. Thanks very much.

Best regards,
tapenot

(in reply to tapenot)
Post #: 28
RE: PICDEM FS USB bootloader command line application p... - Oct. 23, 2007 3:10:34 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
Great! I believe that LINUX is defined by the compiler but maybe I am wrong. Typically this should be done in the Makefile if it is not defined by the compiler. But I am not good at host side programming.

(in reply to tapenot)
Post #: 29
RE: PICDEM FS USB bootloader command line application p... - Oct. 23, 2007 4:38:57 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
I just tried the demo program under Ubuntu 7.10 and it works.

Updated Makefile to fix the LINUX define problem.

# This file is part of fsusb_demo

#

# fsusb_demo is free software; you can redistribute it and/or modify

# it under the terms of the GNU General Public License as published by

# the Free Software Foundation; either version 2 of the License, or

# (at your option) any later version.

#

# fsusb_demo is distributed in the hope that it will be useful, but

# WITHOUT ANY WARRANTY; without even the implied warranty of

# MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU

# General Public License for more details.

#

# You should have received a copy of the GNU General Public License

# along with fsusb_picdem; if not, write to the Free Software

# Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA

# 02110-1301, USA


# For Windows, please put usb.h and MingW version of libusb.a into
# the MingW include and lib directory respectively.
# For Linux only
LIBUSB = /usr/lib


OPTS=-Wall -D_GNU_SOURCE -DLINUX

OBJS=fsusb_demo.o



CFLAGS=$(OPTS) -I$(LIBUSB)/include

LDFLAGS=-L$(LIBUSB)/lib -lusb



# Needed for static linking under OS X:

# LDFLAGS=-lusb -lIOKit -framework CoreFoundation



all: fsusb_demo



fsusb_demo: $(OBJS)

	$(CC) $(CFLAGS) -o $@ $(OBJS) $(LDFLAGS)



clean:

	-rm fsusb_demo *.o

(in reply to tapenot)
Post #: 30
RE: PICDEM FS USB bootloader command line application p... - May 11, 2008 3:11:39 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
quote:

ORIGINAL: xiaofan
Try to use my version of fsusb_demo.c and see how it goes. You may want to change usb_bulk to usb_interrupt as shown below.
/** Send this binary string command. */
static void send_usb(struct usb_dev_handle * d, int len, const char * src)
{
  int r = usb_interrupt_write(d, endpoint_out, (char *)src, len, timeout);
//   if( r != reqLen )
  if( r < 0 )
  {
	  perror("usb PICDEM FS USB write"); bad("USB write failed"); 
  }
}

/** Read this many bytes from this device */
static void recv_usb(struct usb_dev_handle * d, int len, byte * dest)
{
//   int i;
  int r = usb_interrupt_read(d, endpoint_in, dest, len, timeout);
  if( r != len )
  {
	  perror("usb PICDEM FS USB read"); bad("USB read failed"); 
  }
}




The latest V2.1 stack is using Bulk Transfer for the demo project. So we need to change it back to bulk transfer now.

/****************** Internal I/O Commands *****************/

/** Send this binary string command. */
static void send_usb(struct usb_dev_handle * d, int len, const char * src)
{
   int r = usb_bulk_write(d, endpoint_out, (char *)src, len, timeout);
//   if( r != reqLen )
   if( r < 0 )
   {
	  perror("usb PICDEM FS USB write"); bad("USB write failed"); 
   }
}

/** Read this many bytes from this device */
static void recv_usb(struct usb_dev_handle * d, int len, byte * dest)
{
//   int i;
   int r = usb_bulk_read(d, endpoint_in, dest, len, timeout);
   if( r != len )
   {
	  perror("usb PICDEM FS USB read"); bad("USB read failed"); 
   }
}


Tested under Fedore Core 6. Other distro may need similar changes.

The following output is with USB debugging information on.

[mcuee@localhost demo]$ ./fsusb_demo --ledon 3
Locating Microchip(tm) PICDEM(tm) FS USB Demo Board (vendor 0x04d8/product 0x000c)
usb_set_debug: Setting debugging level to 255 (on)
setting USB debug on by adding usb_set_debug(255)
usb_os_init: Found USB VFS at /dev/bus/usb
usb_os_find_busses: Found 003
usb_os_find_busses: Found 001
usb_os_find_busses: Found 002
usb_os_find_devices: couldn't get connect info
usb_os_find_devices: Found 001 on 003
error obtaining child information: Operation not permitted
usb_os_find_devices: couldn't get connect info
usb_os_find_devices: Found 001 on 001
usb_os_find_devices: Found 003 on 001
skipped 1 class/vendor specific interface descriptors
error obtaining child information: Operation not permitted
error obtaining child information: Inappropriate ioctl for device
usb_os_find_devices: couldn't get connect info
usb_os_find_devices: Found 001 on 002
usb_os_find_devices: Found 002 on 002
error obtaining child information: Operation not permitted
error obtaining child information: Inappropriate ioctl for device
Found USB PICDEM FS USB Demo Board as device '002' on USB bus 002
USB error: could not get bound driver: No data available
Communication established.
answer was correct!
Onboard firmware version is 1.0
LED #3 is now on

_____________________________

Blog: http://mcuee.blogspot.com USB links: http://www.microchip.com/forums/tm.aspx?m=123533
No PMs for technical questions, use the forum!

(in reply to xiaofan)
Post #: 31
RE: PICDEM FS USB bootloader command line application p... - May 13, 2008 4:56:32 PM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
I've submitted a patch to Linux ldusb driver maintainer.


---------- Forwarded message ----------
From: Xiaofan Chen
Date: Tue, May 13, 2008 at 9:52 PM
Subject: Linux USB Patch: remove PICDEM FS USB demo (04d8:000c) device from ldusb
To: Greg KH
Cc: Joey Goncalves "Hund, Michael" , USB list <linux-usb AT vger.kernel.org>


On Tue, May 13, 2008 at 1:14 AM, Greg KH wrote:
>
> On Sun, May 11, 2008 at 10:58:42PM +0800, Xiaofan Chen wrote:
> > Microchip has changed the PICDEM FS USB demo device (0x04d8:000c)
> > to use bulk transfer and not interrupt transfer. So I've updated the libusb
> > based program here (Post #31).
> > http://forum.microchip.com/tm.aspx?m=106426&mpage=2
> >
> > So I believe that the in-kernel ldusb driver will no longer work with the
> > demo firmware. Should we just remove it so that no confusions
> > will be caused?
>
> Yes, if you think that is the proper thing to do. Please send me a
> patch to remove this device id from the driver, with this information in
> the body of the email message so that others can refer to it in the
> future.

Joey has agreed to remove this device from ldusb.

Let me try. I have not created any patches for the Linux kernel source.
Hopefully this is ok.


Signed-off-by: Xiaofan Chen
Cc: Michael Hund

--- /home/mcuee/Desktop/linux/linux-2.6.25.3/drivers/usb/misc/ldusb.c.org 2008-05-13
21:37:40.000000000 +0800
+++ /home/mcuee/Desktop/linux/linux-2.6.25.3/drivers/usb/misc/ldusb.c 2008-05-13
21:40:21.000000000 +0800
@@ -63,9 +63,6 @@
#define USB_DEVICE_ID_VERNIER_CYCLOPS 0x0004
#define USB_DEVICE_ID_VERNIER_LCSPEC 0x0006

-#define USB_VENDOR_ID_MICROCHIP 0x04d8
-#define USB_DEVICE_ID_PICDEM 0x000c
-
#ifdef CONFIG_USB_DYNAMIC_MINORS
#define USB_LD_MINOR_BASE 0
#else
@@ -92,7 +89,6 @@ static struct usb_device_id ld_usb_table
{ USB_DEVICE(USB_VENDOR_ID_VERNIER, USB_DEVICE_ID_VERNIER_GOTEMP) },
{ USB_DEVICE(USB_VENDOR_ID_VERNIER, USB_DEVICE_ID_VERNIER_SKIP) },
{ USB_DEVICE(USB_VENDOR_ID_VERNIER, USB_DEVICE_ID_VERNIER_CYCLOPS) },
- { USB_DEVICE(USB_VENDOR_ID_MICROCHIP, USB_DEVICE_ID_PICDEM) },
{ USB_DEVICE(USB_VENDOR_ID_VERNIER, USB_DEVICE_ID_VERNIER_LCSPEC) },
{ } /* Terminating entry */
};


Regards,
Xiaofan
http://mcuee.blogspot.com

_____________________________

Blog: http://mcuee.blogspot.com USB links: http://www.microchip.com/forums/tm.aspx?m=123533
No PMs for technical questions, use the forum!

(in reply to xiaofan)
Post #: 32
RE: PICDEM FS USB bootloader command line application p... - Jul. 26, 2008 8:17:19 PM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
This minor patch has been in the latest Linux 2.6.26 kernel along with another minor patch about PICkit 1 and PICkit 2.

http://www.kernel.org/pub/linux/kernel/v2.6/ChangeLog-2.6.26

********************************************************
commit 5fc89390f74ac42165db477793fb30f6a200e79c
Author: Xiaofan Chen <xiaofanc@gmail.com>
Date: Tue May 13 21:52:00 2008 +0800

USB: remove PICDEM FS USB demo (04d8:000c) device from ldusb

Microchip has changed the PICDEM FS USB demo device (0x04d8:000c)
to use bulk transfer and not interrupt transfer. So I've updated the libusb
based program here (Post #31).
http://forum.microchip.com/tm.aspx?m=106426&mpage=2

So I believe that the in-kernel ldusb driver will no longer work with the
demo firmware. It should be removed.


Signed-off-by: Xiaofan Chen <xiaofanc@gmail.com>
Cc: Michael Hund <MHund@LD-Didactic.de>
Cc: stable <stable@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>


********************************************************
commit f4971031f4acd98423a2903c6517fb3ef1aea8dc
Author: Xiaofan Chen <xiaofanc@gmail.com>
Date: Tue May 13 17:11:59 2008 +0200

HID: add Microchip PICKit 1 and PICkit 2 to blacklist

Microchip PICkit 1 and PICKit 2 USB Programmers are USB HID class of device but
they are not real HID device. They are now supported by libusb based programs
like the following programs.

pk2 and pk2cmd Linux port:
http://home.pacbell.net/theposts/picmicro/
usb_pickit:
http://tfc.duke.free.fr/pickit.html
usb_pickit original version:
http://charm.cs.uiuc.edu/users/olawlor/projects/2003/microchip/

Therefore it ispreferred to blacklist them.

Signed-off-by: Xiaofan Chen <xiaofanc@gmail.com>
Signed-off-by: Jiri Kosina <jkosina@suse.cz>
********************************************************

(in reply to xiaofan)
Post #: 33
RE: PICDEM FS USB bootloader command line application p... - Sep. 7, 2008 6:00:12 PM   
fbcit
Experienced Hobbyist

 

Posts: 1
Joined: Sep. 7, 2008
From: 0
Status: offline
I'm running fsusb_demo on Ubuntu 8.04 Hardy Heron and have noted what appears to be a bug in the PICDEM firmware. When executing --ledon 4, led #3 turns on. Likewise --ledon 3 turns on led #4. I'm new with the PICDEM board and have not looked into the firmware, but fsusb_demo calls for the correct leds to be lit.

(in reply to tapenot)
Post #: 34
RE: PICDEM FS USB bootloader command line application p... - Oct. 18, 2008 3:02:27 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
Some people have some concerns about libusb-win32 0.1.12.1 under Vista. Yes libusb-win32 does not work under Vista 64. It is also said the filter driver will not work under Vista 32 and can cause system problems. But it is said that the device driver works fine.

So when you download libusb-win32 0.1.12.1 release from sourceforge, please just download libusb-win32-device-bin-0.1.12.1.tar.gz.

So I just tried out the demo application under Vista 32 Home premimu using the libusb-win32 device driver and it works fine as reported.

You need to replace the Microchip custom usb driver with the libusb-win32 device driver. You need to use inf wizard to generate the inf file and then "upgrader" Microchip driver to the libusb-win32 device driver. Vista 32 will warn about the unsigned driver during the process.

Here is the sample output.

J:\Downloads\USB\libusb-win32-device-bin-0.1.12.1\bin>ver
Microsoft Windows [Version 6.0.6001]

J:\Downloads\USB\libusb-win32-device-bin-0.1.12.1\bin>fsusb_demo.exe --ledon 4
Locating Microchip(tm) PICDEM(tm) FS USB Demo Board (vendor 0x04d8/product 0x000
c)
setting USB debug on by adding usb_set_debug(255)
LIBUSB_DLL: info: usb_os_init: dll version: 0.1.12.1
LIBUSB_DLL: info: usb_os_init: driver version: 0.1.12.1
LIBUSB_DLL: info: usb_os_find_busses: found bus-0
LIBUSB_DLL: info: usb_os_find_devices: found \\.\libusb0-0001--0x04d8-0x000c on
bus-0
Found USB PICDEM FS USB Demo Board as device '\\.\libusb0-0001--0x04d8-0x000c' o
n USB bus bus-0
Communication established.
answer was correct!
Onboard firmware version is 1.0
LED #4 is now on

J:\Downloads\USB\libusb-win32-device-bin-0.1.12.1\bin>testlibusb.exe -v
Dev #1: Microchip Technology Inc. - PICDEM FS USB Demo Board (C) 2004
wTotalLength:         32
bNumInterfaces:       1
bConfigurationValue:  1
iConfiguration:       0
bmAttributes:         80h
MaxPower:             50
 bInterfaceNumber:   0
 bAlternateSetting:  0
 bNumEndpoints:      2
 bInterfaceClass:    0
 bInterfaceSubClass: 0
 bInterfaceProtocol: 0
 iInterface:         0
   bEndpointAddress: 01h
   bmAttributes:     03h
   wMaxPacketSize:   64
   bInterval:        32
   bRefresh:         0
   bSynchAddress:    0
   bEndpointAddress: 81h
   bmAttributes:     03h
   wMaxPacketSize:   64
   bInterval:        32
   bRefresh:         0
   bSynchAddress:    0

INF file generated:
[Version]
Signature = "$Chicago$"
provider  = %manufacturer%
DriverVer = 03/20/2007,0.1.12.1
CatalogFile = picdemfsusb_000c.cat
CatalogFile.NT = picdemfsusb_000c.cat
CatalogFile.NTAMD64 = picdemfsusb_000c_x64.cat
Class = LibUsbDevices
ClassGUID = {EB781AAF-9C70-4523-A5DF-642A87ECA567}
[ClassInstall]
AddReg=libusb_class_install_add_reg
[ClassInstall32]
AddReg=libusb_class_install_add_reg
[libusb_class_install_add_reg]
HKR,,,,"LibUSB-Win32 Devices"
HKR,,Icon,,"-20"
[Manufacturer]
%manufacturer%=Devices,NT,NTAMD64
;--------------------------------------------------------------------------
; Files
;--------------------------------------------------------------------------
[SourceDisksNames]
1 = "Libusb-Win32 Driver Installation Disk",,
[SourceDisksFiles]
libusb0.sys = 1,,
libusb0.dll = 1,,
libusb0_x64.sys = 1,,
libusb0_x64.dll = 1,,
[DestinationDirs]
libusb_files_sys = 10,system32\drivers
libusb_files_sys_x64 = 10,system32\drivers
libusb_files_dll = 10,system32
libusb_files_dll_wow64 = 10,syswow64
libusb_files_dll_x64 = 10,system32
[libusb_files_sys]
libusb0.sys
[libusb_files_sys_x64]
libusb0.sys,libusb0_x64.sys
[libusb_files_dll]
libusb0.dll
[libusb_files_dll_wow64]
libusb0.dll
[libusb_files_dll_x64]
libusb0.dll,libusb0_x64.dll
;--------------------------------------------------------------------------
; Device driver
;--------------------------------------------------------------------------
[LIBUSB_DEV]
CopyFiles = libusb_files_sys, libusb_files_dll
AddReg    = libusb_add_reg
[LIBUSB_DEV.NT]
CopyFiles = libusb_files_sys, libusb_files_dll
[LIBUSB_DEV.NTAMD64]
CopyFiles = libusb_files_sys_x64, libusb_files_dll_wow64, libusb_files_dll_x64
[LIBUSB_DEV.HW]
DelReg = libusb_del_reg_hw
AddReg = libusb_add_reg_hw
[LIBUSB_DEV.NT.HW]
DelReg = libusb_del_reg_hw
AddReg = libusb_add_reg_hw
[LIBUSB_DEV.NTAMD64.HW]
DelReg = libusb_del_reg_hw
AddReg = libusb_add_reg_hw
[LIBUSB_DEV.NT.Services]
AddService = libusb0, 0x00000002, libusb_add_service
[LIBUSB_DEV.NTAMD64.Services]
AddService = libusb0, 0x00000002, libusb_add_service
[libusb_add_reg]
HKR,,DevLoader,,*ntkern
HKR,,NTMPDriver,,libusb0.sys
; Older versions of this .inf file installed filter drivers. They are not
; needed any more and must be removed
[libusb_del_reg_hw]
HKR,,LowerFilters
HKR,,UpperFilters
; Device properties
[libusb_add_reg_hw]
HKR,,SurpriseRemovalOK, 0x00010001, 1
;--------------------------------------------------------------------------
; Services
;--------------------------------------------------------------------------
[libusb_add_service]
DisplayName    = "LibUsb-Win32 - Kernel Driver 03/20/2007, 0.1.12.1"
ServiceType    = 1
StartType      = 3
ErrorControl   = 0
ServiceBinary  = %12%\libusb0.sys
;--------------------------------------------------------------------------
; Devices
;--------------------------------------------------------------------------
[Devices]
"PICDEM FS USB libusb-win32 Device"=LIBUSB_DEV, USB\VID_04d8&PID_000c
[Devices.NT]
"PICDEM FS USB libusb-win32 Device"=LIBUSB_DEV, USB\VID_04d8&PID_000c
[Devices.NTAMD64]
"PICDEM FS USB libusb-win32 Device"=LIBUSB_DEV, USB\VID_04d8&PID_000c

;--------------------------------------------------------------------------
; Strings
;--------------------------------------------------------------------------
[Strings]
manufacturer = "Microchip Technology, Inc."


< Message edited by xiaofan -- Oct. 18, 2008 3:06:46 AM >


_____________________________

Blog: http://mcuee.blogspot.com USB links: http://www.microchip.com/forums/tm.aspx?m=123533
No PMs for technical questions, use the forum!

(in reply to xiaofan)
Post #: 35
RE: PICDEM FS USB bootloader command line application p... - Sep. 8, 2009 7:13:43 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
The fsusb website is down now. So here is the original code archive in zip format.

Attachment (1)

_____________________________

Blog: http://mcuee.blogspot.com USB links: http://www.microchip.com/forums/tm.aspx?m=123533
No PMs for technical questions, use the forum!

(in reply to xiaofan)
Post #: 36
RE: PICDEM FS USB bootloader command line application p... - Sep. 8, 2009 7:15:21 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
The fsusb zip archive with my minor modifications.

Attachment (1)

_____________________________

Blog: http://mcuee.blogspot.com USB links: http://www.microchip.com/forums/tm.aspx?m=123533
No PMs for technical questions, use the forum!

(in reply to xiaofan)
Post #: 37
RE: PICDEM FS USB bootloader command line application p... - Sep. 8, 2009 7:18:44 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
The zip archive for the demo application (with my modification).

Attachment (1)

_____________________________

Blog: http://mcuee.blogspot.com USB links: http://www.microchip.com/forums/tm.aspx?m=123533
No PMs for technical questions, use the forum!

(in reply to xiaofan)
Post #: 38
RE: PICDEM FS USB bootloader command line application p... - Sep. 8, 2009 7:19:24 AM   
xiaofan

 

Posts: 5331
Joined: Apr. 14, 2005
From: Singapore
Status: offline
Please also take note of the GPL license. Both codes are licensed under GPL.

_____________________________

Blog: http://mcuee.blogspot.com USB links: http://www.microchip.com/forums/tm.aspx?m=123533
No PMs for technical questions, use the forum!

(in reply to xiaofan)
Post #: 39
Page:   <<   < prev  1 [2]
All Forums >> [Microcontroller Discussion Group] >> USB >> RE: PICDEM FS USB bootloader command line application ported to Windows using libusb-win32 Page: <<   < prev  1 [2]
Jump to:





New Messages No New Messages
Hot Topic w/ New Messages Hot Topic w/o New Messages
Locked w/ New Messages Locked w/o New Messages
 Post New Thread
 Reply to Message
 Post New Poll
 Submit Vote
 Delete My Own Post
 Delete My Own Thread
 Rate Posts


  Site Index  |  Legal Information  |  microchipDIRECT  |  Samples  |  Technical Support  |  Investor Information  |  Careers at Microchip  |  Contact Us  |  RSS Feeds ©2009 Microchip Technology Inc.  
  Shanghai ICP Recordal No.09049794  
Forum Software © ASPPlayground.NET Advanced Edition 2.5.5 Unicode

0.266